L2CAP Extension Commands
All L2CAP commands have the following format (this is also displayed for each command description):
Name |
Size (bytes) |
Description |
Opcode |
2 |
|
connectionHandle, CID, or PSM |
2 |
Connection Handle, Channel ID, or Protocol/Service Multiplexer |
Command PDU |
Variable |
Command Parameters |
For the command parameters, please see the corresponding command description below.
Note: The connection handle of 0xFFFE is considered as the loopback connection. All message sent to this connection will be looped back to the local host.
LE Protocol/Service Multiplexer (PSM) values are separated into two ranges:
- Fixed (0x0001 – 0x007F): Values in the first range are assigned by the Bluetooth
SIG and indicate protocols.
- Dynamic (0x0080 – 0x00FF): Values in the second rage are dynamically allocated
and used in conjunction with services defined in the GATT server.
L2CAP_SendData
Opcode: | 0xFCF0 |
Command Description: |
| The L2CAP Data command is used to send an SDU on a Connection Oriented Channel established with the peer device. |
Command Parameters
Layer: |
|
Event Opcode: |
Size: | 2 byte(s) |
Value: | 0xFCF0 |
|
Payload Length(including CID): |
|
Size: | 2 byte(s) |
Value: | size(dataLen)+size(cid) |
|
CID: | Local Channel ID
Size: | 2 byte(s) |
Default: | 0x0040 |
Range: | 0x0040 - 0x007F |
|
SDU: | SDU to be sent on the channel
Size: | input byte(s) |
Default: | “” |
Range: | to L2CAP_SDU_SIZE octets |
|
Events Generated
When this command is received, the host will send the CommandStatus Event. When the SDU transmission is done to the peer device, the L2CAP Send SDU Done Event (L2CAP_SendSduDone) will be generated. If the local channel runs out of credits required to send the SDU, the L2CAP Out of Credit Event (L2CAP_OutOfCredit) will be generated.
L2CAP_RegisterPsm
Opcode: | 0xFCF1 |
Command Description: |
| The L2CAP Register PSM command is used to register a Protocol/Service Multiplexer (PSM) with the L2CAP layer. |
Command Parameters
PSM: | Local Protocol/Service Multiplexer (PSM)
Size: | 2 byte(s) |
Default: | 0x0001 |
Range: | 0x0001 - 0x00FF |
|
MTU: | Maximum SDU size that can be received by PSM
Size: | 2 byte(s) |
Default: | 0x0017 |
Range: | Any 2 byte value |
|
initialPeerCredits: |
| Number of packets that peer device can send to local device
Size: | 2 byte(s) |
Default: | 0x0001 |
Range: | Any 2 byte value |
|
peerCreditThreshold: |
| Low threshold for peer credits
Size: | 2 byte(s) |
Default: | 0x0000 |
Range: | Any 2 byte value |
|
maxNumChannels: | Maximum number of Connection Oriented Channels supported by PSM
Size: | 1 byte(s) |
Default: | 0x01 |
Range: | Any 1 byte value |
|
enableSecurityVerification: |
| Indicates whether to enable security verification by the application for any incoming connection request
Size: | 1 byte(s)
|
Default: | 0x00
|
Range: |
Value |
Description |
0x00 |
No |
0x01 |
Yes |
|
|
Events Generated
When this command is received, the local device will send the CommandStatus Event. If the application wishes to perform its own security verification (by setting enableSecurityVerification to TRUE) for any incoming connection request then an L2CAP Connection Request (L2CAP_ConnectReq) event will be sent up to the application, which must then send an L2CAP Connection Response (L2CAP_ConnectRsp) command back. When the peer credit count reaches the peer credit threshold (specified by peerCreditThreshold), the L2CAP Peer Credit Threshold Event (L2CAP_PeerCreditThreshold) will be generated.
L2CAP_DeregisterPsm
Opcode: | 0xFCF2 |
Command Description: |
| The L2CAP Deregister PSM command is sent to deregister a Protocol/Service Multiplexer (PSM) with the L2CAP layer. |
Command Parameters
PSM: | Local Protocol/Service Multiplexer (PSM) to be deregistered with L2CAP
Size: | 2 byte(s) |
Default: | 0x0001 |
Range: | 0x0001 - 0x00FF |
|
Events Generated
When this request is received, the local device will send the CommandStatus Event.
L2CAP_PsmInfo
Opcode: | 0xFCF3 |
Command Description: |
| The L2CAP PSM Info command is used to get the current information about a given PSM registered with the L2CAP layer. |
Command Parameters
PSM: | Local Protocol/Service Multiplexer (PSM)
Size: | 2 byte(s) |
Default: | 0x0001 |
Range: | 0x0001 - 0x00FF |
|
Events Generated
When this request is received, the local device will send the CommandStatus Event.
Additional Command Status Return Parameters
dataLen: |
|
MTU: |
Condition: | ( StatStatus==0x00) |
Size: | 2 byte(s) |
Range: | |
|
MPS: |
Condition: | ( StatStatus==0x00) |
Size: | 2 byte(s) |
Range: | |
|
initialPeerCredits: |
|
Condition: | ( StatStatus==0x00) |
Size: | 2 byte(s) |
Range: | |
|
peerCreditThreshold: |
|
Condition: | ( StatStatus==0x00) |
Size: | 2 byte(s) |
Range: | |
|
maxNumChannels: |
Condition: | ( StatStatus==0x00) |
Size: | 1 byte(s) |
Range: | |
|
numActiveChannels: |
|
Condition: | ( StatStatus==0x00) |
Size: | 1 byte(s) |
Range: | |
|
L2CAP_PsmChannels
Opcode: | 0xFCF4 |
Command Description: |
| The L2CAP PSM Channels command is used to get the list of all the active Connection Oriented Channels for a given PSM registered with the L2CAP layer. |
Command Parameters
PSM: | Local Protocol/Service Multiplexer (PSM)
Size: | 2 byte(s) |
Default: | 0x0001 |
Range: | 0x0001 - 0x00FF |
|
Events Generated
When this request is received, the local device will send the CommandStatus Event.
Additional Command Status Return Parameters
An array of size “dataLen/2” will be returned containing the parameters starting here:
CID: |
Condition: | ( StatStatus==0x00) |
Size: | 2 byte(s) |
Range: | |
|
The array of parameters ends here.
L2CAP_ChannelInfo
Opcode: | 0xFCF5 |
Command Description: |
| The L2CAP Channel Info command is used to get the current information about an active Connection Oriented Channel. |
Command Parameters
CID: | Local Channel ID
Size: | 2 byte(s) |
Default: | 0x0040 |
Range: | 0x0040 - 0x007F |
|
Events Generated
When this request is received, the local device will send the CommandStatus Event.
Additional Command Status Return Parameters
dataLen: |
|
state: |
Condition: | ( StatStatus==0x00)
|
Size: | 1 byte(s)
|
Range: |
Value |
Description |
0x0000 |
L2CAP_CLOSED |
0x0001 |
L2CAP_OPEN |
0x0002 |
L2CAP_PENDING_CONN_RSP |
0x0003 |
L2CAP_PENDING_DISCONN_RSP |
0x0004 |
L2CAP_PENDING_PARAM_UPDATE_RSP |
0x0005 |
L2CAP_PENDING_INFO_RSP |
0x0006 |
L2CAP_PENDING_SEC_VERIFY |
|
|
PSM: |
Condition: | ( StatStatus==0x00) |
Size: | 2 byte(s) |
Range: | |
|
CID: |
Condition: | ( StatStatus==0x00) |
Size: | 2 byte(s) |
Range: | |
|
MTU: |
Condition: | ( StatStatus==0x00) |
Size: | 2 byte(s) |
Range: | |
|
MPS: |
Condition: | ( StatStatus==0x00) |
Size: | 2 byte(s) |
Range: | |
|
credits: |
Condition: | ( StatStatus==0x00) |
Size: | 2 byte(s) |
Range: | |
|
peerCID: |
Condition: | ( StatStatus==0x00) |
Size: | 2 byte(s) |
Range: | |
|
peerMTU: |
Condition: | ( StatStatus==0x00) |
Size: | 2 byte(s) |
Range: | |
|
peerMPS: |
Condition: | ( StatStatus==0x00) |
Size: | 2 byte(s) |
Range: | |
|
peerCredits: |
Condition: | ( StatStatus==0x00) |
Size: | 2 byte(s) |
Range: | |
|
peerCreditThreshold: |
|
Condition: | ( StatStatus==0x00) |
Size: | 2 byte(s) |
Range: | |
|
L2CAP_ConnectReq
Opcode: | 0xFC94 |
Command Description: |
| The L2CAP Connection Request command is used to create and configure a Connection Oriented Channel between the local and the peer device. |
Command Parameters
Connection Handle: |
| Identifies the connection.
Size: | 2 byte(s) |
Default: | 0x0000 |
Range: | 0x0000 to 0xFFFD |
|
PSM: | Local Protocol/Service Multiplexer (PSM)
Size: | 2 byte(s) |
Default: | 0x0001 |
Range: | 0x0001 - 0x00FF |
|
peerPSM: | Peer Protocol/Service Multiplexer (PSM)
Size: | 2 byte(s) |
Default: | 0x0001 |
Range: | 0x0001 - 0x00FF |
|
Events Generated
When this command is received, the local device will send the CommandStatus Event with the Status parameter after sending an LE Credit Based Connection Request to the peer device. When a new channel has been established, the L2CAP Channel Established Event (L2CAP_ChannelEstablished) will be generated.
L2CAP_ConnectRsp
Opcode: | 0xFC95 |
Command Description: |
| When a device receives an LE Credit Based Connection Request, it must send an LE Credit Based Connection Response back, which is done automatically by the L2CAP layer. However, if the application wishes to perform its own security verification (configurable at PSM registration), then a Connection Request (L2CAP_ConnectReq) event will be sent up to the application which must then send a Connection Response (L2CAP_ConnectRsp) command back indicating the outcome of the connection request. |
Command Parameters
Connection Handle: |
| Identifies the connection.
Size: | 2 byte(s) |
Default: | 0x0000 |
Range: | 0x0000 to 0xFFFD |
|
id: | Identifier to match responses with requests
Size: | 1 byte(s) |
Default: | 0x01 |
Range: | 0x01 - 0xFF |
|
result: | Indicates outcome of connection request
Size: | 2 byte(s)
|
Default: | 0x0000
|
Range: |
Value |
Description |
0x0000 |
L2CAP_CONN_SUCCESS |
0x0001 |
Reserved |
0x0002 |
L2CAP_CONN_PSM_NOT_SUPPORTED |
0x0003 |
Reserved |
0x0004 |
L2CAP_CONN_NO_RESOURCES |
0x0005 |
L2CAP_CONN_INSUFFICIENT_AUTHEN |
0x0006 |
L2CAP_CONN_INSUFFICIENT_AUTHOR |
0x0007 |
L2CAP_CONN_INSUFFICIENT_KEY_SIZE |
0x0008 |
L2CAP_CONN_INSUFFICIENT_ENCRYPT |
0x0009 |
L2CAP_CONN_INVALID_SRC_CID |
0x000A |
L2CAP_CONN_SRC_CID_ALREADY_ALLOC |
|
|
Events Generated
When this request is received, the local device will send the CommandStatus Event with the Status parameter after sending an LE Credit Based Connection Response back to the peer device.
L2CAP_DisconnectReq
Opcode: | 0xFC86 |
Command Description: |
| The L2CAP Disconnection Request is sent to terminate a Connection Oriented Channel established between the local and the peer device. |
Command Parameters
CID: | Local Channel ID
Size: | 2 byte(s) |
Default: | 0x0040 |
Range: | 0x0040 - 0x007F |
|
Events Generated
When this command is received, the local device will send the CommandStatus Event with the Status parameter after forwarding the request to the peer device. When the channel is terminated, the L2CAP Channel Terminated Event (L2CAP_ChannelTerminated) will be generated.
L2CAP_FlowCtrlCredit
Opcode: | 0xFC96 |
Command Description: |
| The LE Flow Control Credit commands are sent when the local device is capable of receiving additional LE-frames on an established L2CAP channel. |
Command Parameters
CID: | Local Channel ID
Size: | 2 byte(s) |
Default: | 0x0040 |
Range: | 0x0040 - 0x007F |
|
peerCredits: | Number of LE-frames that can be sent to local device
Size: | 2 byte(s) |
Default: | 0x0001 |
Range: | 0x0001 - 0xFFFF |
|
Events Generated
When this request is received, the local device will send the CommandStatus Event with the Status parameter after forwarding the request to the peer device. When the peer credit count reaches a specified low threshold (configurable at PSM registration), the L2CAP Peer Credit Threshold Event (L2CAP_PeerCreditThreshold) will be generated.
L2CAP_InfoReq
Opcode: | 0xFC8A |
Command Description: |
| L2CAP Info Request |
Command Parameters
Connection Handle: |
| Identifies the connection.
Size: | 2 byte(s) |
Default: | 0x0000 |
Range: | 0x0000 to 0xFFFD |
|
infoType: | The type of implementation specific information being requested
Size: | 2 byte(s)
|
Default: | 0x0002
|
Range: |
Value |
Description |
0x0001 |
CONNECTIONLESS_MTU |
0x0002 |
EXTENDED_FEATURES |
0x0003 |
FIXED_CHANNELS |
|
|
Events Generated
When this request is received, the local device will send the CommandStatus Event with the Status parameter after forwarding the request to the peer device. After receiving a response from the peer device, the L2CAP_InfoRsp will be generated.
L2CAP_ConnParamUpdateReq
Opcode: | 0xFC92 |
Command Description: |
| The Connection Parameter Update Request is sent from the LE slave device to the LE master device. This request allows the LE slave Host to request a set of new connection parameters. |
Command Parameters
Connection Handle: |
| Identifies the connection.
Size: | 2 byte(s) |
Default: | 0x0000 |
Range: | 0x0000 to 0xFFFD |
|
intervalMin: | The minimum value for the connection event interval
Size: | 2 byte(s) |
Default: | 80 |
Range: | 6 - 3200 |
|
intervalMax: | The maximum value for the connection event interval
Size: | 2 byte(s) |
Default: | 160 |
Range: | 6 - 3200 |
|
slaveLatency: | The slave latency parameter
Size: | 2 byte(s) |
Default: | 0 |
Range: | 0 - 500 |
|
timeoutMultiplier: |
| The connection timeout parameter
Size: | 2 byte(s) |
Default: | 1000 |
Range: | 10 - 3200 |
|
Events Generated
When this request is received, the LE slave host will send the CommandStatus Event with the Status parameter after forwarding the request to the LE master host. The LE master host will send the Connection Parameter Update Response (L2CAP_ConnParamUpdateRsp) event back. If the LE slave host receives this request, it will respond with a Command Reject (L2CAP_CmdReject) with reason 0x0000 (command not understood).