TI Utilities 1.00.00.05 Release Notes

Table of Contents

Introduction

The TI Utilities Component contains generally useful software utilities that are not directly tied to any framework or stack.

Currently, TI Utilities only contains a JSON parser/builder (originally provided with the Network Services Component), but more features will be provided in the future.

Documentation

The following documentation is provided with this release.

What’s New

1.00.00.05

Defects

The following Defects were resolved

ID Summary
None None

Enhancements

The following Enhancements were resolved

ID Summary
TIUTILS-7 Add M33F support
TIUTILS-2 Add M3 support
TIUTILS-1 Move JSON library from Network Services to TI Utilties

Upgrade and Compatibility Information

This is the initial TI Utilities release.

Host Support

Toolchain Support

Network Services supports building libraries for the following ISA/toolchain combinations, your SDK may provide a subset of these libraries:

ISA TI/CCS IAR GCC
M4 18.12.0.LTS 8.32.2 gcc-arm-none-eabi-7-2017-q4-major
M4F 18.12.0.LTS 8.32.2 gcc-arm-none-eabi-7-2017-q4-major

Device Support

Please refer to the SDK Release Notes for device support.

Known Issues

None

Versioning

All releases have 4 segment versions (M.mm.pp.bb). This includes GA and pre-releases (engineering, alpha/EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 1.00.00.00_eng).

This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and bb is an unrestricted set of digits used as an incrementing build counter.

To support multiple side-by-side installations of the product, the product version is encoded in the top level directory.

Subsequent releases of patch upgrades will be identified by the patch number. Typically, these patches only include critical bug fixes.

Technical Support

Last updated: 2019-02-21