GCC Cortex-A9 with hard FP Timing Benchmarks

Target Platform: ti.platforms.sdp4430

Tool Chain Version: 7.2.1

BIOS Version: bios_6_55_00_05_eng

XDCTools Version: xdctools_3_50_05_11_core_eng

Benchmark Cycles
Interrupt Latency 352
Hwi_restore() 8
Hwi_disable() 4
Hwi dispatcher prolog 196
Hwi dispatcher epilog 166
Hwi dispatcher 367
Hardware Interrupt to Blocked Task 617
Hardware Interrupt to Software Interrupt 368
Swi_enable() 78
Swi_disable() 18
Post Software Interrupt Again 24
Post Software Interrupt without Context Switch 81
Post Software Interrupt with Context Switch 151
Create a New Task without Context Switch 1806
Set a Task Priority without a Context Switch 99
Task_yield() 260
Post Semaphore No Waiting Task 81
Post Semaphore No Task Switch 192
Post Semaphore with Task Switch 314
Pend on Semaphore No Context Switch 35
Pend on Semaphore with Task Switch 302
Clock_getTicks() 5
POSIX Create a New Task without Context Switch 3590
POSIX Set a Task Priority without a Context Switch 88
POSIX Post Semaphore No Waiting Task 84
POSIX Post Semaphore No Task Switch 218
POSIX Post Semaphore with Task Switch 343
POSIX Pend on Semaphore No Context Switch 37
POSIX Pend on Semaphore with Task Switch 314

As the timer used to run these benchmarks is run at 1/2 the CPU frequency, an deviation of +-2 cycles is to be expected.

See the SYS/BIOS User’s Guide for more information regarding how interrupt latency is calculated.