279 #ifndef ti_drivers_GPIO__include 280 #define ti_drivers_GPIO__include 306 #define GPIO_STATUS_RESERVED (-32) 314 #define GPIO_STATUS_SUCCESS (0) 322 #define GPIO_STATUS_ERROR (-1) 340 #define GPIO_CFG_IO_MASK 0x00ff0000 341 #define GPIO_CFG_IO_LSB 16 342 #define GPIO_CFG_OUT_TYPE_MASK 0x00060000 343 #define GPIO_CFG_OUT_TYPE_LSB 17 344 #define GPIO_CFG_IN_TYPE_MASK 0x00060000 345 #define GPIO_CFG_IN_TYPE_LSB 17 346 #define GPIO_CFG_OUT_STRENGTH_MASK 0x00f00000 347 #define GPIO_CFG_OUT_STRENGTH_LSB 20 348 #define GPIO_CFG_INT_MASK 0x07000000 349 #define GPIO_CFG_INT_LSB 24 350 #define GPIO_CFG_OUT_BIT 19 360 #define GPIO_CFG_OUTPUT (((uint32_t) 0) << GPIO_CFG_IO_LSB) 361 #define GPIO_CFG_OUT_STD (((uint32_t) 0) << GPIO_CFG_IO_LSB) 362 #define GPIO_CFG_OUT_OD_NOPULL (((uint32_t) 2) << GPIO_CFG_IO_LSB) 363 #define GPIO_CFG_OUT_OD_PU (((uint32_t) 4) << GPIO_CFG_IO_LSB) 364 #define GPIO_CFG_OUT_OD_PD (((uint32_t) 6) << GPIO_CFG_IO_LSB) 366 #define GPIO_CFG_OUT_STR_LOW (((uint32_t) 0) << GPIO_CFG_OUT_STRENGTH_LSB) 367 #define GPIO_CFG_OUT_STR_MED (((uint32_t) 1) << GPIO_CFG_OUT_STRENGTH_LSB) 368 #define GPIO_CFG_OUT_STR_HIGH (((uint32_t) 2) << GPIO_CFG_OUT_STRENGTH_LSB) 370 #define GPIO_CFG_OUT_HIGH (((uint32_t) 1) << GPIO_CFG_OUT_BIT) 371 #define GPIO_CFG_OUT_LOW (((uint32_t) 0) << GPIO_CFG_OUT_BIT) 377 #define GPIO_CFG_INPUT (((uint32_t) 1) << GPIO_CFG_IO_LSB) 378 #define GPIO_CFG_IN_NOPULL (((uint32_t) 1) << GPIO_CFG_IO_LSB) 379 #define GPIO_CFG_IN_PU (((uint32_t) 3) << GPIO_CFG_IO_LSB) 380 #define GPIO_CFG_IN_PD (((uint32_t) 5) << GPIO_CFG_IO_LSB) 386 #define GPIO_CFG_IN_INT_NONE (((uint32_t) 0) << GPIO_CFG_INT_LSB) 387 #define GPIO_CFG_IN_INT_FALLING (((uint32_t) 1) << GPIO_CFG_INT_LSB) 388 #define GPIO_CFG_IN_INT_RISING (((uint32_t) 2) << GPIO_CFG_INT_LSB) 389 #define GPIO_CFG_IN_INT_BOTH_EDGES (((uint32_t) 3) << GPIO_CFG_INT_LSB) 390 #define GPIO_CFG_IN_INT_LOW (((uint32_t) 4) << GPIO_CFG_INT_LSB) 391 #define GPIO_CFG_IN_INT_HIGH (((uint32_t) 5) << GPIO_CFG_INT_LSB) 402 #define GPIO_CFG_IN_INT_ONLY (((uint32_t) 1) << 27) 408 #define GPIO_DO_NOT_CONFIG 0x40000000 422 typedef void (*GPIO_CallbackFxn)(uint_least8_t index); 471 extern void GPIO_getConfig(uint_least8_t index, GPIO_PinConfig *pinConfig);
495 extern uint_fast8_t
GPIO_read(uint_least8_t index);
534 GPIO_PinConfig pinConfig);
549 extern void GPIO_write(uint_least8_t index,
unsigned int value);
void GPIO_write(uint_least8_t index, unsigned int value)
Writes the value to a GPIO pin.
void GPIO_clearInt(uint_least8_t index)
Clear a GPIO pin interrupt flag.
void GPIO_toggle(uint_least8_t index)
Toggles the current state of a GPIO.
void GPIO_enableInt(uint_least8_t index)
Enable a GPIO pin interrupt.
uint32_t GPIO_PinConfig
GPIO pin configuration settings.
Definition: GPIO.h:334
void GPIO_getConfig(uint_least8_t index, GPIO_PinConfig *pinConfig)
Get the current configuration for a gpio pin.
void GPIO_init()
Initializes the GPIO module.
int_fast16_t GPIO_setConfig(uint_least8_t index, GPIO_PinConfig pinConfig)
Configure the gpio pin.
void GPIO_setCallback(uint_least8_t index, GPIO_CallbackFxn callback)
Bind a callback function to a GPIO pin interrupt.
uint_fast8_t GPIO_read(uint_least8_t index)
Reads the value of a GPIO pin.
void GPIO_disableInt(uint_least8_t index)
Disable a GPIO pin interrupt.
void(* GPIO_CallbackFxn)(uint_least8_t index)
GPIO callback function type.
Definition: GPIO.h:422