Quick Start Guide for SimpleLink™ CC13x0 SDK

This guide serves as a road map for users developing applications and products using the TI SimpleLink CC13x0 wireless MCU platform. Whether a seasoned developer or just getting started, TI has created a variety of resources to simplify development on the CC13x0 platform. These resources will enhance your experience with the TI SimpleLink CC13x0 4.10.00.xx Software Development Kit (SDK) from the out-of-the-box demo to production.

This guide will walk you through the initial setup and demonstration of running your first sample application. The guide explains how to install the SimpleLink CC13x0 SDK and lists the various other tools required to get started with your first application. It will also suggest further resources to explore.

Terms and Definitions

General Terms and Acronyms

CCFG
Customer Configuration
Customer Configuration is set by the application and contains configuration parameters for the ROM boot code, device hardware, and device firmware. It contains lock-bits on the last page of flash. You can read more in the Customer Configuration section in the CC13x0 CC26x0 SimpleLink Wireless MCU Technical Reference Manual.
CCS
Code Composer Studio
An integrated development environment to develop applications for Texas Instruments embedded processors. Download: Code Composer Studio
cJTAG
Class 4 IEEE 1149.7: Standard for Reduced-pin and Enhanced-functionality Test Access Port and Boundary-scan Architecture. This is known by acronym cJTAG (compact JTAG).
GCC
GNU Compiler Collection
A compiler system produced by the GNU Project, which support various programming languages such as C and C++.
HIB
Halt In Boot
A mechanism in CC13xx and CC26xx devices to ensure that the external emulator can take control of the device before it executes any application code.
IAR
Refers to IAR Systems’ IAR Embedded Workbench, which is an integrated development environment used for building and debugging embedded applications.
JTAG
IEEE standard 1149.1: Standard Test Access Port and Boundary Scan Architecture Test Access Port (TAP). This standard is known by the acronym JTAG (Joint Test Action Group).
MCU
Microcontroller Unit
A small computer on a single integrated circuit.
OAD
Over the Air Download
The process of performing a device firmware update over the air.
ROM
Read-only Memory
Type of non-volatile memory used in computers. Once data is written to ROM, the data cannot be removed and can only be read.
VIMS
Versatile Instruction Memory System
A system control module that handles access to the device memory areas from the CPU and system bus. You can read more in the CC13x0 CC26x0 SimpleLink Wireless MCU Technical Reference Manual.