Changelog
Table of Contents
New Features
BLE-Stack
ID | Summary |
---|---|
None | None |
EasyLink
ID | Summary |
---|---|
None | None |
TI 15.4-Stack
ID | Summary |
---|---|
TI154STACK-2838 | Moved definition of macMRFSKStdPhyTable and macMRFSKGenPhyTable to mac_cfg.c |
TI-RTOS and Drivers
ID | Summary |
---|---|
TIDRIVERS-3801 | Integrate CC13xx/26xx DriverLib 3.05.12 |
TIDRIVERS-3677 | Restore CRYPTOCC26XX_KEY_ANY to previous enum value |
TIDRIVERS-3657 | Support for TCXO on CC13x2/CC26x2 devices |
TIDRIVERS-3653 | i2secho example improvements: align use of defines, show sample data treatment, use CD quality settings |
Fixed Issues
BLE-Stack
ID | Summary |
---|---|
None | None |
EasyLink
ID | Summary |
---|---|
EZLINKPROP-712 | Error in calculation of command time in EasyLink.c |
EZLINKPROP-654 | wrong switch setting in rfWsnNodeBleAdv |
TI 15.4-Stack
ID | Summary |
---|---|
TI154STACK-2970 | Fixed issue of “Incorrect Readme File present in Sensor_OAD Project” |
TI154STACK-2879 | Fixed issue with “CollectorApp.html not located in the sdk” |
TI154STACK-2859 | Fixed issue of “Collector in Linux GW SDK does not handle the co-processor resets or the collector app reset” |
TI154STACK-2858 | Fixed issue of MT_MSG_reset in Linux Gateway SDK triggering a ping command instead of triggering a reset |
TI154STACK-2670 | Fixed issue of “Sensor fails to decrypt incoming packets after switching through 3 different collectors” |
TI-RTOS and Drivers
ID | Summary |
---|---|
TIRTOS-1891 | include error with errno.h, #include_next errno.h |
TIRTOS-3776 | I2C close should nullify object->handle after delete calls |
TIRTOS-3678 | Remove CryptoCC26XX power notification |
TIRTOS-3669 | All the content of the I2S buffer is not transferred in MONO channel mode |
TIRTOS-3660 | The functions I2S_stopRead() and I2S_stopWrite() cannot be called in a HWI context even if the transactions queue is empty |
TIRTOS-3652 | i2secho example doesn’t align use of frame settings with codec on CC3200AUDBOOST |
TIRTOS-3650 | CC13XX-CC26XX: guarding against I2C hardware state retention issues |
TIRTOS-3647 | CC13XX-CC26XX: I2CCC26XX_hwiFxn post Swi twice following a address NACK |
TIRTOS-3552 | ADCBufCC26XX/X2: Closing the driver does not enforce releasing the semaphore |
TIRTOS-3546 | ADCBufCC26XX/X2: Driver unable to open if ADC previously been used by the Sensor Controller. |
RFDRIVER-89 | Set default value of unused variables in single mode and in RF_postCmd |
RFDRIVER-87 | Weak symbol in RF driver is not being resolved correctly in DMM project |
Known Issues and Limitations
BLE-Stack
ID | Summary |
---|---|
- | Currently there is no API supporting Tx power back-off on an individual channel. As a work-around, please lower the Tx power on every channel. |
- | Number of simultaneous connections may be limited when attempting concurrent LE Secure Connections pairings. Suggested workaround is to perform LE Secure Connections pairing on an individual connection basis. |
- | Calling GAP_DeviceInit twice may result in a “Invalid LMP Parameters” event which can be safely ignored. |
- | The Simple Network Processor (SNP) and L2CAP Connection Oriented Channels (L2CAP COC) are not available in this release. |
- | Cache-As-RAM project configurations are experimental. |
EasyLink
ID | Summary |
---|---|
None | None |
TI 15.4-Stack
ID | Summary |
---|---|
TI154STACK-2928 | Very low polling Interval (<400msec) causes Joining problems |
TI-RTOS and Drivers
ID | Summary |
---|---|
TIDRIVERS-3636 | I2C_transfer() occasionally fails when called from an interrupt context |
TIDRIVERS-3635 | UART_read returns 0 in portable after a power-cycle on CC13x0 and CC26x0 devices |
TIDRIVERS-3626 | Sysconfig cannot configure SPI four pin mode for LPRF boards |
TIDRIVERS-1642 | NVSSPI25x driver does not work when using internal SPI CS |