Changelog
Table of Contents
New Features
BLE-Stack
ID | Summary |
---|---|
None | None |
EasyLink
ID | Summary |
---|---|
None | None |
TI 15.4-Stack
ID | Summary |
---|---|
None | None |
TI-RTOS and Drivers
ID | Summary |
---|---|
TIRTOS-1543 | Update examples and board files to support Sharp128 Display as the default (was Sharp96) |
TIRTOS-1430 | Call pthread_exit() in run stub to handle termination sequence |
TIRTOS-1016 | examplesgen – revise the process of importing examples to IAR |
TIDRIVERS-1539 | Include PDM driver assembly files and give them BSD license |
TIDRIVERS-1436 | Example pinstandby stand-by current is too high |
TIDRIVERS-1421 | SPI drivers for MSP432E and CC13X2/CC26X2 should use the DMA driver in ping-pong mode |
TIDRIVERS-953 | Implement generic AES_CBC driver |
Fixed Issues
BLE-Stack
ID | Summary |
---|---|
BLESTACK-4097 | Fixed Issue where ADV stops after a while |
BLESTACK-4098 | Implement Bluetooth Pairing Erratum 10734 |
BLESTACK-4085 | Fixed Issue where Adv/Data Length RFU Bits did not get masked out |
EasyLink
ID | Summary |
---|---|
EZLINKPROP-554 | The GPTimer module parameters have been updated to include direction and debugStallMode fields |
EZLINKPROP-544 | EasyLink: Fixed an issue where a mutex was not released prior to function returning on an error condition. |
EZLINKPROP-525 | Missing #include “cpu.h” in functions where CPUdelay() is called |
EZLINKPROP-522 | EasyLink NP: Fixed an issue where address filtering did not work for address sizes greater than 2 bytes |
TI 15.4-Stack
ID | Summary |
---|---|
TI154STACK-2296 | Fixed API macWrapperAddKeyInitFCtr to update keys correctly when using newKeyFlag = true |
TI154STACK-2280 | Fixed issue: When removing a device from the network, we are not removing this device from the Key Table |
TI154STACK-2262 | Fixed issue: CLLC does not report to the application if a device rejoins via association req to the network |
TI154STACK-2251 | Fixed issue where 15.4 sensors Disconnect from 10+ node network after 2+ hrs at high report interval and never reconnect |
TI154STACK-2022 | Fixed issue where Energy detect when doing a channel scan to find best channel always returns zero |
TI-RTOS and Drivers
ID | Summary |
---|---|
TIRTOS-1550 | The main_tirtos.c file in many examples has flawed logic |
TIDRIVERS-1703 | ECC drivers do not erase PKA RAM after operation |
TIDRIVERS-1681 | NVSSPI25X_close() does not wait for the external flash to be ready |
TIDRIVERS-1675 | CC13XX-CC26XX: UART_writeCancel do not check if TX is active which can result in pending write due to lost callback |
TIDRIVERS-1659 | CC1350 rfDriverCallback: Need to swtich antenna to Sub-1 GHz for High Speed Mode |
TIDRIVERS-1622 | RF Driver RF_FsmEventInitChangePhy race condition |
TIDRIVERS-1582 | CC13XX-CC26XX: I2C Driver unable to recover from BUSBUSY status if set when performing I2C_close |
TIDRIVERS-1478 | Support dynamic PA switching on CC13x2P devices |
TIDRIVERS-1446 | Race condition in UARTCC26XX_read() for return partial case |
TIDRIVERS-1407 | Make UART_close() more robust against unexpected UART_read() calls |
Known Issues and Limitations
BLE-Stack
ID | Summary |
---|---|
None | None |
EasyLink
ID | Summary |
---|---|
None | None |
TI 15.4-Stack
ID | Summary |
---|---|
TI154STACK-2488 | The SimpleLink LRM on CC13x2 is not compatible with the SimpleLink LRM on CC13x0 |
TI-RTOS and Drivers
ID | Summary |
---|---|
None | None |