Release Notes

Table of Contents

Introduction

This is a GA release of the Core SDK 3.70.00.12 for the CC26xx and CC13xx devices.

Documentation

Open the documentation overview web page file in the SDK’s Doc folder for a full list of documentation.

For further information on the drivers included in this product, see the Drivers Release Notes

What’s New

Upgrade and Compatibility Information

This release breaks compatibility with previous releases of the Core SDK in the following ways:

Host Support

See the SDK release notes for a description of which host operating systems are supported in this release.

Dependencies

See the SDK release notes for a description of which components and tools are required to work with this product.

Device Support

See the SDK release notes for a list of TI devices that are supported in this product.

Validation Information

The Core SDK was validated with the following components:

Known Issues

ID Summary
TIRTOS-1527 clock_settime should not discard tv_nsec
TIRTOS-1435 clock_nanosleep() with CLOCK_REALTIME broken on msp432
TIDRIVERS-1715 Closing uart (but only in callback mode) adds additional current
TIDRIVERS-1642 NVSSPI25x driver does not work when using internal SPI CS
TIDRIVERS-1464 Setting CC26XX IOC config as edge triggered and muxing in a non-GPIO configuration can cause spurrious events

Versioning

This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.

Prior Release Changes

A summary of changes made in previous releases of this product can be found in the product Change Log.