SimpleLink™ CC13x0 SDK 2.30.00.20 Change log
Table of Contents
New Features
TI 15.4 Stack
TI Proprietary-RF
TI-RTOS and Drivers
This release previews a new tool coming out called SysConfig, which allows graphical configuration of TI’s drivers. For more information, see the README file included in the syscfg directory as well as the Wiki page located here.
TIRTOS-1543 |
Update examples and board files to support Sharp128 Display as the default (was Sharp96) |
TIRTOS-1430 |
Call pthread_exit() in run stub to handle termination sequence |
TIRTOS-1016 |
examplesgen – revise the process of importing examples to IAR |
TIRTOS-1539 |
Include PDM driver assembly files and give them BSD license |
TIRTOS-1436 |
Example pinstandby stand-by current is too high |
TIRTOS-1421 |
SPI drivers for MSP432E and CC13X2/CC26X2 should use the DMA driver in ping-pong mode |
TIRTOS-953 |
Implement generic AES_CBC driver |
Fixed Issues
TI 15.4 Stack
TI154STACK-2212 |
Fixed issue where Sensor accepts coordinator realignment from any collector regardless of this collector being its parent |
TI154STACK-2207 |
Fixed issue where Sensor stops working properly if it fails an orphan scan because of channel access failure due to high energy in the channel |
TI154STACK-2183 |
Fixed comments in config.h on CONFIG_SCAN_DURATION |
TI154STACK-2044 |
Fixed issue where adding SPI to TI 15.4 collector example causes autoheap issues in IAR. |
TI Proprietary-RF
EZLINKPROP-477 |
Fixed an issue where the PER example displays incorrect max power for BLE mode. |
EZLINKPROP-462 |
Fixed an issue where the idle timeout was being set incorrectly in EasyLink_Init() and EasyLink_setCtrl(). |
EZLINKPROP-399 |
Fixed an issue where EasyLink_setFrequency only modified the CMD_FS, not the setup command. |
EZLINKPROP-388 |
Fixed an issue where the Tx Power displayed was wrong when using HSM with the PER example when using CC1190. |
EZLINKPROP-386 |
Fixed an issue where the Tx Power displayed was wrong when using OOK with the PER example when using CC1190. |
EZLINKPROP-376 |
Fixed an issue where, when using HSM, the tx power used was sometimes too low. |
TI-RTOS and Drivers
TIRTOS-1550 |
The main_tirtos.c file in many examples has flawed logic |
TIDRIVERS-1703 |
ECC drivers do not erase PKA RAM after operation |
TIDRIVERS-1681 |
NVSSPI25X_close() does not wait for the external flash to be ready |
TIDRIVERS-1675 |
CC13XX-CC26XX: UART_writeCancel do not check if TX is active which can result in pending write due to lost callback |
TIDRIVERS-1659 |
CC1350 rfDriverCallback: Need to swtich antenna to Sub-1 GHz for High Speed Mode |
TIDRIVERS-1622 |
RF Driver RF_FsmEventInitChangePhy race condition |
TIDRIVERS-1582 |
CC13XX-CC26XX: I2C Driver unable to recover from BUSBUSY status if set when performing I2C_close |
TIDRIVERS-1478 |
Support dynamic PA switching on CC13x2P devices |
TIDRIVERS-1446 |
Race condition in UARTCC26XX_read() for return partial case |
TIDRIVERS-1407 |
Make UART_close() more robust against unexpected UART_read() calls |
Known Issues
TI 15.4 Stack
TI Proprietary-RF
TI-RTOS and Drivers