GPIO

Instance: GPIO
Component: GPIO
Base address: 0x40022000


MCU GPIO - I/F for controlling and reading IO status and IO event status

TOP:GPIO Register Summary

Register Name

Type

Register Width (Bits)

Register Reset

Address Offset

Physical Address

DOUT3_0

RW

32

0x0000 0000

0x0000 0000

0x4002 2000

DOUT7_4

RW

32

0x0000 0000

0x0000 0004

0x4002 2004

DOUT11_8

RW

32

0x0000 0000

0x0000 0008

0x4002 2008

DOUT15_12

RW

32

0x0000 0000

0x0000 000C

0x4002 200C

DOUT19_16

RW

32

0x0000 0000

0x0000 0010

0x4002 2010

DOUT23_20

RW

32

0x0000 0000

0x0000 0014

0x4002 2014

DOUT27_24

RW

32

0x0000 0000

0x0000 0018

0x4002 2018

DOUT31_28

RW

32

0x0000 0000

0x0000 001C

0x4002 201C

DOUT31_0

RW

32

0x0000 0000

0x0000 0080

0x4002 2080

DOUTSET31_0

WO

32

0x0000 0000

0x0000 0090

0x4002 2090

DOUTCLR31_0

WO

32

0x0000 0000

0x0000 00A0

0x4002 20A0

DOUTTGL31_0

RW

32

0x0000 0000

0x0000 00B0

0x4002 20B0

DIN31_0

RO

32

0x0000 0000

0x0000 00C0

0x4002 20C0

DOE31_0

RW

32

0x0000 0000

0x0000 00D0

0x4002 20D0

EVFLAGS31_0

RW

32

0x0000 0000

0x0000 00E0

0x4002 20E0

TOP:GPIO Register Descriptions

TOP:GPIO:DOUT3_0

Address Offset 0x0000 0000
Physical Address 0x4002 2000 Instance 0x4002 2000
Description Data Out 0 to 3

Alias register for byte access to each bit in DOUT31_0
Type RW
Bits Field Name Description Type Reset
31:25 RESERVED25 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
24 DIO3 Sets the state of the pin that is configured as DIO#3, if the corresponding DOE31_0 bitfield is set. WO 0
23:17 RESERVED17 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
16 DIO2 Sets the state of the pin that is configured as DIO#2, if the corresponding DOE31_0 bitfield is set. WO 0
15:9 RESERVED9 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
8 DIO1 Sets the state of the pin that is configured as DIO#1, if the corresponding DOE31_0 bitfield is set. WO 0
7:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
0 DIO0 Sets the state of the pin that is configured as DIO#0, if the corresponding DOE31_0 bitfield is set. WO 0

TOP:GPIO:DOUT7_4

Address Offset 0x0000 0004
Physical Address 0x4002 2004 Instance 0x4002 2004
Description Data Out 4 to 7

Alias register for byte access to each bit in DOUT31_0
Type RW
Bits Field Name Description Type Reset
31:25 RESERVED25 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
24 DIO7 Sets the state of the pin that is configured as DIO#7, if the corresponding DOE31_0 bitfield is set. WO 0
23:17 RESERVED17 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
16 DIO6 Sets the state of the pin that is configured as DIO#6, if the corresponding DOE31_0 bitfield is set. WO 0
15:9 RESERVED9 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
8 DIO5 Sets the state of the pin that is configured as DIO#5, if the corresponding DOE31_0 bitfield is set. WO 0
7:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
0 DIO4 Sets the state of the pin that is configured as DIO#4, if the corresponding DOE31_0 bitfield is set. WO 0

TOP:GPIO:DOUT11_8

Address Offset 0x0000 0008
Physical Address 0x4002 2008 Instance 0x4002 2008
Description Data Out 8 to 11

Alias register for byte access to each bit in DOUT31_0
Type RW
Bits Field Name Description Type Reset
31:25 RESERVED25 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
24 DIO11 Sets the state of the pin that is configured as DIO#11, if the corresponding DOE31_0 bitfield is set. WO 0
23:17 RESERVED17 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
16 DIO10 Sets the state of the pin that is configured as DIO#10, if the corresponding DOE31_0 bitfield is set. WO 0
15:9 RESERVED9 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
8 DIO9 Sets the state of the pin that is configured as DIO#9, if the corresponding DOE31_0 bitfield is set. WO 0
7:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
0 DIO8 Sets the state of the pin that is configured as DIO#8, if the corresponding DOE31_0 bitfield is set. WO 0

TOP:GPIO:DOUT15_12

Address Offset 0x0000 000C
Physical Address 0x4002 200C Instance 0x4002 200C
Description Data Out 12 to 15

Alias register for byte access to each bit in DOUT31_0
Type RW
Bits Field Name Description Type Reset
31:25 RESERVED25 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
24 DIO15 Sets the state of the pin that is configured as DIO#15, if the corresponding DOE31_0 bitfield is set. WO 0
23:17 RESERVED17 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
16 DIO14 Sets the state of the pin that is configured as DIO#14, if the corresponding DOE31_0 bitfield is set. WO 0
15:9 RESERVED9 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
8 DIO13 Sets the state of the pin that is configured as DIO#13, if the corresponding DOE31_0 bitfield is set. WO 0
7:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
0 DIO12 Sets the state of the pin that is configured as DIO#12, if the corresponding DOE31_0 bitfield is set. WO 0

TOP:GPIO:DOUT19_16

Address Offset 0x0000 0010
Physical Address 0x4002 2010 Instance 0x4002 2010
Description Data Out 16 to 19

Alias register for byte access to each bit in DOUT31_0
Type RW
Bits Field Name Description Type Reset
31:25 RESERVED25 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
24 DIO19 Sets the state of the pin that is configured as DIO#19, if the corresponding DOE31_0 bitfield is set. WO 0
23:17 RESERVED17 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
16 DIO18 Sets the state of the pin that is configured as DIO#18, if the corresponding DOE31_0 bitfield is set. WO 0
15:9 RESERVED9 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
8 DIO17 Sets the state of the pin that is configured as DIO#17, if the corresponding DOE31_0 bitfield is set. WO 0
7:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
0 DIO16 Sets the state of the pin that is configured as DIO#16, if the corresponding DOE31_0 bitfield is set. WO 0

TOP:GPIO:DOUT23_20

Address Offset 0x0000 0014
Physical Address 0x4002 2014 Instance 0x4002 2014
Description Data Out 20 to 23

Alias register for byte access to each bit in DOUT31_0
Type RW
Bits Field Name Description Type Reset
31:25 RESERVED25 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
24 DIO23 Sets the state of the pin that is configured as DIO#23, if the corresponding DOE31_0 bitfield is set. WO 0
23:17 RESERVED17 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
16 DIO22 Sets the state of the pin that is configured as DIO#22, if the corresponding DOE31_0 bitfield is set. WO 0
15:9 RESERVED9 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
8 DIO21 Sets the state of the pin that is configured as DIO#21, if the corresponding DOE31_0 bitfield is set. WO 0
7:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
0 DIO20 Sets the state of the pin that is configured as DIO#20, if the corresponding DOE31_0 bitfield is set. WO 0

TOP:GPIO:DOUT27_24

Address Offset 0x0000 0018
Physical Address 0x4002 2018 Instance 0x4002 2018
Description Data Out 24 to 27

Alias register for byte access to each bit in DOUT31_0
Type RW
Bits Field Name Description Type Reset
31:25 RESERVED25 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
24 DIO27 Sets the state of the pin that is configured as DIO#27, if the corresponding DOE31_0 bitfield is set. WO 0
23:17 RESERVED17 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
16 DIO26 Sets the state of the pin that is configured as DIO#26, if the corresponding DOE31_0 bitfield is set. WO 0
15:9 RESERVED9 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
8 DIO25 Sets the state of the pin that is configured as DIO#25, if the corresponding DOE31_0 bitfield is set. WO 0
7:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
0 DIO24 Sets the state of the pin that is configured as DIO#24, if the corresponding DOE31_0 bitfield is set. WO 0

TOP:GPIO:DOUT31_28

Address Offset 0x0000 001C
Physical Address 0x4002 201C Instance 0x4002 201C
Description Data Out 28 to 31

Alias register for byte access to each bit in DOUT31_0
Type RW
Bits Field Name Description Type Reset
31:25 RESERVED25 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
24 DIO31 Sets the state of the pin that is configured as DIO#31, if the corresponding DOE31_0 bitfield is set. WO 0
23:17 RESERVED17 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
16 DIO30 Sets the state of the pin that is configured as DIO#30, if the corresponding DOE31_0 bitfield is set. WO 0
15:9 RESERVED9 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
8 DIO29 Sets the state of the pin that is configured as DIO#29, if the corresponding DOE31_0 bitfield is set. WO 0
7:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
0 DIO28 Sets the state of the pin that is configured as DIO#28, if the corresponding DOE31_0 bitfield is set. WO 0

TOP:GPIO:DOUT31_0

Address Offset 0x0000 0080
Physical Address 0x4002 2080 Instance 0x4002 2080
Description Data Output for DIO 0 to 31
Type RW
Bits Field Name Description Type Reset
31 DIO31 Data output for DIO 31 RW 0
30 DIO30 Data output for DIO 30 RW 0
29 DIO29 Data output for DIO 29 RW 0
28 DIO28 Data output for DIO 28 RW 0
27 DIO27 Data output for DIO 27 RW 0
26 DIO26 Data output for DIO 26 RW 0
25 DIO25 Data output for DIO 25 RW 0
24 DIO24 Data output for DIO 24 RW 0
23 DIO23 Data output for DIO 23 RW 0
22 DIO22 Data output for DIO 22 RW 0
21 DIO21 Data output for DIO 21 RW 0
20 DIO20 Data output for DIO 20 RW 0
19 DIO19 Data output for DIO 19 RW 0
18 DIO18 Data output for DIO 18 RW 0
17 DIO17 Data output for DIO 17 RW 0
16 DIO16 Data output for DIO 16 RW 0
15 DIO15 Data output for DIO 15 RW 0
14 DIO14 Data output for DIO 14 RW 0
13 DIO13 Data output for DIO 13 RW 0
12 DIO12 Data output for DIO 12 RW 0
11 DIO11 Data output for DIO 11 RW 0
10 DIO10 Data output for DIO 10 RW 0
9 DIO9 Data output for DIO 9 RW 0
8 DIO8 Data output for DIO 8 RW 0
7 DIO7 Data output for DIO 7 RW 0
6 DIO6 Data output for DIO 6 RW 0
5 DIO5 Data output for DIO 5 RW 0
4 DIO4 Data output for DIO 4 RW 0
3 DIO3 Data output for DIO 3 RW 0
2 DIO2 Data output for DIO 2 RW 0
1 DIO1 Data output for DIO 1 RW 0
0 DIO0 Data output for DIO 0 RW 0

TOP:GPIO:DOUTSET31_0

Address Offset 0x0000 0090
Physical Address 0x4002 2090 Instance 0x4002 2090
Description Data Out Set

Writing 1 to a bit position sets the corresponding bit in the DOUT31_0 register
Type WO
Bits Field Name Description Type Reset
31 DIO31 Set bit 31 WO 0
30 DIO30 Set bit 30 WO 0
29 DIO29 Set bit 29 WO 0
28 DIO28 Set bit 28 WO 0
27 DIO27 Set bit 27 WO 0
26 DIO26 Set bit 26 WO 0
25 DIO25 Set bit 25 WO 0
24 DIO24 Set bit 24 WO 0
23 DIO23 Set bit 23 WO 0
22 DIO22 Set bit 22 WO 0
21 DIO21 Set bit 21 WO 0
20 DIO20 Set bit 20 WO 0
19 DIO19 Set bit 19 WO 0
18 DIO18 Set bit 18 WO 0
17 DIO17 Set bit 17 WO 0
16 DIO16 Set bit 16 WO 0
15 DIO15 Set bit 15 WO 0
14 DIO14 Set bit 14 WO 0
13 DIO13 Set bit 13 WO 0
12 DIO12 Set bit 12 WO 0
11 DIO11 Set bit 11 WO 0
10 DIO10 Set bit 10 WO 0
9 DIO9 Set bit 9 WO 0
8 DIO8 Set bit 8 WO 0
7 DIO7 Set bit 7 WO 0
6 DIO6 Set bit 6 WO 0
5 DIO5 Set bit 5 WO 0
4 DIO4 Set bit 4 WO 0
3 DIO3 Set bit 3 WO 0
2 DIO2 Set bit 2 WO 0
1 DIO1 Set bit 1 WO 0
0 DIO0 Set bit 0 WO 0

TOP:GPIO:DOUTCLR31_0

Address Offset 0x0000 00A0
Physical Address 0x4002 20A0 Instance 0x4002 20A0
Description Data Out Clear

Writing 1 to a bit position clears the corresponding bit in the DOUT31_0 register
Type WO
Bits Field Name Description Type Reset
31 DIO31 Clears bit 31 WO 0
30 DIO30 Clears bit 30 WO 0
29 DIO29 Clears bit 29 WO 0
28 DIO28 Clears bit 28 WO 0
27 DIO27 Clears bit 27 WO 0
26 DIO26 Clears bit 26 WO 0
25 DIO25 Clears bit 25 WO 0
24 DIO24 Clears bit 24 WO 0
23 DIO23 Clears bit 23 WO 0
22 DIO22 Clears bit 22 WO 0
21 DIO21 Clears bit 21 WO 0
20 DIO20 Clears bit 20 WO 0
19 DIO19 Clears bit 19 WO 0
18 DIO18 Clears bit 18 WO 0
17 DIO17 Clears bit 17 WO 0
16 DIO16 Clears bit 16 WO 0
15 DIO15 Clears bit 15 WO 0
14 DIO14 Clears bit 14 WO 0
13 DIO13 Clears bit 13 WO 0
12 DIO12 Clears bit 12 WO 0
11 DIO11 Clears bit 11 WO 0
10 DIO10 Clears bit 10 WO 0
9 DIO9 Clears bit 9 WO 0
8 DIO8 Clears bit 8 WO 0
7 DIO7 Clears bit 7 WO 0
6 DIO6 Clears bit 6 WO 0
5 DIO5 Clears bit 5 WO 0
4 DIO4 Clears bit 4 WO 0
3 DIO3 Clears bit 3 WO 0
2 DIO2 Clears bit 2 WO 0
1 DIO1 Clears bit 1 WO 0
0 DIO0 Clears bit 0 WO 0

TOP:GPIO:DOUTTGL31_0

Address Offset 0x0000 00B0
Physical Address 0x4002 20B0 Instance 0x4002 20B0
Description Data Out Toggle

Writing 1 to a bit position will invert the corresponding DIO output.
Type RW
Bits Field Name Description Type Reset
31 DIO31 Toggles bit 31 RW 0
30 DIO30 Toggles bit 30 RW 0
29 DIO29 Toggles bit 29 RW 0
28 DIO28 Toggles bit 28 RW 0
27 DIO27 Toggles bit 27 RW 0
26 DIO26 Toggles bit 26 RW 0
25 DIO25 Toggles bit 25 RW 0
24 DIO24 Toggles bit 24 RW 0
23 DIO23 Toggles bit 23 RW 0
22 DIO22 Toggles bit 22 RW 0
21 DIO21 Toggles bit 21 RW 0
20 DIO20 Toggles bit 20 RW 0
19 DIO19 Toggles bit 19 RW 0
18 DIO18 Toggles bit 18 RW 0
17 DIO17 Toggles bit 17 RW 0
16 DIO16 Toggles bit 16 RW 0
15 DIO15 Toggles bit 15 RW 0
14 DIO14 Toggles bit 14 RW 0
13 DIO13 Toggles bit 13 RW 0
12 DIO12 Toggles bit 12 RW 0
11 DIO11 Toggles bit 11 RW 0
10 DIO10 Toggles bit 10 RW 0
9 DIO9 Toggles bit 9 RW 0
8 DIO8 Toggles bit 8 RW 0
7 DIO7 Toggles bit 7 RW 0
6 DIO6 Toggles bit 6 RW 0
5 DIO5 Toggles bit 5 RW 0
4 DIO4 Toggles bit 4 RW 0
3 DIO3 Toggles bit 3 RW 0
2 DIO2 Toggles bit 2 RW 0
1 DIO1 Toggles bit 1 RW 0
0 DIO0 Toggles bit 0 RW 0

TOP:GPIO:DIN31_0

Address Offset 0x0000 00C0
Physical Address 0x4002 20C0 Instance 0x4002 20C0
Description Data Input from DIO 0 to 31
Type RO
Bits Field Name Description Type Reset
31 DIO31 Data input from DIO 31 RO 0
30 DIO30 Data input from DIO 30 RO 0
29 DIO29 Data input from DIO 29 RO 0
28 DIO28 Data input from DIO 28 RO 0
27 DIO27 Data input from DIO 27 RO 0
26 DIO26 Data input from DIO 26 RO 0
25 DIO25 Data input from DIO 25 RO 0
24 DIO24 Data input from DIO 24 RO 0
23 DIO23 Data input from DIO 23 RO 0
22 DIO22 Data input from DIO 22 RO 0
21 DIO21 Data input from DIO 21 RO 0
20 DIO20 Data input from DIO 20 RO 0
19 DIO19 Data input from DIO 19 RO 0
18 DIO18 Data input from DIO 18 RO 0
17 DIO17 Data input from DIO 17 RO 0
16 DIO16 Data input from DIO 16 RO 0
15 DIO15 Data input from DIO 15 RO 0
14 DIO14 Data input from DIO 14 RO 0
13 DIO13 Data input from DIO 13 RO 0
12 DIO12 Data input from DIO 12 RO 0
11 DIO11 Data input from DIO 11 RO 0
10 DIO10 Data input from DIO 10 RO 0
9 DIO9 Data input from DIO 9 RO 0
8 DIO8 Data input from DIO 8 RO 0
7 DIO7 Data input from DIO 7 RO 0
6 DIO6 Data input from DIO 6 RO 0
5 DIO5 Data input from DIO 5 RO 0
4 DIO4 Data input from DIO 4 RO 0
3 DIO3 Data input from DIO 3 RO 0
2 DIO2 Data input from DIO 2 RO 0
1 DIO1 Data input from DIO 1 RO 0
0 DIO0 Data input from DIO 0 RO 0

TOP:GPIO:DOE31_0

Address Offset 0x0000 00D0
Physical Address 0x4002 20D0 Instance 0x4002 20D0
Description Data Output Enable for DIO 0 to 31
Type RW
Bits Field Name Description Type Reset
31 DIO31 Data output enable for DIO 31 RW 0
30 DIO30 Data output enable for DIO 30 RW 0
29 DIO29 Data output enable for DIO 29 RW 0
28 DIO28 Data output enable for DIO 28 RW 0
27 DIO27 Data output enable for DIO 27 RW 0
26 DIO26 Data output enable for DIO 26 RW 0
25 DIO25 Data output enable for DIO 25 RW 0
24 DIO24 Data output enable for DIO 24 RW 0
23 DIO23 Data output enable for DIO 23 RW 0
22 DIO22 Data output enable for DIO 22 RW 0
21 DIO21 Data output enable for DIO 21 RW 0
20 DIO20 Data output enable for DIO 20 RW 0
19 DIO19 Data output enable for DIO 19 RW 0
18 DIO18 Data output enable for DIO 18 RW 0
17 DIO17 Data output enable for DIO 17 RW 0
16 DIO16 Data output enable for DIO 16 RW 0
15 DIO15 Data output enable for DIO 15 RW 0
14 DIO14 Data output enable for DIO 14 RW 0
13 DIO13 Data output enable for DIO 13 RW 0
12 DIO12 Data output enable for DIO 12 RW 0
11 DIO11 Data output enable for DIO 11 RW 0
10 DIO10 Data output enable for DIO 10 RW 0
9 DIO9 Data output enable for DIO 9 RW 0
8 DIO8 Data output enable for DIO 8 RW 0
7 DIO7 Data output enable for DIO 7 RW 0
6 DIO6 Data output enable for DIO 6 RW 0
5 DIO5 Data output enable for DIO 5 RW 0
4 DIO4 Data output enable for DIO 4 RW 0
3 DIO3 Data output enable for DIO 3 RW 0
2 DIO2 Data output enable for DIO 2 RW 0
1 DIO1 Data output enable for DIO 1 RW 0
0 DIO0 Data output enable for DIO 0 RW 0

TOP:GPIO:EVFLAGS31_0

Address Offset 0x0000 00E0
Physical Address 0x4002 20E0 Instance 0x4002 20E0
Description Event Register for DIO 0 to 31

Reading this registers will return 1 for triggered event and 0 for non-triggered events.
Writing a 1 to a bit field will clear the event.

The configuration of events is done inside MCU IOC, e.g. events for DIO #0 is configured in IOC:IOCFG0.EDGE_DET and IOC:IOCFG0.EDGE_IRQ_EN.
Type RW
Bits Field Name Description Type Reset
31 DIO31 Event for DIO 31 RW 0
30 DIO30 Event for DIO 30 RW 0
29 DIO29 Event for DIO 29 RW 0
28 DIO28 Event for DIO 28 RW 0
27 DIO27 Event for DIO 27 RW 0
26 DIO26 Event for DIO 26 RW 0
25 DIO25 Event for DIO 25 RW 0
24 DIO24 Event for DIO 24 RW 0
23 DIO23 Event for DIO 23 RW 0
22 DIO22 Event for DIO 22 RW 0
21 DIO21 Event for DIO 21 RW 0
20 DIO20 Event for DIO 20 RW 0
19 DIO19 Event for DIO 19 RW 0
18 DIO18 Event for DIO 18 RW 0
17 DIO17 Event for DIO 17 RW 0
16 DIO16 Event for DIO 16 RW 0
15 DIO15 Event for DIO 15 RW 0
14 DIO14 Event for DIO 14 RW 0
13 DIO13 Event for DIO 13 RW 0
12 DIO12 Event for DIO 12 RW 0
11 DIO11 Event for DIO 11 RW 0
10 DIO10 Event for DIO 10 RW 0
9 DIO9 Event for DIO 9 RW 0
8 DIO8 Event for DIO 8 RW 0
7 DIO7 Event for DIO 7 RW 0
6 DIO6 Event for DIO 6 RW 0
5 DIO5 Event for DIO 5 RW 0
4 DIO4 Event for DIO 4 RW 0
3 DIO3 Event for DIO 3 RW 0
2 DIO2 Event for DIO 2 RW 0
1 DIO1 Event for DIO 1 RW 0
0 DIO0 Event for DIO 0 RW 0