AON_RTC

Instance: AON_RTC
Component: AON_RTC
Base address: 0x40092000


This component control the Real Time Clock residing in AON

Note: This module is only supporting 32 bit ReadWrite access.

TOP:AON_RTC Register Summary

Register Name

Type

Register Width (Bits)

Register Reset

Address Offset

Physical Address

CTL

RW

32

0x0000 0000

0x0000 0000

0x4009 2000

EVFLAGS

RW

32

0x0000 0000

0x0000 0004

0x4009 2004

SEC

RW

32

0x0000 0000

0x0000 0008

0x4009 2008

SUBSEC

RW

32

0x0000 0000

0x0000 000C

0x4009 200C

SUBSECINC

RO

32

0x0080 0000

0x0000 0010

0x4009 2010

CHCTL

RW

32

0x0000 0000

0x0000 0014

0x4009 2014

CH0CMP

RW

32

0x0000 0000

0x0000 0018

0x4009 2018

CH1CMP

RW

32

0x0000 0000

0x0000 001C

0x4009 201C

CH2CMP

RW

32

0x0000 0000

0x0000 0020

0x4009 2020

CH2CMPINC

RW

32

0x0000 0000

0x0000 0024

0x4009 2024

CH1CAPT

RO

32

0x0000 0000

0x0000 0028

0x4009 2028

SYNC

RW

32

0x0000 0000

0x0000 002C

0x4009 202C

TOP:AON_RTC Register Descriptions

TOP:AON_RTC:CTL

Address Offset 0x0000 0000
Physical Address 0x4009 2000 Instance 0x4009 2000
Description Control

This register contains various bitfields for configuration of RTC
Type RW
Bits Field Name Description Type Reset
31:19 RESERVED19 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b0 0000 0000 0000
18:16 COMB_EV_MASK Eventmask selecting which delayed events that form the combined event.
Value ENUM Name Description
0x0 NONE No event is selected for combined event.
0x1 CH0 Use Channel 0 delayed event in combined event
0x2 CH1 Use Channel 1 delayed event in combined event
0x4 CH2 Use Channel 2 delayed event in combined event
RW 0b000
15:12 RESERVED12 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0
11:8 EV_DELAY Number of SCLK_LF clock cycles waited before generating delayed events. (Common setting for all RTC cannels) the delayed event is delayed
Value ENUM Name Description
0x0 D0 No delay on delayed event
0x1 D1 Delay by 1 clock cycles
0x2 D2 Delay by 2 clock cycles
0x3 D4 Delay by 4 clock cycles
0x4 D8 Delay by 8 clock cycles
0x5 D16 Delay by 16 clock cycles
0x6 D32 Delay by 32 clock cycles
0x7 D48 Delay by 48 clock cycles
0x8 D64 Delay by 64 clock cycles
0x9 D80 Delay by 80 clock cycles
0xA D96 Delay by 96 clock cycles
0xB D112 Delay by 112 clock cycles
0xC D128 Delay by 128 clock cycles
0xD D144 Delay by 144 clock cycles
RW 0x0
7 RESET RTC Counter reset.

Writing 1 to this bit will reset the RTC counter.

This bit is cleared when reset takes effect
WO 0
6:3 RESERVED3 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0
2 RTC_4KHZ_EN RTC_4KHZ is a 4 KHz reference output, tapped from SUBSEC.VALUE bit 19 which is used by AUX timer.

0: RTC_4KHZ signal is forced to 0
1: RTC_4KHZ is enabled ( provied that RTC is enabled EN)
RW 0
1 RTC_UPD_EN RTC_UPD is a 16 KHz signal used to sync up the radio timer. The 16 Khz is SCLK_LF divided by 2

0: RTC_UPD signal is forced to 0
1: RTC_UPD signal is toggling @16 kHz
RW 0
0 EN Enable RTC counter

0: Halted (frozen)
1: Running
RW 0

TOP:AON_RTC:EVFLAGS

Address Offset 0x0000 0004
Physical Address 0x4009 2004 Instance 0x4009 2004
Description Event Flags, RTC Status

This register contains event flags from the 3 RTC channels. Each flag will be cleared when writing a '1' to the corresponding bitfield.
Type RW
Bits Field Name Description Type Reset
31:17 RESERVED17 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000
16 CH2 Channel 2 event flag, set when CHCTL.CH2_EN = 1 and the RTC value matches or passes the CH2CMP value.

An event will be scheduled to occur as soon as possible when writing to CH2CMP provided that the channel is enabled and the new value matches any time between next RTC value and 1 second in the past

Writing 1 clears this flag. Note that a new event can not occur on this channel in first 2 SCLK_LF cycles after a clearance.

AUX_SCE can read the flag through AUX_WUC:WUEVFLAGS.AON_RTC_CH2 and clear it using AUX_WUC:WUEVCLR.AON_RTC_CH2.
RW 0
15:9 RESERVED9 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
8 CH1 Channel 1 event flag, set when CHCTL.CH1_EN = 1 and one of the following:
- CHCTL.CH1_CAPT_EN = 0 and the RTC value matches or passes the CH1CMP value.
- CHCTL.CH1_CAPT_EN = 1 and capture occurs.

An event will be scheduled to occur as soon as possible when writing to CH1CMP provided that the channel is enabled, in compare mode and the new value matches any time between next RTC value and 1 second in the past.

Writing 1 clears this flag. Note that a new event can not occur on this channel in first 2 SCLK_LF cycles after a clearance.
RW 0
7:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
0 CH0 Channel 0 event flag, set when CHCTL.CH0_EN = 1 and the RTC value matches or passes the CH0CMP value.

An event will be scheduled to occur as soon as possible when writing to CH0CMP provided that the channels is enabled and the new value matches any time between next RTC value and 1 second in the past.

Writing 1 clears this flag. Note that a new event can not occur on this channel in first 2 SCLK_LF cycles after a clearance.
RW 0

TOP:AON_RTC:SEC

Address Offset 0x0000 0008
Physical Address 0x4009 2008 Instance 0x4009 2008
Description Second Counter Value, Integer Part
Type RW
Bits Field Name Description Type Reset
31:0 VALUE Unsigned integer representing Real Time Clock in seconds.

When reading this register the content of SUBSEC.VALUE is simultaneously latched. A consistent reading of the combined Real Time Clock can be obtained by first reading this register, then reading SUBSEC register.
RW 0x0000 0000

TOP:AON_RTC:SUBSEC

Address Offset 0x0000 000C
Physical Address 0x4009 200C Instance 0x4009 200C
Description Second Counter Value, Fractional Part
Type RW
Bits Field Name Description Type Reset
31:0 VALUE Unsigned integer representing Real Time Clock in fractions of a second (VALUE/2^32 seconds) at the time when SEC register was read.

Examples :
- 0x0000_0000 = 0.0 sec
- 0x4000_0000 = 0.25 sec
- 0x8000_0000 = 0.5 sec
- 0xC000_0000 = 0.75 sec
RW 0x0000 0000

TOP:AON_RTC:SUBSECINC

Address Offset 0x0000 0010
Physical Address 0x4009 2010 Instance 0x4009 2010
Description Subseconds Increment
Value added to SUBSEC.VALUE on every SCLK_LFclock cycle.
Type RO
Bits Field Name Description Type Reset
31:24 RESERVED24 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x00
23:0 VALUEINC This value compensates for a SCLK_LF clock which has an offset from 32768 Hz.

The compensation value can be found as 2^38 / freq, where freq is SCLK_LF clock frequency in Hertz

This value is added to SUBSEC.VALUE on every cycle, and carry of this is added to SEC.VALUE. To perform the addition, bits [23:6] are aligned with SUBSEC.VALUE bits [17:0]. The remaining bits [5:0] are accumulated in a hidden 6-bit register that generates a carry into the above mentioned addition on overflow.
The default value corresponds to incrementing by precisely 1/32768 of a second.

NOTE: This register is read only. Modification of the register value must be done using registers AUX_WUC:RTCSUBSECINC1 , AUX_WUC:RTCSUBSECINC0 and AUX_WUC:RTCSUBSECINCCTL
RO 0x80 0000

TOP:AON_RTC:CHCTL

Address Offset 0x0000 0014
Physical Address 0x4009 2014 Instance 0x4009 2014
Description Channel Configuration
Type RW
Bits Field Name Description Type Reset
31:19 RESERVED19 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b0 0000 0000 0000
18 CH2_CONT_EN Set to enable continuous operation of Channel 2 RW 0
17 RESERVED17 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0
16 CH2_EN RTC Channel 2 Enable

0: Disable RTC Channel 2
1: Enable RTC Channel 2
RW 0
15:10 RESERVED10 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000
9 CH1_CAPT_EN Set Channel 1 mode

0: Compare mode (default)
1: Capture mode
RW 0
8 CH1_EN RTC Channel 1 Enable

0: Disable RTC Channel 1
1: Enable RTC Channel 1
RW 0
7:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
0 CH0_EN RTC Channel 0 Enable

0: Disable RTC Channel 0
1: Enable RTC Channel 0
RW 0

TOP:AON_RTC:CH0CMP

Address Offset 0x0000 0018
Physical Address 0x4009 2018 Instance 0x4009 2018
Description Channel 0 Compare Value
Type RW
Bits Field Name Description Type Reset
31:0 VALUE RTC Channel 0 compare value.

Bit 31 to 16 represents seconds and bits 15 to 0 represents subseconds of the compare value.

The compare value is compared against SEC.VALUE (15:0) and SUBSEC.VALUE (31:16) values of the Real Time Clock register. A Cannel 0 event is generated when {SEC.VALUE(15:0),SUBSEC.VALUE (31:16)} is reaching or exciting the compare value.

Writing to this register can trigger an immediate*) event in case the new compare value matches a Real Time Clock value from 1 second in the past up till current Real Time Clock value.

Example:
To generate a compare 5.5 seconds RTC start,- set this value = 0x0005_8000

*) It can take up to 2 SCLK_LF clock cycles before event occurs due to synchronization.
RW 0x0000 0000

TOP:AON_RTC:CH1CMP

Address Offset 0x0000 001C
Physical Address 0x4009 201C Instance 0x4009 201C
Description Channel 1 Compare Value
Type RW
Bits Field Name Description Type Reset
31:0 VALUE RTC Channel 1 compare value.

Bit 31 to 16 represents seconds and bits 15 to 0 represents subseconds of the compare value.

The compare value is compared against SEC.VALUE (15:0) and SUBSEC.VALUE (31:16) values of the Real Time Clock register. A Cannel 0 event is generated when {SEC.VALUE(15:0),SUBSEC.VALUE (31:16)} is reaching or exciting the compare value.

Writing to this register can trigger an immediate*) event in case the new compare value matches a Real Time Clock value from 1 second in the past up till current Real Time Clock value.

Example:
To generate a compare 5.5 seconds RTC start,- set this value = 0x0005_8000

*) It can take up to 2 SCLK_LF clock cycles before event occurs due to synchronization.
RW 0x0000 0000

TOP:AON_RTC:CH2CMP

Address Offset 0x0000 0020
Physical Address 0x4009 2020 Instance 0x4009 2020
Description Channel 2 Compare Value
Type RW
Bits Field Name Description Type Reset
31:0 VALUE RTC Channel 2 compare value.

Bit 31 to 16 represents seconds and bits 15 to 0 represents subseconds of the compare value.

The compare value is compared against SEC.VALUE (15:0) and SUBSEC.VALUE (31:16) values of the Real Time Clock register. A Cannel 0 event is generated when {SEC.VALUE(15:0),SUBSEC.VALUE (31:16)} is reaching or exciting the compare value.

Writing to this register can trigger an immediate*) event in case the new compare value matches a Real Time Clock value from 1 second in the past up till current Real Time Clock value.

Example:
To generate a compare 5.5 seconds RTC start,- set this value = 0x0005_8000

*) It can take up to 2 SCLK_LF clock cycles before event occurs due to synchronization.
RW 0x0000 0000

TOP:AON_RTC:CH2CMPINC

Address Offset 0x0000 0024
Physical Address 0x4009 2024 Instance 0x4009 2024
Description Channel 2 Compare Value Auto-increment

This register is primarily used to generate periodical wake-up for the AUX_SCE module, through the [AUX_EVCTL.EVSTAT0.AON_RTC] event.
Type RW
Bits Field Name Description Type Reset
31:0 VALUE If CHCTL.CH2_CONT_EN is set, this value is added to CH2CMP.VALUE on every channel 2 compare event. RW 0x0000 0000

TOP:AON_RTC:CH1CAPT

Address Offset 0x0000 0028
Physical Address 0x4009 2028 Instance 0x4009 2028
Description Channel 1 Capture Value

If CHCTL.CH1_EN = 1and CHCTL.CH1_CAPT_EN = 1, capture occurs on each rising edge of the event selected in AON_EVENT:RTCSEL.
Type RO
Bits Field Name Description Type Reset
31:16 SEC Value of SEC.VALUE bits 15:0 at capture time. RO 0x0000
15:0 SUBSEC Value of SUBSEC.VALUE bits 31:16 at capture time. RO 0x0000

TOP:AON_RTC:SYNC

Address Offset 0x0000 002C
Physical Address 0x4009 202C Instance 0x4009 202C
Description AON Synchronization

This register is used for synchronizing between MCU and entire AON domain.
Type RW
Bits Field Name Description Type Reset
31:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000 0000 0000 0000 0000
0 WBUSY This register will always return 0,- however it will not return the value until there are no outstanding write requests between MCU and AON

Note: Writing to this register prior to reading will force a wait until next SCLK_LF edge. This is recommended for syncing read registers from AON when waking up from sleep
Failure to do so may result in reading AON values from prior to going to sleep
RW 0