SimpleLink™ CC13x0 SDK 1.50.00.08 Release Notes
Table of Contents
Introduction
The SimpleLink CC13x0 SDK is part of TI’s SimpleLink MCU platform, offering a single development environment that delivers flexible hardware, software and tool options for customers developing wired and wireless applications. For more information about the SimpleLink MCU platform, visit www.ti.com/simplelink.
SimpleLink™ CC13x0 Software Development Kit (SDK) is a set of software development tools that enables engineers to develop software applications on the SimpleLink™ CC13x0 ULP devices. This powerful software toolkit provides a cohesive and consistent software experience for all SimpleLink™ CC13x0 users by packaging essential software components such as TI RTOS, peripheral drivers, TI 15.4-Stack, Bluetooth Low Energy, and RF-Proprietary examples in one easy-to-use software package along with exhaustive documentation.
Documentation
What’s New
Third release of SimpleLink™ CC13x0 SDK, based on the Core-SDK version 3_30_00_13
TI 15.4 Stack
ID | Summary |
---|---|
TIMAC-1568 | Enabled broadcast mechanism in frequency hopping mode, allowing PAN Coordinator to send broadcast to the network devices |
TIMAC-1556 | TI 15.4-Stack supports the 200 Kbps data rate for beacon mode. |
SDKSYSAPPS-43 | IAR Projects for 15.4 Embedded Sensor and Collector |
TI Proprietary-RF
ID | Summary |
---|---|
SDKSYSAPPS-191 | ON-CHIP OAD Capability for EasyLink WSN examples |
SDKSYSAPPS-138 | Integrated micro-BLE to provide BLE advertisements for EasyLink WSN DM examples |
EZLINKPROP-44 | Fixed Power_idleFunc references in nortos examples |
EZLINKPROP-41 | Support 433MHz band for CC13x0 |
EZLINKPROP-29 | Added no-RTOS PER example for CC13x0 |
EZLINKPROP-25 | No-RTOS support for EasyLink on CC13x0 |
Fixed Issues
TI 15.4 Stack
ID | Summary |
---|---|
TIMAC-1581 | Fixed an issue where scan with energy Detect returns RSSIas 0xe4 instead of 0x0 for a free channel |
SDKSYSAPPS-272 | Optimized the antenna switching between sub1 GHz and 2.4GHz and fixed a power bug when using micro BLE |
SDKSYSAPPS-218 | Modified URLs of uBLE beacons to be https to work with native android BLE beacon scan. |
SDKSYSAPPS-204 | External flash was not being erased properly if OAD_BLOCK_SIZE was not a multiple of flashPageSize |
SDKSYSAPPS-168 | Fixed an issue where sensor device backoff interval in orphan mode gets reset with CONFIG_SCAN_BACKOFF instead of CONFIG_ORPHAN_BACKOFF_INTERVAL |
SDKSYSAPPS-167 | Renamed the board file in collector and sensor applications to CC13x0_LAUNCHXL.c/h |
SDKSYSAPPS-162 | Fixed the issue where sensor device could not sleep before start event and between scans |
SDKSYSAPPS-158 | Fixed an issue where Sensor application with micro BLE enabled was not going to sleep after sending BLE beacons |
SDKSYSAPPS-152 | Fixed an issue where TIREX did not show the example readme.html, only the readme.md. |
SDKSYSAPPS-131 | Updated app.cfg for TI 15.4-Stack example applications to have a similar look and feel to other SimpleLink SDK examples |
SDKSYSAPPS-2 | Fixed an issue where 15.4 Stack examples has build error when board_led.h is modified |
TI Proprietary-RF
ID | Summary |
---|---|
SDKSYSAPPS-218 | Modified URLs of uBLE beacons to be https to work with native android BLE beacon scan. |
SDKSYSAPPS-204 | External flash was not being erased properly if OAD_BLOCK_SIZE was not a multiple of flashPageSize |
EZLINKPROP-83 | Fixed PER for Interference Case |
EZLINKPROP-74 | Changed Easylink_RadioTime_to_ms macro to avoid overflow |
EZLINKPROP-38 | Changed the hard coded systemReset in NP example to the systemReset API from driverlib |
Known Issues
TI 15.4 Stack
ID | Summary |
---|---|
None | None |
TI Proprietary-RF
ID | Summary |
---|---|
EZLINKPROP-80 | EasyLink_getRfPwr has function type int_8, but may return a status (EasyLink_Status_Config_Error) |
Upgrade and Compatibility Information
This is the second release of SimpleLink™ CC13x0 SDK. If you are migrating from existing TI 15.4-Stack or Proprietary-RF examples, please review the SimpleLink™ CC13x0 SDK Migration Guide
Operating System Support
SimpleLink™ CC13x0 SDK is supported on the Microsoft Windows®, Linux Ubuntu 14.04 and macOS Sierra platform
Dependencies
SimpleLink™ CC13x0 SDK 1.50.00.08 was built & tested on a Windows 7 host platform using the following Integrated Development Environment (IDE) and components. Using an IDE version or TI-RTOS version not listed below may result in compatibility issues with this SDK release.
- Code Composer Studio: 7.3.0.00019
- IAR Embedded Workbench: 8.11.2.50
- TI-RTOS for CC13XX: 3_30_00_13
- C Compiler for ARM: 16.9.4.LTS
- XDCTools: 3.50.03.33
Device Support
Development Board Support
Versioning
This product follows a version format, M.mm.pp.bb, where:
- M is a 1 digit major number,
- mm is a 2 digit minor number,
- pp is a 2 digit patch number,
- bb is a 2 digit incrementing build counter.