TI 15.4-Stack 2.03.00.00 Release Notes
Table of Contents
Introduction
TI 15.4-Stack is an IEEE 802.15.4e/g based software stack part of the SimpleLink CC13x0 SDK that supports a Star network topology for Sub-1GHz applications. TI 15.4-Stack software runs on TI’s SimpleLink™ Sub-1GHz wireless microcontrollers, including the CC1310 and CC1350. Devices running TI 15.4-Stack offer key benefits, such as longer range in the FCC band and better protection against in-band interference through use of WiSun based frequency hopping, ability to send BLE beacons while operating on Sub1GHz TI 15.4-Stack network when using dual-band CC1350. TI 15.4-Stack provides a complete end-to-end wireless application development solution to reduce time and cost of getting your product to market quickly.
Documentation
- TI 15.4-Stack Quick Start Guide
- TI 15.4-Stack User’s Guide
- TI 15.4-Stack CoP Interface Guide
- TI 15.4 Stack APIs
- Software License
- Software Manifest
What’s New
ID | Summary |
---|---|
TIMAC-1568 | Enabled broadcast mechanism in frequency hopping mode, allowing PAN Coordinator to send broadcast to the network devices |
TIMAC-1556 | TI 15.4-Stack supports the 200 Kbps data rate for beacon mode. |
SDKSYSAPPS-43 | IAR Projects for 15.4 Embedded Sensor and Collector |
Fixed Issues
ID | Summary |
---|---|
TIMAC-1581 | Fixed an issue where scan with energy Detect returns RSSIas 0xe4 instead of 0x0 for a free channel |
SDKSYSAPPS-272 | Optimized the antenna switching between sub1 GHz and 2.4GHz and fixed a power bug when using micro BLE |
SDKSYSAPPS-218 | Modified URLs of uBLE beacons to be https to work with native android BLE beacon scan. |
SDKSYSAPPS-204 | External flash was not being erased properly if OAD_BLOCK_SIZE was not a multiple of flashPageSize |
SDKSYSAPPS-168 | Fixed an issue where sensor device backoff interval in orphan mode gets reset with CONFIG_SCAN_BACKOFF instead of CONFIG_ORPHAN_BACKOFF_INTERVAL |
SDKSYSAPPS-167 | Renamed the board file in collector and sensor applications to CC13x0_LAUNCHXL.c/h |
SDKSYSAPPS-162 | Fixed the issue where sensor device could not sleep before start event and between scans |
SDKSYSAPPS-158 | Fixed an issue where Sensor application with micro BLE enabled was not going to sleep after sending BLE beacons |
SDKSYSAPPS-152 | Fixed an issue where TIREX did not show the example readme.html, only the readme.md. |
SDKSYSAPPS-131 | Updated app.cfg for TI 15.4-Stack example applications to have a similar look and feel to other SimpleLink SDK examples |
SDKSYSAPPS-2 | Fixed an issue where 15.4 Stack examples has build error when board_led.h is modified |
Known Issues
ID | Summary |
---|---|
None | None |
Upgrade and Compatibility Information
Operating System Support
The TI 15.4-Stack SDK is supported on the Microsoft Windows® platform.
Dependencies
TI 15.4-Stack 2.03.00.00 was built & tested on a Windows 7 host platform using the following Integrated Development Environment (IDE) and components. Using an IDE version or TI-RTOS version not listed below may result in compatibility issues with this SDK release.
- Code Composer Studio: 7.3.0.00019
- IAR Embedded Workbench: 8.11.2.50
- TI-RTOS for CC13XX: 3_30_00_13
- C Compiler for ARM: 16.9.4.LTS
- XDCTools: 3.50.03.33
Device Support
Development Board Support
Validation
TI 15.4-Stack 2.03.00.00 was tested using the following components:
- TI-RTOS for CC13XX: 3_30_00_13
- C Compiler for ARM: 16.9.4.LTS
- XDCTools: 3.50.03.33
- CC1310 LaunchPad
- CC1350 LaunchPad
Versioning
This product follows a version format, M.mm.pp.bb, where:
- M is a 1 digit major number,
- mm is a 2 digit minor number,
- pp is a 2 digit patch number,
- bb is a 2 digit incrementing build counter.