rfWsnNodeDmOad_internalFlash Example
Example Summary
The WSN Node example illustrates how to create a Dual Mode Wireless Sensor Network Node device which sends sensor data to a Sub-1GHz concentrator and also send out BLE beacons. The BLE beacons can be picked up by any BLE capable device. This example is meant to be used together with the WSN Dual Mode Concentrator example.
This examples showcases the use of several Tasks, Semaphores and Events to get sensor updates and send packets with acknowledgement from the concentrator. For the radio layer, this example uses the EasyLink API which provides an easy-to-use API for the most frequently used radio operations.
Peripherals Exercised
Board_PIN_LED1
- Toggled when Sub1-GHz data is sent over the RF interface.Board_PIN_LED2
- Toggled when a BLE beacon is sent over the RF interface.Board_PIN_BUTTON0
- Selects fast report or slow report mode. In slow report mode the sensor data is sent at least every 5s or as fast as every 1s if there is a significant change in the ADC reading. In fast reporting mode the sensor data is sent every 1s regardles of the change in ADC value. The default is slow reporting mode.Board_PIN_BUTTON1
- Selects the BLE beacon type used;- Manufacturer Specific (MS) + Eddystone URL. This is the default.
- MS
- Eddystone URL + TLM
- Eddystone UID + TLM
None
Resources & Jumper Settings
If you’re using an IDE (such as CCS or IAR), please refer to Board.html in your project directory for resources used and board-specific jumper settings. Otherwise, you can find Board.html in the directory <SDK_INSTALL_DIR>/source/ti/boards/<BOARD>.
Fields left blank have no specific settings for this example.
Example Usage
Run the example. On another board run the WSN Dual Mode Concentrator example. This node should show up on the LCD/UART of the Concentrator. To create a sub-1GHz only device, without the capability to send BLE beacon, one can use the Wireless Sensor Network examples also.
The example also support Over The Air Update (OAD), where new FW can be loaded over OAD. The must be an OAD Server, which is included in the concentrator, and an OAD client which is included in the sensor.
Generating the required binary images
For generating the images the following tools are required:
CCSv7
https://processors.wiki.ti.com/index.php/Download_CCSsimplelink_cc13x0_sdk_1_31_00_xx
https://www.ti.com/tool/simplelink-cc13x0-sdkPython 2.7
Python intelhex-2.1
Python crcmod-1.7
The prebuilt BIM binary is generated from the BLE SDK projects:
- CCS:
<SDK_DIR>\examples\rtos\CC1350_LAUNCHXL\blestack\util\bim_extflash\tirtos\ccs
- IAR:
<SDK_DIR>\examples\rtos\CC1350_LAUNCHXL\blestack\util\bim_extflash\tirtos\iar
The python intelhex merge utility is used to combine the BIM and App into one hex file that can be downloaded with SmartRF Studio:
cd <SDK_DIR>/examples/rtos/CC1310_LAUNCHXL/easylink/hexfiles/oad
python /usr/bin/hexmerge.py -o rfWsnNodeOad_CC1310LP_all.hex "--overlap=error" rfWsnNodeOad_CC1310LP_app.hex bim_extflash_cc1350lp_bim.hex
An OAD image can then be created from the application image with the oad_image_tool.py:
python ../../../../../../tools/easylink/oad_image_tool.py -v 0x[major version:minor version] -i app rfWsnNodeOad_CC1310LP_app.hex -ob rfWsnNodeOad_CC1310LP_app.bin -m 0x1000
Where major version (XX) and minor version (YY) must be of the format 0xXXYY, for example 2.3 would be 0x0203.
Using the OAD example
To be safe when using for the first time the external flash of the Concentrator and the Node should be wiped. Program both LP boards with bin/CC1350LaunchPad_ExtFlashErase.hex. The program will flash the LED’s while erasing and once finished the LED’s will stop flashing. Allow the application to run until the external flash has been erased and the LED’s stop flashing.
The wipe flash FW can be found in below lacation and should be downloaded with Uniflash programmer: <SDK_DIR>/hexfiles/native_oad/CC1350LaunchPad_ExtFlashErase.hex
The Concetrator OAD Server and Node OAD Client FW must then be loaded in to the LP’s using the Uniflash programmer:
- Load
\examples\rtos\CC1310_LAUNCHXL\easylink\hexfiles\oad\rfWsnConcentratorOad_CC1310LP_all.hex into a CC1310LP/CC1350LP - Load
\examples\rtos\CC1310_LAUNCHXL\easylink\hexfiles\oad\rfWsnNodeOad_CC1310LP_all.hex into a CC1310LP/CC1350LP
The Concetrator will display the below on the UART terminal:
Nodes Value SW RSSI
0x0b 0887 0 -080
0xdb 1036 0 -079
0x91 0940 0 -079
*Action: Update available FW
Info: Available FW unknown
cmd:
The node OAD image can be loaded into the external flash of the Concentrator over the UART with the oad_wrtie_bin.py script. The action must first be selected using BTN-2. Press BTN-2 until the Action is set to Update available FW
, then Press BTN-1 and Press BTN-2 to execute the action.
When “Available FW” is selected and BTN-2 is pressed the terminal will display:
Waiting for Node FW update...
The UART terminal must first be closed to free the com port. Then the python script run:
python ../../../../../../tools/easylink/oad/oad_wrtie_bin.py /dev/ttyS28 rfWsnNodeOad_CC1310LP_app.bin
After the download the UART terminal can be re-opened and the “Available FW” will be updated to reflect the new FW.
The current FW version running on the node can be requested using the Send FW Ver Req
action. This is done by pressing BTN-1 until Action
is selected. Then press BTN-2 until the Action is set to Update available FW
, The Press BTN-1 until intended device is selected. Press BTN-2 to execture the action.
The next time the node sends data it will respond and the FW version will be displayed:
Nodes Value SW RSSI
0x0b 0887 0 -080
0xdb 1036 0 -079
*0x91 0940 0 -079
Action: Update available FW
Info: Node 0x91 FW v1.0
The FW running on the nodes can now be updated to the available fw on the concentrator. The Action
must first be selected using BTN-1. The Press BTN-2 until the Action is set to Update node FW
, and Press BTN-1 until the intended device is selected. Press BTN-2 to execture the action.
The next time the node sends data it will respond and the FW update request and start requesting OAD blocks, which will be displayed:
Nodes Value SW RSSI
0x0b 0887 0 -080
0xdb 1036 0 -079
*0x91 0940 0 -079
Action: Update available FW
Info: OAD Block 14 of 1089
Once the OAD has completed the node will reset (if not yo may need to do a manual reset).
Building an OAD hex
The following steps talk through how to use CCS or IAR to create an OAD hex file which can be used to create the OAD biniaries as described in previous sections
Building the hex file in CCS
- Import the CCS porject into CCS(for more information conslt the Examples Users Guide in the proprietary-rf documentation)
- Exclude the ccfg.c file from the project.
- Enable hex file conversion in Project->Properties Arm Hex Utility
- Set memory width to 8 in General options
- Set output format to intel hex.
- Make a code change, for testing this can just be updating the nodeFwVersion string in NodeTask.c
- build
- copy hex from the projects Debug dir to the bin folder
Building the hex file in IAR
- Create a new IAR workspace
- Creae a new Empty IAR projectect and save it as rfWsnNodeOad
- Select Project -> “Add Project Connection” and add C:\ti\simplelink_cc13x0_sdk_1_xx_xx_xx\examples\rtos\CC1350_LAUNCHXL\easylink\rfWsnDmNodeOad\tirtos\iar\rfWsnDmNodeOad.ipcf
- Remove the ccfg.c file from the project.
- Enable hex file conversion in Project->Option Arm Hex Output Converter
- Check “Generate additional output”
- Set output format to Intel Extended hex.
- Make a code change, for testing this can just be updating the nodeFwVersion string in NodeTask.c
- build
- copy hex from the projects Debug dir to the bin folder
Building the hex file in CCS
- Import the GCC porject into CCS (for more information conslt the Examples Users Guide in the proprietary-rf documentation)
- Exclude the ccfg.c file from the project.
- Enable hex file conversion in Project->GNU Objcopy Utility
- In Edit flags add the following:
-O ihex --remove-section .vtable --remove-section .dmaSpi0RxControlTableEntry --remove-section .dmaSpi0TxControlTableEntry --remove-section .dmaSpi1RxControlTableEntry --remove-section .dmaSpi1TxControlTableEntry --gap-fill 0xff
- Make a code change, for testing this can just be updating the nodeFwVersion string in NodeTask.c
- Build
- copy hex from the projects Debug dir to the bin folder
Application Design Details
This examples consists of two tasks, one application task and one radio protocol task. It also consists of an Sensor Controller Engine (SCE) task which samples the ADC once per second.
On initialisation the CM3 application sets the minimum report interval and the minimum change value which is used by the SCE task to wake up the CM3. The ADC task on the SCE checks the ADC value once per second. If the ADC value has changed by the minimum change amount since the last time it notified the CM3, it wakes it up again. If the change is less than the masked value, then it does not wake up the CM3 unless the minimum report interval time has expired.
The NodeTask waits to be woken up by the SCE. When it wakes up it toggles
Board_PIN_LED1
and sends the new ADC value to the NodeRadioTask. Then it sends out sensor data on the sub-1GHz RF interface and if configured to do so it will also send a BLE Beacon. The sensor data is; ADC value, battery level, time since last reboot, number of packets sent and the button state.The NodeRadioTask handles the radio protocol. This sets up the EasyLink API and uses it to send new ADC values to the concentrator. After each sent packet it waits for an ACK packet back. If it does not get one, then it retries three times. If it did not receive an ACK by then, then it gives up.
RadioProtocol.h can also be used to change the PHY settings to be either the default IEEE 802.15.4g 50kbit, Long Range Mode or custom settings. In the case of custom settings, the smartrf_settings.c file is used. This can be changed either by exporting from Smart RF Studio or directly in the file.
For SensorTags there is a pin conflict, so either the DEVPACK-DEBUG or the DEVPACK-WATCH must be used and
BOARD_DISPLAY_EXCLUDE_UART
must be added to the global precompiler defines in order to use LCD.
For IAR users using any SensorTag(STK) Board, the XDS110 debugger must be selected with the 4-wire JTAG connection within your projects’ debugger configuration.
References
- For more information on the EasyLink API and usage refer to SimpleLink-EasyLink.