rfWsnConcentratorOad Example
Example Summary
The WSN Concentrator example illustrates how to create a simple Wireless Sensor Network Concentrator device which listens for packets from other nodes. This example is meant to be used together with the WSN Node example to form a one- to-many network where the nodes send messages to the concentrator.
This examples showcases the use of several Tasks, Semaphores and Events to receive packets, send acknowledgements and display the received data on the LCD. For the radio layer, this example uses the EasyLink API which provides an easy-to-use API for the most frequently used radio operations.
Refer to EasyLink API for more information on the EasyLink API.
Peripherals Exercised
Board_PIN_LED0
- Toggled when data is received over the RF interface
Resources & Jumper Settings
If you’re using an IDE (such as CCS or IAR), please refer to Board.html in your project directory for resources used and board-specific jumper settings. Otherwise, you can find Board.html in the directory <SDK_INSTALL_DIR>/source/ti/boards/<BOARD>.
Example Usage
Run the example. On another board (or several boards) run the WSN Node example. The LCD will show the discovered node(s). When the collector receives data from a new node, it is given a new row on the display and the received value is shown. If more than 7 nodes are detected, the device list rolls over, overriding the first. Whenever an updated value is received from a node, it is updated on the LCD display.
The example also support Over The Air Update (OAD), where new FW can be loaded over OAD. The must be an OAD Server, which is included in the concentrator, and an OAD client which is included in the sensor.
Generating the required binary images
For generating the images the following tools are required:
CCSv7
https://processors.wiki.ti.com/index.php/Download_CCSsimplelink_cc13x0_sdk_1_31_00_xx
https://www.ti.com/tool/simplelink-cc13x0-sdkPython 2.7
Python intelhex-2.1
Python crcmod-1.7
The prebuilt BIM binary is generated from the BLE SDK projects:
- CCS:
<SDK_DIR>\examples\rtos\CC1350_LAUNCHXL\blestack\util\bim_extflash\tirtos\ccs
- IAR:
<SDK_DIR>\examples\rtos\CC1350_LAUNCHXL\blestack\util\bim_extflash\tirtos\iar
The python intelhex merge utility is used to combine the BIM and App into one hex file that can be downloaded with SmartRF Studio:
cd <SDK_DIR>/examples/rtos/CC1310_LAUNCHXL/easylink/hexfiles/oad/<int_flash/ext_flash>/
python /usr/bin/hexmerge.py -o rfWsnNodeOad_CC1310LP_all.hex "--overlap=error" rfWsnNodeOad_CC1310LP_app.hex bim_extflash_cc1350lp_bim.hex
Note: Select the relevant int_flash/ext_flash files.
An OAD image can then be created from the application image with the oad_image_tool.py:
python ../../../../../../tools/easylink/oad_image_tool.py -v 0x[major version:minor version] -i app rfWsnNodeOad_CC1310LP_app.hex -ob rfWsnNodeOad_CC1310LP_app.bin -m 0x1000
Where major version (XX) and minor version (YY) must be of the format 0xXXYY, for example 2.3 would be 0x0203.
Using the OAD example
To be safe when using for the first time the external flash of the Concentrator and the Node should be wiped. Program both LP boards with bin/CC1350LaunchPad_ExtFlashErase.hex. The program will flash the LED’s while erasing and once finished the LED’s will stop flashing. Allow the application to run until the external flash has been erased and the LED’s stop flashing.
The wipe flash FW can be found in below location and should be downloaded with Uniflash programmer: <SDK_DIR>/hexfiles/native_oad/CC1350LaunchPad_ExtFlashErase.hex
The Concentrator OAD Server and Node OAD Client FW must then be loaded in to the LP’s using the Uniflash programmer:
- Load
\examples\rtos\CC1310_LAUNCHXL\easylink\hexfiles\oad\rfWsnConcentratorOad_CC1310LP_all.hex into a CC1310LP/CC1350LP - Load
\examples\rtos\CC1310_LAUNCHXL\easylink\hexfiles\oad\rfWsnNodeOad_CC1310LP_all.hex into a CC1310LP/CC1350LP
The Concetrator will display the below on the UART terminal:
Nodes Value SW RSSI
0x0b 0887 0 -080
0xdb 1036 0 -079
0x91 0940 0 -079
*Action: Update available FW
Info: Available FW unknown
cmd:
The node OAD image can be loaded into the external flash of the Concentrator over the UART with the oad_wrtie_bin.py script. The action must first be selected using BTN-2. Press BTN-2 until the Action is set to Update available FW
, then Press BTN-1 and Press BTN-2 to execute the action.
When “Available FW” is selected and BTN-2 is pressed the terminal will display:
Waiting for Node FW update...
The UART terminal must first be closed to free the com port. Then the python script run:
python ../../../../../../tools/easylink/oad/oad_wrtie_bin.py /dev/ttyS28 rfWsnNodeOad_CC1310LP_app.bin
After the download the UART terminal can be re-opened and the “Available FW” will be updated to reflect the new FW.
The current FW version running on the node can be requested using the Send FW Ver Req
action. This is done by pressing BTN-1 until Action
is selected. Then press BTN-2 until the Action is set to Update available FW
, The Press BTN-1 until intended device is selected. Press BTN-2 to execute the action.
The next time the node sends data it will respond and the FW version will be displayed:
Nodes Value SW RSSI
0x0b 0887 0 -080
0xdb 1036 0 -079
*0x91 0940 0 -079
Action: Update available FW
Info: Node 0x91 FW v1.0
The FW running on the nodes can now be updated to the available fw on the concentrator. The Action
must first be selected using BTN-1. The Press BTN-2 until the Action is set to Update node FW
, and Press BTN-1 until the intended device is selected. Press BTN-2 to execture the action.
The next time the node sends data it will respond and the FW update request and start requesting OAD blocks, which will be displayed:
Nodes Value SW RSSI
0x0b 0887 0 -080
0xdb 1036 0 -079
*0x91 0940 0 -079
Action: Update available FW
Info: OAD Block 14 of 1089
Once the OAD has completed the node will reset (if not yo may need to do a manual reset).
Building an OAD hex
The following steps talk through how to use CCS or IAR to create an OAD hex file which can be used to create the OAD binaries as described in previous sections
Building the hex file in CCS
- Import the CCS porject into CCS(for more information consult the Examples Users Guide in the proprietary-rf documentation)
- Exclude the ccfg.c file from the project.
- Enable hex file conversion in Project->Properties Arm Hex Utility
- Set memory width to 8 in General options
- Set output format to intel hex.
- Make a code change, for testing this can just be updating the nodeFwVersion string in NodeTask.c
- build
- copy hex from the projects Debug dir to the bin folder
Building the hex file in IAR
- Create a new IAR workspace
- Creae a new Empty IAR project and save it as rfWsnNodeOad
- Select Project -> “Add Project Connection” and add C:\ti\simplelink_cc13x0_sdk_1_xx_xx_xx\examples\rtos\CC1350_LAUNCHXL\easylink\rfWsn
NodeOadClient\tirtos\iar\rfWsn NodeOadClient.ipcf - Remove the ccfg.c file from the project.
- Enable hex file conversion in Project->Option Arm Hex Output Converter
- Check “Generate additional output”
- Set output format to Intel Extended hex.
- Make a code change, for testing this can just be updating the nodeFwVersion string in NodeTask.c
- build
- copy hex from the projects Debug dir to the bin folder
Building the hex file in CCS
- Import the GCC project into CCS (for more information consult the Examples Users Guide in the proprietary-rf documentation)
- Exclude the ccfg.c file from the project.
- Enable hex file conversion in Project->GNU Objcopy Utility
- In Edit flags add the following:
-O ihex --remove-section .vtable --remove-section .dmaSpi0RxControlTableEntry --remove-section .dmaSpi0TxControlTableEntry --remove-section .dmaSpi1RxControlTableEntry --remove-section .dmaSpi1TxControlTableEntry --gap-fill 0xff
- Make a code change, for testing this can just be updating the nodeFwVersion string in NodeTask.c
- Build
- copy hex from the projects Debug dir to the bin folder
Application Design Details
This examples consists of two tasks, one application task and one radio protocol task.
The ConcentratorRadioTask handles the radio protocol. This sets up the EasyLink API and uses it to always wait for packets on a set frequency. When it receives a valid packet, it sends an ACK and then forwards it to the ConcentratorTask.
The ConentratorTask receives packets from the ConcentratorRadioTask, displays the data on the LCD and toggles Board_PIN_LED0.
RadioProtocol.h can also be used to change the PHY settings to be either the default IEEE 802.15.4g 50kbit, Long Range Mode or custom settings. In the case of custom settings, the smartrf_settings.c file is used. This can be changed either by exporting from Smart RF Studio or directly in the file.
Note for IAR users: When using the CC1310DK, the TI XDS110v3 USB Emulator must be selected. For the CC1310_LAUNCHXL, select TI XDS110 Emulator. In both cases, select the cJTAG interface.