Introduction

Z-Stack 3.10 is a plugin for the SimpleLink™ CC26x2 SDK, which contains the supported software for the CC26x2R1. Z-Stack is based on ZigBee® which is based on the IEEE™ 802.15.4 specification with the added benefit of running on top of TI-RTOS. Please refer to the Z-Stack Overview section for more information about the Z-Stack implementation. The SimpleLink™ CC26x2R1 SDK supports a Zigbee solution, delivered as plugin, which runs on the SimpleLink MCU framework (TI-RTOS, CCS / CCS Cloud). The Zigbee plugin contains everything needed for a Zigbee compliant solution, including tools, application examples, documentation, and source code. It also includes a Zigbee Pro compliant Zigbee stack, as well as Green Power device and sink support. Example applications include door lock, light, switch, temperature sensor and thermostat. Sample applications are zigbee certification-ready.

The Z-Stack plugin also includes support for Zigbee Network Processor configuration, which can be used in two chip architectures where the host implements the Cluster Library and the Zigbee applications.

../_images/intro-example-apps.png

Figure 1. Examples of Zigbee end product applications.

Zigbee is a standards-based technology for remote monitoring, control and sensor network applications. The standard was created to address the need for a cost-effective, standards-based wireless networking solution that supports low data-rates, low-power consumption, security, and reliability. With its support of self-healing mesh networking, Zigbee is a decentralized network topology very similar to the Internet. It allows nodes to find new routes throughout the network if one route fails, making it a robust wireless solution.

A technology specifically targeted for wireless sensor networks, Zigbee can be used in any monitoring and control application that requires a wireless link. The primary target markets are: - Home, building and industrial automation - Smart wireless lighting control - Home control and security - Medical and patient monitoring - Logistics and asset tracking - Sensor networks and active RFID - Advanced metering amd smart energy - Commercial building automation - Energy harvesting

For more information, please visit the Zigbee Alliance.

Note

Do not use this document as a substitute for the complete specification.

Disclaimer

  • SimpleLink, TI-RTOS, Code Composer Studio, Sensor Controller Studio, SmartRF, BoosterPack are trademarks of Texas Instruments.
  • ARM, Cortex are registered trademarks of ARM Ltd.
  • Wireshark is a trademark of CACE Technologies, LLC.
  • IEEE is a trademark of International Electrical and Electronics Engineers.
  • Node.js is a registered trademark of Joyent, Inc.
  • Linux is a registered trademark of Linus Torvalds.
  • Windows is a registered trademark of Microsoft Corporation.
  • All other trademarks are the property of their respective owners.