Table of Contents
Example Summary
This example introduce the user to the easily configurable power management drivers on CC32xx devices.
Peripherals Exercised
Board_LED0
- Indicates that the board was initialized withinmain()
and while blinking, indicates that the board is trying to connect to AP.
Example Usage
Connect current measurement tool.
Remove the jumper from J12 (VBAT) and connect your current measurement tool to it.
Open the common.h file and configure your network parameters. Set values for the: SSID_NAME, SECURITY_TYPE and SECURITY_KEY defines
Build the project and flash it by using the SimpleLink Uniflash application
The example could not be executed from the debugger.
Open a serial session (e.g.
HyperTerminal
,puTTY
, etc.) to the appropriate COM port.The COM port can be determined via Device Manager in Windows or via
ls /dev/tty*
in Linux.
The connection should have the following settings
Baud-rate: 115200
Data bits: 8
Stop bits: 1
Parity: None
Flow Control: None
Run the example by pressing the reset button.
Board_LED0
turns ON to indicate TI-RTOS driver initialization is complete.The example starts by showing on the terminal the following options:
1) for Hibernate. 2) for LPDS. 3) for Transceiver Mode 4) for Intermittently Connected. 5) for Always Connected
Select the request power mode by pressing the appropriate number
- The example proceeds according to the selected mode:
Hibernate mode enters immediately to hibernate which represents the lowest power state of the device.
LPDS mode enters immediately to low power deep sleep.
Transceiver mode enters the device into the user selected state between operation times. For more details refer to the transceiver mode section under Application Design Details.
Intermittently Connected mode enters the device into hibernate state and try to establish connection with the access point between operation times.
Always Connected mode enters the device into LPDS and periodically wakes up to service beacons in order to keep connected with the access point.
Start measure current
Please refer to the expected power consumption website link (see References).
Reset the device in order to start measure again
Application Design Details
This example provides users the ability to configure the device in various low power uses cases, for the purposes of current consumption measurements. The following describes the power profiles details:
Hibernate mode enters immediately to hibernate which represents the lowest power state of the device. In this mode, all the voltage sources, like DCDC or LDOs, within the power management unit are shut off. Very few logic, which works directly on battery power, is ON and they work on 32 KHz clock.
LPDS mode enters immediately to low power deep sleep with current range (0.12mA - 0.14mA) In this mode each subsystem processor requests the clock management unit for shutting off their subsystem. When both the subsystems request for this mode, Clock management unit will turn off the PLL, 40Mhz xtal, and the power management unit will shut off the power to each subsystem and scale down the voltage of always on domain to 0.9V. Active logic in this mode will work on 32 KHz clock.
- Transceiver mode provides the user with multiple configuration options as follows:
- number of packets per channel
- packet size between 50 bytes to 1400 bytes
- delay between channels tuning in miliseconds
- wifi rate of the transmitted packet
- channels mask representing all the desired channels. Each channel is represented by an ordered bit in the mask. For example, if channels 1,6,11 are desired, the mask is 421 (represented in hexadecimal format)
- power backoff from the maximal power of the specific rate. value of 0 in dB represents full power. Values can range from 0 to 15
- cycle period in seconds
- the power level between cycles. Can be Shutdown, Hibernate or LPDS. Shutdown is using the nRESET pin of the CC3120 whereas Hibernate is using the nHIB pin of the CC3120. The user should configure the correct pin in gpioPinConfigs[] under MSP.c board file. In MSP_EXP432P401R example, nHib is GPIOMSP432_P4_1* and nRESET is GPIOMSP432_P3_6. The example should be recompiled for these changes to take effect
The configuration options are test for validity before taking effect. The socket in use in Transceiver mode is RAW hence not requires use of networking services.
Intermittently Connected mode is for devices that need to operate between long time intervals. In this mode, the device is trying to connect to the access point (Board_LED0 starts blinking) then enters hibernate state between working cycles. Almost all the device components are shut-down, hence when waking up a new connection needs to be established. In order to change the network parameters (e.g.
SSID_NAME
), open for edit the common.h file, make your changes and build. ‘NOT_ACTIVE_DURATION_MSEC’ defines the hibernate time period between 2 working cycles.Always Connected mode is trying to connect to the access point (Board_LED0 starts blinking) then enters the entire system is in LPDS with only the WLAN subsystem periodically waking up to service beacons. In order to change the network parameters (e.g.
SSID_NAME
), open for edit the common.h file, make your changes and build. ‘LSI_DURATION_IN_MSEC’ definition configures the device wake up only on every n-th beacon thus providing longer Sleep periods. minimal value is 100 milliseconds.
Please install the latest CC32xx Service Pack in order to get the most optimization and lowest current consumption.
References
- The expected power consumption numbers are described in the the following website: https://www.ti.com/product/CC3220/datasheet/specifications#SWAS031889