Table of Contents
Example Summary
This example demonstrates the functionality of the over-the-air updates of the CC31xx’s firmware file as well as the MSP432’s firmware by leveraging the device’s active Wi-Fi connection. A local web server is started that accepts a prebuilt TAR file that contains updated firmware for the MSP432 as well as any relevant user files. After submission of the TAR file, the MSP432 and CC31xx processes the file, performs a calculation and verification of the SHA256 hash, and then proceed to update any relevant files and firmware upon success.
Hardware Prerequisites
This code example was designed to work with the MSP432P4 family of devices and their corresponding LaunchPad evaluation modules:
Note that over-the-air updates on MSP432E4 families is not currently supported.
The host MSP432 LaunchPad requires either a CC3120 BoosterPack or a CC3135 BoosterPack to act as an application processor and gateway for cloud communication. Additionally a CC31XXEMUBOOST is required for initial flashing and configuration of the OTA device.
A picture of the MSP432P401 LaunchPad with the required CC3120 BoosterPack can be seen below:
A picture of the MSP432P4111 LaunchPad with the required CC3120 BoosterPack can be seen below:
Note that if the CC3135 is being used instead, the hardware configuration with the MSP432P4 devices is similar.
Software Prerequisites
This example has been validated against the latest software versions listed in the Release Notes.
For more information on how to import this project into your IDE workspace and build/run, please refer to the main user’s guide.
Note that the Uniflash utility is also required for creation and authoring of the OTA firmware package. A tutorial on how to use Uniflash as well as instructions on how to package an OTA image for firmware updates can be found in the main user’s guide.
Provisioning Method
Provisioning for this code example is done via the use of a mobile application. The following two mobile applications are supported.
- SimpleLink SDK Explorer (iOS)
- SimpleLink SDK Explorer (Android)
- Simplelink WiFi Starter Pro (iOS and Android)
Please refer to the User’s Guide section on provisioning for more information.
Usage
For a full tutorial/guide on how to use the OTA firmware update (both the local_ota and cloud_ota), please refer to the SimpleLink Academy Training Module on TI’s Resource Explorer.