6 #ifndef LV_IMG_DEOCER_H 7 #define LV_IMG_DEOCER_H 16 #ifdef LV_CONF_INCLUDE_SIMPLE 19 #include "../../../lv_conf.h" 23 #include "../lv_misc/lv_fs.h" 24 #include "../lv_misc/lv_types.h" 25 #include "../lv_misc/lv_area.h" 26 #include "../lv_core/lv_style.h" 32 #if LV_COLOR_DEPTH == 1 || LV_COLOR_DEPTH == 8 33 #define LV_IMG_PX_SIZE_ALPHA_BYTE 2 34 #elif LV_COLOR_DEPTH == 16 35 #define LV_IMG_PX_SIZE_ALPHA_BYTE 3 36 #elif LV_COLOR_DEPTH == 32 37 #define LV_IMG_PX_SIZE_ALPHA_BYTE 4 63 uint32_t always_zero : 3;
66 uint32_t reserved : 2;
161 lv_coord_t x, lv_coord_t y, lv_coord_t len, uint8_t * buf);
178 lv_img_decoder_user_data_t user_data;
340 lv_coord_t y, lv_coord_t len, uint8_t * buf);
uint8_t lv_img_cf_t
Definition: lv_img_decoder.h:116
Definition: lv_img_decoder.h:95
void lv_img_decoder_set_read_line_cb(lv_img_decoder_t *decoder, lv_img_decoder_read_line_f_t read_line_cb)
void(* lv_img_decoder_close_f_t)(struct _lv_img_decoder *decoder, struct _lv_img_decoder_dsc *dsc)
Definition: lv_img_decoder.h:168
Definition: lv_img_decoder.h:79
Definition: lv_img_decoder.h:102
Definition: lv_img_decoder.h:99
Definition: lv_img_decoder.h:105
lv_res_t(* lv_img_decoder_read_line_f_t)(struct _lv_img_decoder *decoder, struct _lv_img_decoder_dsc *dsc, lv_coord_t x, lv_coord_t y, lv_coord_t len, uint8_t *buf)
Definition: lv_img_decoder.h:160
Definition: lv_img_decoder.h:107
Definition: lv_img_decoder.h:111
void lv_img_decoder_built_in_close(lv_img_decoder_t *decoder, lv_img_decoder_dsc_t *dsc)
Definition: lv_img_decoder.h:114
Definition: lv_img_decoder.h:97
Definition: lv_img_decoder.h:100
Definition: lv_img_decoder.h:76
Definition: lv_img_decoder.h:113
void lv_img_decoder_set_info_cb(lv_img_decoder_t *decoder, lv_img_decoder_info_f_t info_cb)
struct _lv_img_decoder_dsc lv_img_decoder_dsc_t
Definition: lv_img_decoder.h:98
Definition: lv_img_decoder.h:74
Definition: lv_img_decoder.h:109
Definition: lv_img_decoder.h:103
void lv_img_decoder_close(lv_img_decoder_dsc_t *dsc)
Definition: lv_img_decoder.h:50
Definition: lv_img_decoder.h:88
lv_res_t lv_img_decoder_built_in_open(lv_img_decoder_t *decoder, lv_img_decoder_dsc_t *dsc)
Definition: lv_img_decoder.h:94
Definition: lv_img_decoder.h:47
Definition: lv_img_decoder.h:49
lv_res_t lv_img_decoder_read_line(lv_img_decoder_dsc_t *dsc, lv_coord_t x, lv_coord_t y, lv_coord_t len, uint8_t *buf)
Definition: lv_img_decoder.h:90
const char * error_msg
Definition: lv_img_decoder.h:210
struct _lv_img_decoder lv_img_decoder_t
const uint8_t * data
Definition: lv_img_decoder.h:124
const lv_style_t * style
Definition: lv_img_decoder.h:192
lv_img_decoder_info_f_t info_cb
Definition: lv_img_decoder.h:172
lv_res_t(* lv_img_decoder_info_f_t)(struct _lv_img_decoder *decoder, const void *src, lv_img_header_t *header)
Definition: lv_img_decoder.h:139
Definition: lv_img_decoder.h:110
Definition: lv_img_decoder.h:112
lv_img_decoder_t * decoder
Definition: lv_img_decoder.h:186
Definition: lv_img_decoder.h:87
Definition: lv_img_decoder.h:101
const void * src
Definition: lv_img_decoder.h:189
Definition: lv_img_decoder.h:84
Definition: lv_img_decoder.h:82
void lv_img_decoder_delete(lv_img_decoder_t *decoder)
lv_img_header_t header
Definition: lv_img_decoder.h:198
uint32_t time_to_open
Definition: lv_img_decoder.h:206
void lv_img_decoder_init(void)
lv_res_t lv_img_decoder_get_info(const char *src, lv_img_header_t *header)
lv_res_t lv_img_decoder_built_in_info(lv_img_decoder_t *decoder, const void *src, lv_img_header_t *header)
lv_res_t(* lv_img_decoder_open_f_t)(struct _lv_img_decoder *decoder, struct _lv_img_decoder_dsc *dsc)
Definition: lv_img_decoder.h:147
void * user_data
Definition: lv_img_decoder.h:213
Definition: lv_img_decoder.h:48
Definition: lv_img_decoder.h:120
lv_img_decoder_t * lv_img_decoder_create(void)
const uint8_t * img_data
Definition: lv_img_decoder.h:202
uint8_t lv_res_t
Definition: lv_types.h:33
lv_img_src_t src_type
Definition: lv_img_decoder.h:195
uint32_t data_size
Definition: lv_img_decoder.h:123
Definition: lv_img_decoder.h:170
lv_res_t lv_img_decoder_built_in_read_line(lv_img_decoder_t *decoder, lv_img_decoder_dsc_t *dsc, lv_coord_t x, lv_coord_t y, lv_coord_t len, uint8_t *buf)
lv_res_t lv_img_decoder_open(lv_img_decoder_dsc_t *dsc, const void *src, const lv_style_t *style)
Definition: lv_img_decoder.h:108
void lv_img_decoder_set_close_cb(lv_img_decoder_t *decoder, lv_img_decoder_close_f_t close_cb)
lv_img_decoder_read_line_f_t read_line_cb
Definition: lv_img_decoder.h:174
void lv_img_decoder_set_open_cb(lv_img_decoder_t *decoder, lv_img_decoder_open_f_t open_cb)
Definition: lv_img_decoder.h:92
Definition: lv_img_decoder.h:83
Definition: lv_img_decoder.h:93
uint8_t lv_img_src_t
Definition: lv_img_decoder.h:53
Definition: lv_img_decoder.h:183
Definition: lv_style.h:57
Definition: lv_img_decoder.h:104
lv_img_decoder_open_f_t open_cb
Definition: lv_img_decoder.h:173
lv_img_decoder_close_f_t close_cb
Definition: lv_img_decoder.h:175
Definition: lv_img_decoder.h:89
lv_img_header_t header
Definition: lv_img_decoder.h:122
Definition: lv_img_decoder.h:77