Table of Contents
- Introduction
- Hardware Prerequisites
- Software Prerequisites
- Service/Profile Table
- Usage
- IR Temperature Data (UUID: F000AA01-0451-4000-B000-000000000000)
- Humidity Data (UUID: F000AA21-0451-4000-B000-000000000000)
- Optical Data (UUID: F000AA71-0451-4000-B000-000000000000)
- Barometer Data (UUID: F000AA41-0451-4000-B000-000000000000)
- Movement Data (UUID: F000AA81-0451-4000-B000-000000000000)
- SBL Update
Introduction
The Sensors BoosterPack code example is a feature-rich code example that utilizes a variety of different sensors on the Sensors BoosterPack. Each sensor has it’s unique BLE profile and provides all relevant data from periodic sensor readings. When possible, each sensor characteristic tries to present readings in a human readable format (such a floats for temperature data) and provides a format presentation descriptor for convenience.
Hardware Prerequisites
The Sensors BoosterPack code example requires the standard configuration of an MSP-EXP432P401R LaunchPad with an attached BOOSTXL-CC2650 BoosterPack. Additionally, the Sensor BoosterPack code example requires the use of the Sensors BoosterPack. There is no specific order of stacking the LaunchPad/BoosterPacks, however to easily get to the sensor for testing it is recommended to put the Sensors BoosterPack on top. This hardware configuration is shown in the below image:
Note that due to memory limitations on the CC2640R2 SNP the CC2650 BoosterPack must be used.
For reference, the sensors that are included on the Sensors BoosterPack (and utilized in this code example) are as follows:
- Bosch BME280 - Temperature/humidity/barometric pressure sensor
- Bosch BMI160 - Accelerometer/gyrometer/magnetometer
- TI OPT3001 Digital ambient light sensor
- TI TMP007 Contactless infrared temperature sensor
Software Prerequisites
This code example has been tested with the tool and compiler versions listed in the Release Notes. For more information on how to import this project into your IDE workspace and build/run, please refer to the main user’s guide.
Note that this code example relies heavily on the Sensor and Actuator Interface Library (SAIL) Plugin. The SAIL plugin will provide all necessary software libraries and sensor interfacing APIs that are used to read out sensor data from the Sensors BoosterPack. This plugin must either be downloaded manually from the SAIL Plugin Product Page or from TI Resource Explorer in order for this code example to work correctly.
Service/Profile Table
Purpose | UUID | Format | Unit | Properties | Profile Source |
---|---|---|---|---|---|
IR Temperature Data | F000AA01-0451-4000-B000-000000000000 | IEEE-754 32-bit floating point | °C | Notify | ir_temp_service.c |
IR Temperature Config (enable) | F000AA02-0451-4000-B000-000000000000 | Integer | N/A | Read/Write | ir_temp_service.c |
IR Temperature Notification Period | F000AA03-0451-4000-B000-000000000000 | Integer | ms | Read/Write | ir_temp_service.c |
Humidity Data | F000AA21-0451-4000-B000-000000000000 | IEEE-754 32-bit floating point | Percent | Notify | humidity_service.c |
Humidity Config (enable) | F000AA22-0451-4000-B000-000000000000 | Integer | N/A | Read/Write | humidity_service.c |
Humidity Notification Period | F000AA23-0451-4000-B000-000000000000 | Integer | ms | Read/Write | humidity_service.c |
Barometer Data | F000AA41-0451-4000-B000-000000000000 | Integer | Pascals | Notify | barometer_service.c |
Barometer Config (enable) | F000AA42-0451-4000-B000-000000000000 | Integer | N/A | Read/Write | barometer_service.c |
Barometer Notification Period | F000AA43-0451-4000-B000-000000000000 | Integer | ms | Read/Write | barometer_service.c |
Optic Data | F000AA71-0451-4000-B000-000000000000 | IEEE-754 32-bit floating point | lux | Notify | optic_service.c |
Optic Config (enable) | F000AA72-0451-4000-B000-000000000000 | Integer | N/A | Read/Write | optic_service.c |
Optic Notification Period | F000AA73-0451-4000-B000-000000000000 | Integer | ms | Read/Write | optic_service.c |
Movement Data | F000AA81-0451-4000-B000-000000000000 | Integer | Custom | Notify | movement_service.c |
Movement Config (enable) | F000AA82-0451-4000-B000-000000000000 | Integer | N/A | Read/Write | movement_service.c |
Movement Notification Period | F000AA83-0451-4000-B000-000000000000 | Integer | ms | Read/Write | movement_service.c |
Usage
Once the sensors code example starts the output to the terminal will notify the user of initialization and then set the state of the application to idle:
In idle mode, the application is in a low power mode and not actively advertising. In order to start advertising, the S1 switch on the LaunchPad needs to be pressed. The S1 switch can be found on the left side of the LaunchPad as pictured below:
Once the S1 button is pressed, the device will start advertising itself with a device name of “MSP432 SensorHub”. Also note that once advertising (and while connected) the LED on the MSP432 LaunchPad’s LED1 pin is turned red to signify activity.
After connecting to the MSP432 SensorHub device, the terminal screen should print that the peer was connected and also print the ID of the peer:
At this point the device is connected and successfully negotiated the connection details. Scrolling down past the product information (this might be different depending on your client) there should be a list of four different characteristics and their corresponding properties/values (these are described in detail in the following sections):
Note that for each sensor service there are three different characteristics. The first characteristic (data) is a notification characteristic of the actual read sensor value. This notification only starts when an integer value of 1 is written to the second (conf) characteristic. Without writing a 1 value to the conf characteristic no data will be sent to the data notification characteristic. Writing a value of 0 to this characteristic will subsequently halt notifications. The third characteristic (period) is the period (in ms) of the notifications and can be changed at the user’s preference. The enabling/disabling of data notifications for each individual sensor is omitted from the subsequent systems for the sake of simplicity.
Also note that multiple notifications can be enabled in parallel without issue. All of the enabling of sensor notifications is logged through the UART console:
IR Temperature Data (UUID: F000AA01-0451-4000-B000-000000000000)
The temperature service gathers sensor readings from the TI TMP007 optical sensor. This is a contactless temperature sensor that can read temperature values at variable distances. Once enabled, place your finger on (or right above) the TMP007 sensor on the BoosterPack and you should see the temperature steadily rise. Note that for legible temperature readings you might need to set your mobile application to display float values.
Humidity Data (UUID: F000AA21-0451-4000-B000-000000000000)
The humidity service probes the Bosch BME280 sensor for a humidity reading and presents it as a percentage in float format. Once enabled, breath with some humidity directly on the BME270 sensor and you should see the humidity steadily rise (unless you are performing this test in a jungle somewhere). Note that for legible temperature readings you might need to set your mobile application to display float values.
Optical Data (UUID: F000AA71-0451-4000-B000-000000000000)
The optical service provides ambient light data (in lux) via the TI OPT3001 ambient light sensor. Once enabled, shine a bright light on the OPT3001 (perhaps with your phone’s LED) and you should see the lux value steadily rise. According to Wikipedia, the average lux level of an office environment is around 80 lux so shining an LED directly into the sensor should cause it to jump to around 2000 lux (as seen below):
Barometer Data (UUID: F000AA41-0451-4000-B000-000000000000)
Barometric pressure information is provided by the Bosch BME280 sensor and is presented in Pascal units as an integer value. After enabling the service, a steady stream of barometric pressure notifications should occur. Also according to Wikipedia, the standard barometric pressure is 101325 Pascals- so use this as a benchmark if you are living on Earth.
Movement Data (UUID: F000AA81-0451-4000-B000-000000000000)
The movement service provides several different positional and movement measurements from the Bosch BMI160 - accelerometer/gyrometer/magnetometer. The measurement format for this characteristic is a bit unique and consists of an 18 byte array with three different 6 byte sections. Each 6 byte sections contains the x/y/z measurements from the respective sensor.
For example, say that the sensor broadcasts a complete 16 byte array of values as:
0x010000000000 DEFFC5FFD83F 53FFB9FEA301
Parsing out each sensor reading, we would have:
- Gyrometer: 0x010000000000
- Accelerometer: 0xDEFFC5FFD83F
- Gyrometer: 0x53FFB9FEA301
Parsing out either further (and converting from little endian):
- Gyrometer:
- X: 0x0001
- Y: 0x0000
- Z: 0x0000
- Accelerometer
- X: 0xFFDE
- Y: 0xFFC5
- Z: 0x3FD8
- Magnetometer
- X: 0xFF53
- Y: 0xFEB9
- Z: 0x01A3
Note these values are parsed directly from the BMI160 registers readings. For more information on how to interpret the values, please refer to the BMI160 sensor datasheet.
SBL Update
Updating the firmware on the CC2650 BoosterPack uses the SBL libraries to invoke the CC2650’s bootloader and transfer the new firmware over serial. For Sensor BoosterPack, the method to trigger this invocation is to press and release the S2 button on the LaunchPad. Note that in order to trigger the firmware update, no active BLE device can be connected. Once S2 has been pressed, LED2 on the LaunchPad will toggle red to signal the BSL start:
*** Note that due to memory limitations in the CC2640R2 the CC2650 must be used for the Sensors BoosterPack example. ***
The console screen will print the status of the firmware update as well as signal when the update has finished. At the end of the update the status of the update will be printed over the serial port and the MSP432 will reboot itself: