Table of Contents

Introduction

The BLE Wi-Fi Provisioning example is an example that is designed to showcase the provisioning of Wi-Fi parameters (SSID, network key, etc.) over a BLE connection in a secure manner to a CC32xx host microcontroller. Wi-Fi provisioning over BLE provide various tangible benefits such as eliminating the need to explicitly connect to a shared network and simplified confirmation processes.

It is important to note that while the CC32xx is used for this code example, the host microcontroller is used as it would be for any other code example. All of the logic and BLE services/characteristics are handled on the CC32xx microcontroller and the CC26xx device is used in SNP mode as a “black box radio”. Once the SNP image is flashed onto the CC26xx device (see programming the SNP image section in the main user’s guide), no explicit programming on the CC26xx device needs to take place.

This example also allows the user to switch the provisioning mode from BLE provisioning to Access Point/SmartConfig (AP/SC) provisioning, as well as enabling the user to perform a SBL firmware update of the firmware running on the CC26xx SNP device.

Hardware Prerequisites

The BLE Wi-Fi Provisioning code example supports the following CC26xx BLE radios:

The CC26xx radio is connected to one of the supported host microcontrollers:

The LaunchPad configurations will have identical source code (with the exception of the board/hardware configuration files).

Note that because of pin assignments and the existence of “do not populate pins” on the CC32xx LaunchPads, a couple of minor rerouting of signals must be done in order to facilitate the pre-build CC26xx SNP image.

The following pins must be connected in order for the CC32xx to be able to successfully communicate with the CC26xx device. Pin numbers are given as reference to the CC32XX LaunchPad (and not the CC26xx SNP):

An example of these connections can be seen in the picture below:

WiFi Provisioning

Alternate Pin Mapping

Alternate SNP images are provided which remap the MRDY and SRDY signals of the CC26xx to different pins on the CC26xx LaunchPad or BoosterPack in order to simplify the hardware setup required when working with the CC32xx as the host. The alternate SNP images can be found in the source/ti/snp/cc3220_custom folder of the plugin installation. When working with the alternate SNP images, the MRDY and SRDY signals (from the perspective of the CC26xx) are moved to the following LaunchPad/BoosterPack headers:

In order to support the new locations of MRDY and SRDY from the host side, the GPIO pin configuration in the CC32xx_LAUNCHXL.c file of the host application must be updated. The MRDY and SRDY definitions in gpioPinConfigs[] must be updated as follows:

Once updated, gpioPinConfigs[] in CC32xx_LAUNCHXL.c should look as follows:

WiFi Provisioning

The actual digital IOs that the headers correspond to are different on the CC2640R2 LaunchPad and CC2650 BoosterPack. However, the following CC32xx pin must still be rerouted when working with the alternate SNP images. Pin numbers are given as a reference to the CC32XX LaunchPad:

An example of the connection for the alternate SNP image can be found below:

WiFi Provisioning

Software Prerequisites

This code example has been tested with the tool and compiler versions listed in the Release Notes. For more information on how to import this project into your IDE workspace and build/run, please refer to the main user’s guide.

Service/Profile Table

Purpose UUID Format Properties Profile Source
Provisioning Status FFF2 Integer Read/Write ble_wifi_provision_profile.c
Provisioning Notify FFF3 Integer Read/Write ble_wifi_provision_profile.c
SSID FFF4 String Encrypted Read/Encrypted Write ble_wifi_provision_profile.c
Security Key FFF5 String Encrypted Read/Encrypted Write ble_wifi_provision_profile.c
Device Name FFF6 String Read/Write ble_wifi_provision_profile.c
Provisioning Start FFF7 Integer Read/Write ble_wifi_provision_profile.c

Provisioning Process

The BLE provisioning process implemented in this example provides a method for programmers to fully configure and provision their CC32xx Wi-Fi device over BLE, which are described in the steps below:

  1. Provisioner (mobile phone) connects to advertised BLE service
  2. Passkey is displayed to user, which is entered into the provisioner to establish secure pairing
  3. SSID, Security Key, and Device Name are written to corresponding BLE characteristics
  4. Provisioning is initiated by writing 0x01 to “Provisioning Start” characteristic
  5. CC32xx device disconnects from BLE, attempts to connect to provisioned profile over Wi-Fi
  6. Once IP is obtained the device pings the resolved gateway to verify connectivity
  7. After successful ping the Wi-Fi radio disconnects and BLE is again advertised
  8. Provisioner reconnects to device over BLE and reads “Provisioning Status” characteristic
    • If the status signifies success the provisioner writes 0x02 to the “Provisioning Start” characteristic to signify confirmation
    • If the status signifies failure the provisioner reports the failure to the user and disconnects.
  9. After successful confirmation the device disconnects from BLE and reconnects to the provisioned network
  10. Once connected the device will go into a “ping loop” where gateway is repeatedly pinged

A graphical representation of the entire provisioning process can be seen in the flow chart below:

WiFi Provisioning

When a device has not been provisioned (or the device cannot connect with any of the provisioned profiles) it will enter a “provision loop” mode. In this mode the device will cycle infinitely between the following two steps:

  1. Advertising over BLE and waiting for a connection
  2. Trying to connect to any provisioned profiles.

The reasoning for this loop is to allow the opportunity for the device to connect to a provisioned network that might have come within range from device startup. The BLE will disconnect and try to connect to a provisioned network every thirty seconds.

As seen, if at any point during the provisioning process the device runs into an error state (such as gateway ping failure or failure to obtain an IP) the provisioning process bails out and the device returns to its “provisioning loop” stage.

Confirmation Status

As described in step eight of the provisioning process from the section above, the BLE central device (mobile phone) must reconnect to the CC32xx after initially writing the provisioning information to perform a confirmation. During this step the value of the “Provision Status” characteristic is read.

This characteristics can have one of the following values:

Re-Provisioning Device

Once the device has been successfully provisioned the device will enter a “ping loop” mode where the device will repeatedly ping the resolved gateway and report the result over UART terminal:

WiFi Provisioning

If at any point during the ping loop the user would like to re-provision the device the SW3 button should be quick pressed (if held longer than five seconds a SBL update will be initialized).

WiFi Provisioning

This will force the ping loop to start, the Wi-Fi to disconnect, and the BLE radio to start advertising to begin provisioning. If a timeout happens after a re-provision event has been initialized the Wi-Fi thread will connect back to the previously provisioned network and the ping loop will continue.

Coexistence of BLE/Wi-Fi Radio

In order to foster low noise across different wireless radios this application implements a form of coexistence between the BLE radio and the Wi-Fi radio. This means that whenever the Wi-Fi radio is active the BLE radio is disabled (and vice-versa). To signify when the BLE radio is active the LED attached to D10 is illuminated. When the BLE radio is inactive the LED attached to D10 is turned off.

Switching Provisioning Modes

This example also supports the AP/SC provisioning mode. To enable this mode, SW3 button should be held for at least three seconds (if held longer than five seconds a SBL update will be initialized). This will switch from BLE provisioning to AP/SC provisioning, and vice-versa. After the device is connected to a provisioner, the provisioning mode cannot be switched until the device is disconnected.

For an in-depth explanation of the AP and SC provisioning processes and how to connect to a network with this mode, please visit the SimpleLink Academy Wi-Fi Provisioning Lab.

Anatomy of the Code

The code in this code example is segregated into three different threads:

The bleThread and the wifiThread are active when BLE provisioning is being used.

The bleThread is responsible for managing the communication between the configured peripheral device (the CC32XX) and the central device connecting and configuring each of the configured BLE characteristics. Furthermore, the bleThread is responsible for initiating and performing the SBL firmware update of the firmware running on the CC26xx SNP device.

The following image shows the provisioning state machine that is implemented in the bleThread. The events that cause the transitions between states are shown.

WiFi Provisioning

The wifiThread is responsible for managing all aspects of the Wi-Fi connection the the CC32XX network processor. This involves communicating and configuring the Wi-Fi on startup, persisting provisioning parameters, and managing confirmation logic. Once a device is successfully provisioned the “ping loop” which perpetually pings the gateway is also setup in the ping loop itself.

The following image shows the provisioning state machine that is implemented in the wifiThread. The events or conditions that cause the transitions between states are shown.

WiFi Provisioning

The apThread is active when AP/SC provisioning is being used. This thread is responsible for configuring the device to run AP provisioning and SmartConfig provisioning simultaneously. Once the device is successfully provisioned, feedback is displayed to the user on the terminal window and the provisioning process ends.

The following image shows the provisioning state machine that is implemented in the apThread. The events or conditions that cause the transitions between states are shown.

WiFi Provisioning

Warning Codes

In the case that the state machine receives an unexpected event, a message will be displayed to the terminal window stating which thread received the event, and the event number that was received. The possible events that can be received are listed in the tables below. These events can also be found in ble_provisioning.h and ap_provisioning.h.

bleThread Event Name Value (Decimal)
BLE_NONE 1
BLE_EVT_PUI 2
BLE_EVT_ADV_ENB 4
BLE_EVT_ADV_END 8
BLE_EVT_CONN_EST 16
BLE_EVT_CONN_TERM 32
BLE_EVT_BUTTON_RESET 64
BLE_EVT_START_ADV 128
BLE_EVT_START_PROVISION 512
BLE_EVT_PROV_COMPLETE 1024
BLE_EVT_START_PAIR 1536
BLE_EVT_PAIRED 1792
BLE_EVT_WRONG_PASSKEY 1872
BLE_EVT_BSL_BUTTON 2048
BLE_EVT_SWITCH_PROV 2128
BLE_EVT_ERROR 2147483648
wifiThread Event Name Value (Decimal)
WIFI_NONE 1
WIFI_EVT_BLE_INITI 2
WIFI_EVT_RESET 4
WIFI_EVT_BLE_PROV_START 8
WIFI_EVT_SL_STARTED 16
WIFI_EVT_SL_CONNECTED 32
WIFI_EVT_BLE_PROV_COMPLETE 64
WIFI_EVT_REPROVISION 128
WIFI_EVT_BLE_TIME 512
WIFI_EVT_CONF_FAIL 1024
WIFI_EVT_ERROR 2147483648
apThread Event Name Value (Decimal)
PrvnEvent_Triggered 0
PrvnEvent_Started 1
PrvnEvent_StartFailed 2
PrvnEvent_ConfirmationSuccess 3
PrvnEvent_ConfirmationFailed 4
PrvnEvent_Stopped 5
PrvnEvent_WaitForConn 6
PrvnEvent_Timeout 7
PrvnEvent_Error 8
PrvnEvent_Max 9

BLE Mobile Provisioning

BLE Provisioning

The SimpleLink Starter Pro mobile application that is released with the CC32XX SDKs supports BLE provisioning. This applications supports both Android and iOS and supports advanced features such as SmartConfig, access point provisioning, and BLE provisioning. Legacy versions of iOS are supported and the program (for iOS) is written entirely in ObjectiveC. To download and use SimpleLink SDK Starter Pro please refer to the link below:

https://www.ti.com/tool/wifistarterpro

Note the screenshots below show iOS, however the interface/steps are identical for Android.

Open SimpleLink Starter Pro. From the main screen select BLE Provisioning from the tab bar on the bottom.

WiFi Provisioning

Touch on the BLE Devices drop down and select the device that is being advertised.

WiFi Provisioning

If this is your first time connecting to the BLE device, the mobile application will ask to pair with the device. To complete pairing, a passkey will appear on the terminal window. If you do not have your terminal window set up, please refer to the main user’s guide for help. Enter this passkey into your mobile application. If the correct passkey is entered, pairing is complete and the device is now bonded, so if the device is disconnected and then reconnects, the mobile phone will remember the device and a passkey does not need to be entered. Bonded devices can be forgotten through the phone’s Bluetooth settings.

WiFi Provisioning

Once the device is selected, fill out the relevant information about your network setup.

WiFi Provisioning

After all of the information is populated, press Start Configuration to start the configuration process and provision the device.

WiFi Provisioning

AP/SC Provisioning

The SimpleLink Starter Pro mobile application also supports AP/SC provisioning. These steps are listed in detail in the SimpleLink Academy Wi-Fi Provisioning Lab.

Generic Mobile Application

In addition to the specialized mobile applications that TI provide, generic mobile applications can also be used to directly provision the CC32xx device at a more low level. Any BLE application can be used, but TI recommends:

When using these applications the following flow can be used to provision the device in a simple barebone manner. These screenshots show how to provision the device with LightBlue for iOS, however other BLE applications will have a similar flow.

Connect to advertised BLE device (device name as “CC32XX WiFi” byte default)

WiFi Provisioning

If this is your first time connecting to the BLE device, the mobile application will ask to pair with the device. To complete pairing, a passkey will appear on the terminal window. If you do not have your terminal window set up, please refer to the main user’s guide for help. Enter this passkey into your mobile application. If the correct passkey is entered, pairing is complete and the device is now bonded, so if the device is disconnected and then reconnects, the mobile phone will remember the device and a passkey does not need to be entered. Bonded devices can be forgotten through the phone’s Bluetooth settings.

WiFi Provisioning

Write SSID (required), security key (optional), and device name (optional)

WiFi Provisioning

WiFi Provisioning

Write 0x01 to “Provision Start” characteristic

WiFi Provisioning

WiFi Provisioning

Wait for IP to be acquired (this will be displayed on the terminal output). Once acquired, reconnect to the device and read the “Provision Status” register. Verify that it is 0x00 (provision success):

WiFi Provisioning

Write 0x02 to the “Provision Start” register and the device will disconnect. The device is now provisioned. In the terminal window the ping loop will display.

SBL Update

Updating the firmware on the CC26xx device uses the SBL libraries to invoke the CC26xx’s bootloader and transfer the new firmware over serial. For LCD BoosterPack Text, the method to trigger this invocation is to hold down the SW3 on the LaunchPad for a duration of at least five seconds. Note that in order to trigger the firmware update, no active BLE device can be connected. Once SW3 is held down for five seconds, a message will be displayed on the UART terminal and LED2 on the LaunchPad will illuminate to signal the BSL start.

The image for the SNP resides on the CC32XX device’s external flash must be explicitly programmed by the user using the Uniflash programming tool. When the SBL is invoked, the device will disconnect from BLE and Wi-Fi and enter in “SBL” mode. The CC32XX device will then open the file located at /cc26xx/snp_image.bin and attempt to program the CC26xx device using the CC26xx’s external UART bootloader. The CC26xx SBL interface is documented in the CC26xx Bootloader Interface document.

Note that the path to the SNP image on the CC32xx’s external flash can be programmed by changing the SNP_FIRMWARE_PATH variable in sbl_wifi_snp_update.h.

The console screen will print the status of the firmware update as well as signal when the update has finished. At the end of the update the status of the update will be printed over the serial port and the CC32xx will reboot itself:

WiFi Provisioning

Use of an External LCD

It is entirely possible to connect an external LCD BoosterPack such as the 430BOOST-SHARP96 or BOOSTXL-K350QVG-S1 to the hardware configuration. The main purpose of having a dedicated LCD would be to have a mechanism to display the pairing/bonding pass code during the connection process without explicitly requiring the user to hook their LaunchPad up to a UART terminal.

When using an external LCD one consideration is that there will likely be pin conflicts with the CC32xx LaunchPad and the CC26XX SNP radio. Since many of the pins on the LCD BoosterPacks conflict with those used for the CC32xx<->CC26XX communication interface there will likely be a physical modification of the signals on the LCD BoosterPack that needs to occur. In actual design this will not be an issue as a custom layout/PCB will be made, but for evaluation be mindful that the signal requirements of the LCD BoosterPack will need to be made compatible with the CC32XX<->CC26XX communication.

Once the correct hardware modifications are made, displaying the passcode for use in the pairing process can be easily done using the Graphics Library that is included in the CC32xx SDK. Specifically, the Display to LCD example of the platform SDK will show the required software hooks necessary to display a text string to an external LCD using the Display driver.