TEXAS INSTRUMENTS, INC. ----------------------- Title: Windows CE 6.0 TI_DEFAULT Images for AM35XX, OMAP35XX and AM/DM37XX ********************************************************************** NOTICE The item accompanying this notice does not constitute a Formal Release from Texas Instruments, Inc. (as defined in the Texas Instruments, Inc. Release Note Standard and Procedure) and, as such, Texas Instruments, Inc. can accept no liability and offer no warranty on the accompanying item. The item is offered only for evaluation or demonstration purposes ********************************************************************** INTRODUCTION ------------ This is a release notification for v1.00.00 of the Windows CE 6.0 Demo Images for the AM35XX and OMAP35XX EVMs . This is a binary only release of a demonstration build of the CE 6.0 BSP. The demo images are built from the AM35x_OSDesign and EVM_3530 OSDesigns found in the source release. The demo images contain: - Silverlight sample application - Windows Media Player/ DVSDK - Internet Explorer 6.0 Sample Browser - Graphics(PowerVR) demos DISTRIBUTION CONTENTS --------------------- ReadMe.txt - This release note AM35x demo: Demo_images\AM35XX\AM35x-nand.raw - AM35x image file (XLDR and EBoot) to be flashed in NAND Demo_images\AM35XX\AM35x-nand-logo.raw - AM35x image file (XLDR, EBoot and logo) to be flashed in NAND Demo_images\AM35XX\EBOOTSD.nb0 - EBOOT image for SD boot Demo_images\AM35XX\MLO - XLDR image for SD boot Demo_images\AM35XX\XLDRUART.nb0 - XLDR image for UART boot, used for flashing NAND Demo_images\AM35XX\NK_demo.bin - default NK.bin image built from sample OSDesign Demo_images\AM35XX\NK_PM_Policies.bin - NK.bin image with PM policy enabled Demo_images\AM35XX\NK_usbfn_active_sync.bin - NK.bin image with active sync enabled for USB port Demo_images\AM35XX\NK_usbfn_rndis.bin - NK.bin image with RNDIS enabled for USB port OMAP35xx and DM/AM37xx demo: Demo_images\OMAP35XX_AMDM37XX\OMAP35xx-nand.raw - OMAP35xx/DM37xx image file (XLDR and EBoot) to be flashed in NAND Demo_images\OMAP35XX_AMDM37XX\OMAP35xx-nand-logo.raw - OMAP35xx/DM37xx image file (XLDR, EBoot and logo) to be flashed in NAND Demo_images\OMAP35XX_AMDM37XX\EBOOTSD.nb0 - EBOOT image for SD boot Demo_images\OMAP35XX_AMDM37XX\MLO - XLDR image for SD boot Demo_images\OMAP35XX_AMDM37XX\XLDRUART.nb0 - XLDR image for UART boot, used for flashing NAND Demo_images\OMAP35XX_AMDM37XX\NK_demo.bin - default NK.bin image built from sample OSDesign Demo_images\OMAP35XX_AMDM37XX\NK_PM_Policies.bin - NK.bin image with PM policy enabled REQUIREMENTS ------------ Hardware requirements: - For AM35xx processors: o ZOOM AM3517 EVM Development Kit. (http://www.logicpd.com/) - For OMAP35xx and AM/DM37xx processors: o OMAP35x Evaluation Module (EVM) (http://www.mistralsolutions.com/) - Windows PC with a serial port - Serial cable to connet the PC to the EVM (supplied with the EVM) - SD/MMC card to boot the CE image from - PC SD/MMC card reader (e.g. USB SD/MMC card reader) Software requirements: - Serial terminal application (e.g. Hyperterminal or TeraTerm) INSTALLATION INSTRUCTIONS ------------------------- Write the CE 6.0 image to the SD card and configure EBOOT to boot from SD card by following the instructions in section "Running OS Designs" of BSP_WINCE_ARM_A8 Quick Start Guide. NOTES ----- Notes: 1. The same image can be used for OMAP35xx processors, as well as AM/DM37xx processors. The detection of the processor is at run time. PROBLEM REPORTING ----------------- Please use TI e2e WinCE Community forum(http://e2e.ti.com/support/embedded/f/353.aspx) ---------------------------------------------------------------------------- End