This is an GA release of the SYS/BIOS OpenMP runtime environement.
This is a SYS/BIOS port of the libgomp OpenMP runtime environment. This product is designed to eventually integrate with OpenMP-aware Texas Instruments compilers. This runtime environemnt is designed to be a layer between the lowered code generated by the compiler and SYS/BIOS.
The OpenMP product is comprised of one main package
The following documentation is available:
User Install Guide | Documents how to use this product |
Cdoc API guide | Documents config-time (RTSC) APIs, Asserts and Errors |
Highlights:
For information on enhancements and defect fixes in earlier releases, please refer to the release notes from previous releases that are available in the relnotes_archive directory.
This release supports the following hosts:
Windows XP SP2/SP3
Windows Vista
Linux (Redhat 4 and 5)
This release requires the following other software components and tools versions to successfully function:
All releases have 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 1.00.00.00_eng).
This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. omp_1_00_00_00_eng.
Subsequent releases of patch upgrades will be identified by the patch number, ex. OMP 1.00.00.00 with directory omp_1_00_00_00_eng. Typically, these patches only include critical bug fixes.
Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.
For technical support, use the community forum TI E2E Community, or email softwaresupport@ti.com.
Last updated: