IMGLIB 3_0_1_0 Product Download Page
Generated On: 06212011
This is a patch release of the Image and Video Processing Library
(IMGLIB) for C64x+/C66x processors.
IMGLIB contains optimized general-purpose image/video processing routines that
are used in computationally-intensive real-time applications. These C-callable
routines operate considerably faster than equivalent code written in ANSI C language.
The deliverables in this release include a Windows or Linux installation
executable for either the C64x+ or C66x processors. Each executable installs a
component package repository, a documentation directory, an Eclipse plugin
directory and an expanded component directory structure with component libraries,
header files and test examples.
NOTE: This release of IMGLIB provides a subset of the kernels in the
IMGLIB 2.x baseline
and consists of the following categories:
- Boundary and Perimeter
- Dilation and Erosion
- Edge Detection
- Histogram
- Image Thresholding
- Convolution
- Correlation
- Median Filtering
Categories missing from the release 2.x baseline will be considered for inclusion
in upcoming releases of the 3.x baseline.
Software Defects
A list of tracked software defects can be found here.
(Note: If prompted for login/password, close the window and try the link again)
Related Links
|
|