=== LAB SETUP === 1. Download all components to a local directory. 2. Extract the file to the local directory. This will create a directory CCS5.2.1.00018_win32\ 3. From inside the directory CCS5.2.1.00018_win32\, execute the installer Use c:\ti as the installation location 4. Execute the Use c:\ti as the installation location 5. Install a new release of the TMS470 compiler. - Start CCS by double-clicking on its icon. Choose the default workspace. - Go to menu "Help" --> "Install New Software" - In the drop-down menu "Work with:" select "Code Generation Tools Updates" - Expand the TI Compiler Updates and select "ARM Compiler Tools" Version "4.9.6" (you may need to uncheck the box "Show only the latest versions of available software") - Click Next - Click Next again - Accept the license terms. Click Finish. - Restart the workbench as instructed. The plug-in is installed. 6. Copy the file to the directory c:\ti 7. Install the Terminal plugin (requires an active internet connection) - Start CCS by double-clicking on its icon. Choose the default workspace. - Go to menu "Help" --> "Install New Software" - Click on the hyperlink "Available Software Sites" - Scroll down on the list and check the box beside the following Location: http://download.eclipse.org/tm/updates/3.3 - Click OK - In the drop-down menu "Work with:", select the entry that corresponds to the link in the previous step. Wait until it finishes loading. - Click on the checkbox next to "Target Management Terminal" under "TM and RSE 3.31 Main Features". Click Next - Click Next again - Accept the license terms. Click Finish. - Restart the workbench as instructed. The plug-in is installed.