2.3. Yocto Layer ConfigurationΒΆ

Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:

$ ./oe-layersetup.sh -f <config>


The following config files are located in the configs/processor-sdk directory of the oe-layersetup git repo.
Config File Description Supported machines/platforms
processor-sdk-06.02.00.81-config.txt Processor SDK 6.2.0.81 Release am57xx-evm, am65xx-evm