2.3. Yocto Layer ConfigurationΒΆ

Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:

$ ./oe-layersetup.sh -f <config>


The following config files are located in the configs/processor-sdk directory of the oe-layersetup git repo.
Config File Description Supported machines/platforms
processor-sdk-06.00.00.07-config.txt Processor SDK 6.0.0.7 Release am335x-evm, am437x-evm, am57xx-evm, am65xx-evm, k2hk-evm, k2e-evm, k2l-evm, k2g-evm, omapl138-lcdk