1.6. GPLv3 DisclaimerΒΆ

There are GPLv3 licensed software components contained within the Processor SDK for Android on both the target and the host. The software manifest (Processor-SDK_Android_AM57X_Manifest.html) for the Android SDK is located in the docs/ directory of the installed SDK. The NOTICE.html file for the Android Open Source Project is also located in the docs/ directory. All GPLv3 components for both target and host are contained in the SDK directory.