SimpleLink SDK CC3x20 Service Pack
Table of Contents
Introduction
The SimpleLink™ Wi-Fi® CC3220 device is a single-chip microcontroller (MCU) with built-in Wi-Fi connectivity, created for the Internet of Things (IoT). The CC3220 device is a wireless MCU that integrates a high-performance ARM® Cortex®-M4 MCU, allowing customers to develop an entire application with a single IC.
Content and Documentation
This release include the ServicePack binary image to be programmed into CC3120/CC3220 devices. ServicePack must be applied both in production and development stage of the CC3120/CC3220 devices
File | Notes |
---|---|
sp_3.5.0.0_2.0.0.0_2.2.0.5.bin | ServicePack binary for UniFlash |
sp_3.5.0.0_2.0.0.0_2.2.0.5.ucf | ServicePack UCF for host driver API |
sp_3.5.0.0_2.0.0.0_2.2.0.5.ucf.signed.bin | ServicePack UCF signature |
Version information
Component | Version |
---|---|
NWP | 3.5.0.0 |
MAC | 2.0.0.0 |
PHY | 2.2.0.5 |
Note: Upon successful ServicePack programming, version can be retrieved using ‘sl_DeviceGet()’ API, with SL_DEVICE_GENERAL_VERSION option.
What’s New
- Support installing a certificate only in the crypto util module (until now private key is a must when installing a security element in the crypto util). the certificate is used only for verification of a buffer.
- Support ECDSAwithSHA256 signature verification in the crypto util.
- Support ECDSAwithDIGEST in the crypto util. this enables checking a message with a message digested in the application layer.
Upgrade and Compatibility Information
The ServicePack can be programmed using UniFlash utility version v4.3 and up. Latest UniFlash utility can be downloaded from https://www.ti.com/tool/UniFlash.
The ServicePack can also be flushed using host driver API’s or OTA application (please refer for the SimpleLink CC3x20 SDK for more information)
Dependencies
This release requires the following software components and tools:
- UniFlash utility v4.3 and up - Download page.
- The ServicePack is bounded to host driver 2.0.1.22
Device Support
- CC3120R
- CC3220R – Base variant
- CC3220S – CC3220 and MCU security
- CC3220SF – CC3220S and internal flash.
Evaluation Boards
- CC3120_LAUNCHXL
- CC3220R_LAUNCHXL
- CC3220S_LAUNCHXL
- CC3220SF_LAUNCHXL
Fixed Issues
${GEN2_3500_FIXED}
Known Issues
${GEN2_OPEN_ISSUES}
Versioning
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp should be zero indicating official version and b is an unrestricted set of digits used as an incrementing build counter.
Technical Support and Product Updates
- Visit the E2E Forum