LCD Text Display Code Example
Table of Contents
- Introduction
- Hardware Prerequisites
- Software Prerequisites
- Service/Profile Table
- Usage
- Text String Characteristic (UUID: F0001131-0451-4000-B000-000000000000)
- Text Color Characteristic (UUID: F0001132-0451-4000-B000-000000000000)
- X Position Characteristic (UUID: F0001133-0451-4000-B000-000000000000)
- Y Position Characteristic (UUID: F0001134-0451-4000-B000-000000000000)
- Text Size Characteristic (UUID: F0001135-0451-4000-B000-000000000000)
- Background Color Characteristic (UUID: F0001136-0451-4000-B000-000000000000)
- SBL Update
Introduction
The LCD BoosterPack Text example is an application that demonstrates the use of the Kentec QVGA BoosterPack to display text on an LCD screen with a variety of different styling configurations. The user has the ability to display a variable text message of their choice and change the font size, font color, text position, and background color. This code example leverages the MSP432 Graphics Library that is shipped with the SimpleLink MSP432 SDK.
Hardware Prerequisites
The LCD BoosterPack Text ccode example requires the standard configuration of an MSP-EXP432P401R LaunchPad with an attached BOOSTXL-CC2650 BoosterPack or LAUNCHXL-CC2640R2 Launchpad. Additionally, a Kentec QVGA BoosterPack must be stacked on top of the CC2650 BoosterPack. This hardware configuration is shown in the below image:
Alternatively, the CC2640R2 LaunchPad can be used in lieu of the CC2650 BoosterPack. In this case the CC2640R2 LaunchPad should be stacked on the MSP432 LaunchPad as seen below:
Software Prerequisites
This code example has been tested with IAR Embeded Workbench 8.11, Code Composer Studio v7.4, and gcc-arm-none-eabi-6-2017-q1-update. For more information on how to import this project into your IDE workspace and build/run, please refer to the main user’s guide.
Service/Profile Table
Purpose | UUID | Format | Properties | Profile Source |
---|---|---|---|---|
Text String | F0001131-0451-4000-B000-000000000000 | Integer | Read/Write | lcd_service.c |
Text Color | F0001132-0451-4000-B000-000000000000 | Integer | Read/Write | lcd_service.c |
X Position | F0001133-0451-4000-B000-000000000000 | Integer | Read/Write | lcd_service.c |
Y Position | F0001134-0451-4000-B000-000000000000 | Integer | Read/Write | lcd_service.c |
Text Size | F0001135-0451-4000-B000-000000000000 | Integer | Read/Write | lcd_service.c |
Background Color | F0001136-0451-4000-B000-000000000000 | Integer | Read/Write | lcd_service.c |
Usage
Once the LCD BoosterPack Text code example starts, the LCD will turn to a black background with the text “Simplelink MSP432 SDK Bluetooth Plugin” displayed on the screen.
By default, this code example starts with BLE advertisement enabled indefinitely. Using your BLE client of choice, search for the “MSP432 LCD” device and connect:
Once connected, scroll down past the product information (this might be different depending on your client) and there should be a list of six different characteristics and their corresponding properties/values (these are described in detail in the following sections):
Text String Characteristic (UUID: F0001131-0451-4000-B000-000000000000)
The text string characteristic will change the value of the text that is displayed on the screen. From your client application, write any desired string value to this characteristic and the displayed text on the LCD will change:
Text Color Characteristic (UUID: F0001132-0451-4000-B000-000000000000)
The text color characteristic is a three byte value that controls the RGB value of the font display. The byte order is in the format of BB GG RR. For example, writing a value of 0000FF to the characteristic would change the text color to full red.
Note that any combination of RGB values can be used.
X Position Characteristic (UUID: F0001133-0451-4000-B000-000000000000)
The X Position characteristic is the position of the beginning of the text string starting from the left side of the screen. The position is limited by the X resolution of the LCD screen (320) and a value from 0 to 320 can be used. A value of 160 will roughly put the text in the horizontal center of the screen.
Y Position Characteristic (UUID: F0001134-0451-4000-B000-000000000000)
The Y Position characteristic is the position of the top of the text starting from the top side of the screen. This value is limited by the Y resolution of the LCD screen (240) and a value from 0 to 240 can be used. A value of 120 will roughly put the text in the vertical center of the screen.
Text Size Characteristic (UUID: F0001135-0451-4000-B000-000000000000)
The text size characteristic changes the font size of the text on the screen. This code example has a total of eighteen different fonts (0 being the smallest, 17 being the largest). Changing the value of this characteristic will change the font size of the displayed string:
The last characteristic controls the background color of the LCD. The format of this characteristic is identical to the format of the text color characteristic (six byte BB GG RR value). Write to this value to change the background color:
Background Color Characteristic (UUID: F0001136-0451-4000-B000-000000000000)
SBL Update
With the LCD BoosterPack code example a considerable amount of memory is used to store the various fonts used in displaying the text on the LCD screen. For this reason the SBL feature has been disabled to reserve room for the font files used in display.