Ultrasonic Sensing Design Center Release Notes
Table of Contents
Introduction
The ultrasonic design center is a one stop resource for everything related to ultrasonic sensing technology using MSP430™ microcontrollers (MCUs). It includes tools, graphical user interface (GUI), documentation, software library and application examples for developers to get started with project developments. The ultrasonic design center GUI is a rapid development tool for configuring and customizing various parameters related to transducers, pipe size as well as analyzing and capturing waveforms.
This is version 02.40.00.00 of Ultrasonic Sensing Design Center.
Features
- Provides API set for ultrasonic sensing on the MSP430FR604x device family
- Provides ultrasonic sensing design center for GUI-based tuning and visualization of library functionality
- Provides examples for out-of-the-box integration with application code and GUI configuration The MSP430 MCU gas library (MSP-GASLIB) provides the means to configure the internal ADC for ultrasonic captures and help to integrate it with the application software for ultrasonic gas metrology applications. The library also takes advantage of LEA module in MSP43FR599x devices to compute time of flight (ToF) measurement
Documentation
- License
- Software Library Manifest
- Design Center User’s Guide
- Software Library User’s Guide
- Software Library API Guide
What’s New
Design Center
Software Library
Upgrade and Compatibility Information
No special action is required to upgrade to this release.
Installation and Usage
- Download Ultrasonic Design Center
- Run the appropriate platform specific installer: USSLib-
- -installer - Follow the installer directions
- To launch tool, use the desktop icon or execute the tool directly:
- Windows
- Start Menu -> All Programs -> Texas Instruments -> USS_<version> -> USS
- C:/ti/msp/USS_<version>/USS.exe
- OS X
- /Applications/ti/msp/USS_<version>/USS
- Linux OS
- ~/ti/msp/USS_<version>/USS
- Windows
Host Support
Supported Operating Systems:
- Windows 7, 10
- Linux OS
- Apple OS X
Dependencies
- Java JRE 1.7 or later must be installed on the host system. Click here to go to Java Download Page.
- Source code generated by this release requires:
- Code Composer Studio (CCS) v10.0.0 or higher
- IAR Embedded Workbench 7.20 or higher
Device Support
The following list of devices with are supported in this release of Ultrasonic Sensing Design Center:
- MSP430FR5041
- MSP430FR5043
- MSP430FR50431
- MSP430FR6005
- MSP430FR6007
- MSP430FR6041
- MSP430FR6043
- MSP430FR60431
- MSP430FR6045
- MSP430FR6047
- MSP430FR60471
Validation Information
The Ultrasonic Sensing Design Center was validated with the following components:
- IDE
- Code Composer Studio 10.0.0
- TI Code Generation Tools : TI v20.2.0.LTS
- IAR Embedded Workbench 7.20
- EVM Hardware
- EVM430-FR6047
Known Issues
- Configuration parameter
algorithmsConfig.dcOffset
is only applied to VFR calculation. If users want to apply the same correction to DToF calculation it has to be done at the application level.
Versioning
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
Technical Support and Product Updates
- Visit the MSP E2E Forum for support.