Speech Recognizer Project API Guide
v1.00.00.00
|
The MinHMM API | The MinHMM API is the top-level API |
MinHMM Configuration | Build-time configuration parameters that specify what functions and capabilities were included when the MinHMM Library was built |
MinHMM Memory Allocation Defines | Macro definitions that the application uses to allocate memory for MinHMM |
MinHMM Structs and Types | Structures and types used in performing the tasks of the top-level user interface functions of MinHMM |
MinHMM User Functions | The top-level user interface functions within MinHMM |
The VAD API | The VAD API implements general audio activity detection based on the energy of an audio signal |
VAD API functions | Functions of the VAD API |
VAD Parameter Defaults | Default parameter settings for the VAD API |
VAD Typedefs and Enums | Enums and types used by the VAD API |