SMBus Library for MSP430G2xx3 Devices
1.10.00.00
Main Page
Modules
Data Structures
Files
File List
All
Data Structures
Functions
Variables
Enumerations
Enumerator
Modules
Pages
mainpage_MSP430G2xx3.h
1
/**
2
* @mainpage MSP430&tm; SMBusLib for MSP430G2xx3 Devices
3
*
4
* @section intro Introduction
5
*
6
* This document describes the implementation of the system management bus (SMBus) using the
7
* MSP430&tm; microcontroller I2C peripheral. SMBus is used as a communication link for smart batteries,
8
* power-related devices, and a wide variety of other system devices.
9
*
10
* The MSP430&tm; SMBus Library is a royalty-free set of API's that provide support for master
11
* and slave protocols in a SMBus communication system.
12
*
13
*
14
* This API document is broken out into the following sections:
15
* - Modules Tab
16
* - Application API layer, a list of the public API's designed to be called by user
17
* applications.
18
* - Network layer, the functions that implement and manage the internal SMBus state.
19
* User applications should not call functions in this layer.
20
* - Phyical layer, the functions that implement the device dependent calls to the
21
* microcontroller. User applications should not call functions in this layer.
22
* User application should not call functions in this layer.
23
* - Data Structures Tab
24
* - Data Structures, a list of data structures defined by MSP430&tm; SMBus Library
25
* - Data Fields, a list of fields available in the data structures
26
* - Files Tab
27
* - File List, an alphabetical list of API's avaialable in MSP430&tm; SMBus Library
28
* - Globals, an alphabetical list of MSP430&tm; SMBus Library global definitions
29
* - Related Pages Tab
30
* - Legal disclaimer*
31
*
32
* Also note the existence of the following content available on disk. This is not
33
* part of this API but contains useful example code and documentation.
34
*
35
* - Example Code
36
* - under examples/driverlib/MSP430G2xx3/{peripheral}
37
* - Users Guide
38
* - doc/driverlib/MSP430G2xx3/MSP430G2xx3_DriverLib_Users_Guide-1.10.00.00.pdf
39
*
40
*/
Copyright 2015, Texas Instruments Incorporated