NFCLink 1_0_0_3
Build date: 12012014
Release Information
Click on the links in the table below to download.
NFCLink
Description
This application has an NFC Host and an NFC Controller which communicate using the NFC Controller Interface(NCI). The controller runs on the MSP430F5529 Experimenter's board + TRF7970A NFC transciever- supporting Reader/Writer, Peer to Peer, and Card Emulation. The host runs on a GUI for Windows XP/7. There are two modules the MSP430F5529 can use to interface with a PC: UART and USB CDC. For the UART project, an external UART-to-USB bridge is required (not included in the MSP430F5529 Experimenter's board).
Dependencies
NFCLink Tool Chain Dependencies:
Device Support
This release supports the following devices:
Legend
|
Fill in Form. Approved users receive download URL in 1 minute. |
|
|
Fill in Form. TI will contact you in 1-2+ business days. |
|
For more information:
Mon Dec 1 16:03:11 CST 2014