MSP_GANG 1_01_02_00
Build date: 03062013
Release Information
Click on the links in the table below to download.
The
MSP
Gang Programmer is an MSP430 device programmer that can program up to
eight identical MSP430 flash or FRAM devices at the same time. The MSP
Gang Programmer connects to a host PC using a standard RS-232 or USB
connection and provides flexible programming options that allow the
user to fully customize the process.
The MSP Gang Programmer is
provided with an expansion board, called the Gang Splitter, that
implements the interconnections between the MSP Gang Programmer and
multiple target devices. Eight cables are provided that connect the
expansion board to eight target devices (via JTAG or Spy-Bi-Wire
connectors). The programming can be done with a PC or as a standalone
device. A PC-side Graphical User Interface is also available and is
DLL-based.
Features
- 3x Faster than the previous GANG programmer version,
MSP-GANG430
- Quickly program Flash or FRAM-based MSP
devices via an RS-232 or USB interface
- Several programming modes:
- Interactive Mode – Programming while connected to PC
using the MSP GANG Programmer GUI
- Program
from Image – An image can be stored, which contains configuration
options and code files. This allows users to program MSP devices
standalone, without a PC
- Programming from Script – Enables developers to automate
more complicated programming procedures.
- Intuitive GUI for configuring, programming &
testing production setup
- SD Card slot for storing images
- LCD screen for easy programming without a PC
- Supports up to 8 targets simultaneously
- Supports all current and future MSP430 devices
Changes in This Release
- Added support for
• MSP430G2444, MSP430G2544, MSP430G2744, MSP430G2755, MSP430G2855, MSP430G2955
- Fixes for following bugs/issues:
• MSP430F47126 and MSP430F47127 not recongnized.
• Open Notepad in Windows 64bit does not work.
• The programming over the BSL without using the password file doesn't work if password from the file option is selected.
• Writing the Serial Number to protected Info-A sector using function MSPGANG_Interactive_Copy_GANG_Buffer_to_FLASH(address, size) failed.
• Erasing a lot of sectors of the flash - sector by sector can reset the MSP-GANG.
Known Issues
On FRxx devices a 0x0000 is written into the address following the last write operation.
This can cause a problem if for example a JTAG- or BSL-password is overwritten.
Fixed as of version 1.1.6.0.
Older Releases
1_00_05_00
1_00_06_00
1_00_07_00
1_00_08_00
1_00_09_00
1_01_00_00
Legend
|
Fill in Form. Approved users receive download URL in 1 minute. |
|
|
Fill in Form. TI will contact you in 1-2+ business days. |
|
For more information:
Wed Mar 6 09:46:20 CST 2013
|