TI Software


MSPWare  2_00_00_41

Build date: 03192015

Release Information

Click on the links in the table below to download.

MSPWare is a collection of code examples, datasheets and other design resources for ALL MSP430 and MSP432 devices delivered in a convenient package - essentially everything developers need to become MSP experts!

What's New?

  • Renamed MSP430Ware -> MSPWare
  • Updated MSP430 Driver Library to version 2_00_00_16
  • Updated Graphics Library to version 2_00_00_17
  • Updated MSP430 USB Developer’s Package to version 5_00_00
  • Updated IEC60730 Library to version 1_04_00_05
  • Updated IQMath Library to version 01_10_00_05
  • Added MSP432 Driver Library version 01_04_00_18
  • Added MSP-EXP432P401R Software Collateral version 1_00_05_00
  • Added MSP-EXP432P401R Hardware Collateral version 1_00_05_00
  • Added BOOSTXL-K350QVG-S1 Hardware Collateral version 1_00_00_00
  • Added MSP432P4xx Deep Dive Training Material
  • Added MSP432P4xx Family Collateral. Includes datasheet, user’s guide, erratasheet and code examples
  • Added links to MSP LaunchPad Training Workshops
  • Added SMBusLib Software Library version 1_10_00_00

Install/Upgrade

There are two methods to install MSPWare:

Installing via the Code Composer Studio (CCS) App Center

If you have CCS 6.0 or later you can install MSPWare via the CCS App Center.

  1. Open up CCS
  2. Click “View->CCS App Center”
  3. Click the checkbox next to MSPWare
  4. Then click “Install Software” in the top left corner of the app center.
  5. Let CCS restart and discover the software. You can now use TI Resource Explorer within CCS

Installing via the Standalone Installer

If CCS is not your primary IDE or want an offline installer on hand you can download the standalone installer.

  1. Download the standalone installer from the table below.
  2. Double click to run the installer, the default installation path is discoverable by CCS
  3. Run CCS and let it discover the MSPWare installation. You can now use TI Resource Explorer within CCS.

FAQ

What is the difference between MSPWare and Driver Library?

MSPWare is a collection of MSP430 and MSP432 software and tools. One of the main components of MSPWare is Driver Library (DriverLib).

Why are there multiple driverlib folders within MSPWare?

MSPWare contains many different software libraries and projects. Some of these components depend on a specific version of Driver Library. Each component ships the version of Driver Library they tested with to ensure that all software works for you out of the box.

Can I have multiple versions of MSPWare installed?

Yes! MSPWare installations can exist alongside each other. You should only see the latest installed version within the TI Resource Explorer window of Code Composer Studio however.

How can I get support for MSPWare?

Feel free to use the TI E2E forum to ask anything MSPWare related.

Legend

Locked Fill in Form. Approved users receive download URL in 1 minute.   Locked Fill in Form. TI will contact you in 1-2+ business days.

MSPWare Product Downloads
Title Description Size
Code Composer Studio with MSP430ware Recomended CCS Download
Unlocked MSPWare_2_00_00_41_setup.exe Standalone MSPWare 2.00.00.41. Please see "How to Upgrade?" form above 322468K
MSP430 Driver Library BSD Release of MSP430 Driver Library
MSP432 Driver Library BSD Release of MSP432 Driver Library
MSPWare Documentation
MSPWare Release Notes
md5sum.txt MD5 Checksums 4K
  • For more information:
  • Thu Mar 19 09:13:08 CDT 2015