Build date: 11162017
Release Information
Click on the links in the table below to download.
The MSP debug stack (MSPDS) for all MSP430 and SimpleLink™ MSP432™ devices consists of a static library as well as
embedded firmware that runs on flash emulation tools (FETs) such as the
MSP-FET,
MSP-FET430UIF or
eZ emulators.
It is the bridging element between all PC software and all MSP430 and SimpleLink™ MSP432™ microcontroller derivatives and handles tasks such as
code download, stepping through code, break point handling and so forth. The MSP Debug Stack is used in IDEs such as Code Composer Studio (CCS),
IAR's Embedded Workbench or other tools like Smart RF Studio or Elprotronic's FlashPro430.
Changes in this Release
- New device support: MSP430FR2522, MSP430FR2512, MSP430FR2422
New Features
- Added an option on API level to customize JTAG lock key for 5xx devices - see MSP430_Configure() for more details
- Added support for MSP432 I2C and UART BSL on the MSP-FET
- Showing more detailed progress bar during firmware update
- Added FRAM/Flash overwrite functionality on API level
- Added support for new eZ-FET rev. 2.0 tool
- Switching power supply to on-board LDO on new eZ-FET rev. 2.0 tool while Energy Trace is not used
- Disabling write protection on FRAM devices during memory write access
Bug Fixes
- Fixed a possible race condition during USB communication for eZ430 amd MSP-FET430UIF emulation tool
- Fixed an issue when trying to erase main memory while MPU protection for the vector table is enabled
- Fixed a possible issue when trying to connect to a device which is externally supplied with VCC
- Fixed an issue when trying to erase BSL memory on MSP432 and second info memory on MSP432P4111
- Fixed an issue when backchannel UART is configured to use even parity
- Fixed an issue which prevented warning messages to update properly
- Fixed memory access to TinyRAM
Known Issues
- On devices with FLL, clock control does not allow to keep clocks running, while the device is halted and the clock is sourced by the FLL
- V1.3 of UIF does not work in SBW2 mode with 2.2nf cap on reset line
- eZ-FET UART might lose bytes with 115k baud (no handshake enabled) and DMA as data loopback on target device
- MSP-FET EEM access to F149 and L092 devices is only possible with JTAG speed slow
Older Releases
MSPDS Product downloads
Legend
Fill in Form. Approved users receive download URL in 1 minute.
Fill in Form. TI will contact you in 1-2+ business days.
For more information