MSP430_DLL 3_02_004_005 Product Download Page
Build date: 07132012
The MSP debug stack (MSPDS) for all MSP430 devices consists of a dynamic link library as well as
embedded firmware that runs on flash emulation tools (FETs) such as the MSP-FET,
MSP-FET430UIF or eZ emulators.
It is the bridging element between all PC software and all MSP430 microcontroller derivatives and handles tasks such as
code download, stepping through code, break point handling and so forth. The MSP Debug Stack is used in IDEs such as Code Composer Studio (CCS),
IAR's Embedded Workbench for MSP430 or other tools like Smart RF Studio or Elprotronic's FlashPro430.
Included in
- CCSv5.2.1.00018
- IAR EW430 v5.50.1
New Device Support
MSP430SL5438A, MSP430F6779(1), CC430F5123, CC430F5125, CC430F5143, CC430F5145, CC430F5147, CC430F6143, CC430F6145, CC430F6147, MSP430FR5969, MSP430FR5949 (Wolverine)
New Features
- MPU and IP protection are handled by the DLL on all MSP430FRxx devices -> Access violations will be suppressed by the debugger
- Implemented WriteMemoryQuick() function to write directly into the FRAM memory using JTAG
- Removed write and erase funclets for MSP430FR59xx devices - erase is now handled using the JTAG mailbox, write is done using WriteMemoryQuick()
- Implemented erase mechanism to erase IP protected memory areas without accessing it
- Enhanced USB-FET VCC startup behavior to match the V2 DLL (VCC will be activated when the USB connector of the USB-FET is plugged in)
- Enhanced EEM support (state storage implementation fully functional; implemented cycle counter for counting cycles during a single run)
Bug Fixes
- Corrected DLL database entry for min. flash voltage on 471x devices
- Fixed single stepping issues on L092
- Fixed DCO calibration bug, where the original DCO setting was not restored after debug break (device running slower after read)
- Fixed DLL database entry for the EEM level of the MSP430F5228
- Fixed disassembly window issues on MSP430FR59xx devices
- Fixed issues with fast port close/open
Known Issues
- This MSP430.dll version might not be compatible with revision 1.3 of the MSP-FET430UIF if a capacitor is connected to the RST pin.
Older Releases
2_04_007_001
2_04_008_002
2_04_009_001
3_02_001_009
3_02_003_015
Related Links
|