General Purpose Input/Output to control port settings. More...
Macros | |
#define | GPIO_PORT_P1 1 |
#define | GPIO_PORT_P2 2 |
#define | GPIO_PORT_P3 3 |
#define | GPIO_PORT_P4 4 |
#define | GPIO_PORT_P5 5 |
#define | GPIO_PORT_P6 6 |
#define | GPIO_PORT_P7 7 |
#define | GPIO_PORT_P8 8 |
#define | GPIO_PORT_P9 9 |
#define | GPIO_PORT_P10 10 |
#define | GPIO_PORT_PA 1 |
#define | GPIO_PORT_PB 3 |
#define | GPIO_PORT_PC 5 |
#define | GPIO_PORT_PD 7 |
#define | GPIO_PORT_PE 9 |
#define | GPIO_PORT_PJ 11 |
#define | GPIO_PIN0 (0x0001) |
#define | GPIO_PIN1 (0x0002) |
#define | GPIO_PIN2 (0x0004) |
#define | GPIO_PIN3 (0x0008) |
#define | GPIO_PIN4 (0x0010) |
#define | GPIO_PIN5 (0x0020) |
#define | GPIO_PIN6 (0x0040) |
#define | GPIO_PIN7 (0x0080) |
#define | GPIO_PIN8 (0x0100) |
#define | GPIO_PIN9 (0x0200) |
#define | GPIO_PIN10 (0x0400) |
#define | GPIO_PIN11 (0x0800) |
#define | GPIO_PIN12 (0x1000) |
#define | GPIO_PIN13 (0x2000) |
#define | GPIO_PIN14 (0x4000) |
#define | GPIO_PIN15 (0x8000) |
#define | PIN_ALL8 (0xFF) |
#define | PIN_ALL16 (0xFFFF) |
#define | GPIO_PRIMARY_MODULE_FUNCTION (0x01) |
#define | GPIO_SECONDARY_MODULE_FUNCTION (0x02) |
#define | GPIO_TERTIARY_MODULE_FUNCTION (0x03) |
#define | GPIO_HIGH_TO_LOW_TRANSITION (0x01) |
#define | GPIO_LOW_TO_HIGH_TRANSITION (0x00) |
#define | GPIO_INPUT_PIN_HIGH (0x01) |
#define | GPIO_INPUT_PIN_LOW (0x00) |
#define | GPIO_selectInterruptEdge GPIO_interruptEdgeSelect |
#define | GPIO_clearInterrupt GPIO_clearInterruptFlag |
Functions | |
void | GPIO_setAsOutputPin (uint_fast8_t selectedPort, uint_fast16_t selectedPins) |
This function configures the selected Pin as output pin. More... | |
void | GPIO_setAsInputPin (uint_fast8_t selectedPort, uint_fast16_t selectedPins) |
This function configures the selected Pin as input pin. More... | |
void | GPIO_setAsPeripheralModuleFunctionOutputPin (uint_fast8_t selectedPort, uint_fast16_t selectedPins, uint_fast8_t mode) |
This function configures the peripheral module function in the output direction for the selected pin for either primary, secondary or ternary module function modes. More... | |
void | GPIO_setAsPeripheralModuleFunctionInputPin (uint_fast8_t selectedPort, uint_fast16_t selectedPins, uint_fast8_t mode) |
This function configures the peripheral module function in the input direction for the selected pin for either primary, secondary or ternary module function modes. More... | |
void | GPIO_setOutputHighOnPin (uint_fast8_t selectedPort, uint_fast16_t selectedPins) |
This function sets output HIGH on the selected Pin. More... | |
void | GPIO_setOutputLowOnPin (uint_fast8_t selectedPort, uint_fast16_t selectedPins) |
This function sets output LOW on the selected Pin. More... | |
void | GPIO_toggleOutputOnPin (uint_fast8_t selectedPort, uint_fast16_t selectedPins) |
This function toggles the output on the selected Pin. More... | |
void | GPIO_setAsInputPinWithPullDownResistor (uint_fast8_t selectedPort, uint_fast16_t selectedPins) |
This function sets the selected Pin in input Mode with Pull Down resistor. More... | |
void | GPIO_setAsInputPinWithPullUpResistor (uint_fast8_t selectedPort, uint_fast16_t selectedPins) |
This function sets the selected Pin in input Mode with Pull Up resistor. More... | |
uint8_t | GPIO_getInputPinValue (uint_fast8_t selectedPort, uint_fast16_t selectedPins) |
This function gets the input value on the selected pin. More... | |
void | GPIO_enableInterrupt (uint_fast8_t selectedPort, uint_fast16_t selectedPins) |
This function enables the port interrupt on the selected pin. More... | |
void | GPIO_disableInterrupt (uint_fast8_t selectedPort, uint_fast16_t selectedPins) |
This function disables the port interrupt on the selected pin. More... | |
uint_fast16_t | GPIO_getInterruptStatus (uint_fast8_t selectedPort, uint_fast16_t selectedPins) |
This function gets the interrupt status of the selected pin. More... | |
void | GPIO_clearInterruptFlag (uint_fast8_t selectedPort, uint_fast16_t selectedPins) |
This function clears the interrupt flag on the selected pin. More... | |
void | GPIO_interruptEdgeSelect (uint_fast8_t selectedPort, uint_fast16_t selectedPins, uint_fast8_t edgeSelect) |
This function selects on what edge the port interrupt flag should be set for a transition. More... | |
uint_fast16_t | GPIO_getEnabledInterruptStatus (uint_fast8_t selectedPort) |
This function gets the interrupt status of the provided PIN and masks it with the interrupts that are actually enabled. This is useful for inside ISRs where the status of only the enabled interrupts needs to be checked. More... | |
void | GPIO_registerInterrupt (uint_fast8_t selectedPort, void(*intHandler)(void)) |
void | GPIO_unregisterInterrupt (uint_fast8_t selectedPort) |
void | GPIO_setDriveStrengthHigh (uint_fast8_t selectedPort, uint_fast8_t selectedPins) |
void | GPIO_setDriveStrengthLow (uint_fast8_t selectedPort, uint_fast8_t selectedPins) |
General Purpose Input/Output to control port settings.
Devices within the family may have up to twelve digital I/O ports implemented (P1 to P11 and PJ). Most ports contain eight I/O lines; however, some ports may contain less (see the device-specific data sheet for ports available). Each I/O line is individually configurable for input or output direction, and each can be individually read or written. Each I/O line is individually configurable for pullup or pulldown resistors. PJ contains only four I/O lines.
Individual ports can be accessed as byte-wide ports or can be combined into word-wide ports and accessed via word formats. Port pairs P1/P2, P3/P4, P5/P6, P7/P8, etc., are associated with the names PA, PB, PC, PD, etc., respectively. All port registers are handled in this manner with this naming convention.
When writing to port PA with word operations, all 16 bits are written to the port. When writing to the lower byte of the PA port using byte operations, the upper byte remains unchanged. Similarly, writing to the upper byte of the PA port using byte instructions leaves the lower byte unchanged. When writing to a port that contains less than the maximum number of bits possible, the unused bits are a "don't care". Ports PB, PC, PD, PE, and PF behave similarly.
Reading of the PA port using word operations causes all 16 bits to be transferred to the destination. Reading the lower or upper byte of the PA port (P1 or P2) and storing to memory using byte operations causes only the lower or upper byte to be transferred to the destination, respectively. Reading of the PA port and storing to a general-purpose register using byte operations causes the byte transferred to be written to the least significant byte of the register. The upper significant byte of the destination register is cleared automatically. Ports PB, PC, PD, PE, and PF behave similarly. When reading from ports that contain less than the maximum bits possible, unused bits are read as zeros (similarly for port PJ).
The GPIO pin may be configured as an I/O pin with GPIO_setAsOutputPin, GPIO_setAsInputPin, GPIO_setAsInputPinWithPullDownResistor or GPIO_setAsInputPinWithPullUpResistor . The GPIO pin may instead be configured to operate in the Peripheral Module assigned function by configuring the GPIO using GPIO_setAsPeripheralModuleFunctionOutputPin or GPIO_setAsPeripheralModuleFunctionInputPin.
Below is a simple example of how to set up a GPIO in output mode and toggle an LED using a simple delay:
#define GPIO_PORT_P1 1 |
Referenced by GPIO_getEnabledInterruptStatus().
#define GPIO_PORT_P2 2 |
Referenced by GPIO_getEnabledInterruptStatus().
#define GPIO_PORT_P3 3 |
Referenced by GPIO_getEnabledInterruptStatus().
#define GPIO_PORT_P4 4 |
Referenced by GPIO_getEnabledInterruptStatus().
#define GPIO_PORT_P5 5 |
Referenced by GPIO_getEnabledInterruptStatus().
#define GPIO_PORT_P6 6 |
Referenced by GPIO_getEnabledInterruptStatus().
#define GPIO_PORT_P7 7 |
Referenced by GPIO_getEnabledInterruptStatus().
#define GPIO_PORT_P8 8 |
Referenced by GPIO_getEnabledInterruptStatus().
#define GPIO_PORT_P9 9 |
Referenced by GPIO_getEnabledInterruptStatus().
#define GPIO_PORT_P10 10 |
Referenced by GPIO_getEnabledInterruptStatus().
#define GPIO_PORT_PA 1 |
#define GPIO_PORT_PB 3 |
#define GPIO_PORT_PC 5 |
#define GPIO_PORT_PD 7 |
#define GPIO_PORT_PE 9 |
#define GPIO_PORT_PJ 11 |
Referenced by GPIO_getEnabledInterruptStatus().
#define GPIO_PIN0 (0x0001) |
#define GPIO_PIN1 (0x0002) |
#define GPIO_PIN2 (0x0004) |
#define GPIO_PIN3 (0x0008) |
#define GPIO_PIN4 (0x0010) |
#define GPIO_PIN5 (0x0020) |
#define GPIO_PIN6 (0x0040) |
#define GPIO_PIN7 (0x0080) |
#define GPIO_PIN8 (0x0100) |
#define GPIO_PIN9 (0x0200) |
#define GPIO_PIN10 (0x0400) |
#define GPIO_PIN11 (0x0800) |
#define GPIO_PIN12 (0x1000) |
#define GPIO_PIN13 (0x2000) |
#define GPIO_PIN14 (0x4000) |
#define GPIO_PIN15 (0x8000) |
#define PIN_ALL8 (0xFF) |
#define PIN_ALL16 (0xFFFF) |
#define GPIO_PRIMARY_MODULE_FUNCTION (0x01) |
#define GPIO_SECONDARY_MODULE_FUNCTION (0x02) |
#define GPIO_TERTIARY_MODULE_FUNCTION (0x03) |
#define GPIO_HIGH_TO_LOW_TRANSITION (0x01) |
#define GPIO_LOW_TO_HIGH_TRANSITION (0x00) |
Referenced by GPIO_interruptEdgeSelect().
#define GPIO_INPUT_PIN_HIGH (0x01) |
Referenced by GPIO_getInputPinValue().
#define GPIO_INPUT_PIN_LOW (0x00) |
Referenced by GPIO_getInputPinValue().
#define GPIO_selectInterruptEdge GPIO_interruptEdgeSelect |
#define GPIO_clearInterrupt GPIO_clearInterruptFlag |
void GPIO_setAsOutputPin | ( | uint_fast8_t | selectedPort, |
uint_fast16_t | selectedPins | ||
) |
This function configures the selected Pin as output pin.
This function selected pins on a selected port as output pins.
selectedPort | is the selected port. Valid values are:
|
selectedPins | is the specified pin in the selected port. Mask value is the logical OR of any of the following:
|
Modified bits of PxDIR register and bits of PxSEL register.
References HWREG16, OFS_LIB_PADIR, OFS_LIB_PASEL0, and OFS_LIB_PASEL1.
void GPIO_setAsInputPin | ( | uint_fast8_t | selectedPort, |
uint_fast16_t | selectedPins | ||
) |
This function configures the selected Pin as input pin.
This function selected pins on a selected port as input pins.
selectedPort | is the selected port. Valid values are:
|
selectedPins | is the specified pin in the selected port. Mask value is the logical OR of any of the following:
|
Modified bits of PxDIR register, bits of PxREN register and bits of PxSEL register.
References HWREG16, OFS_LIB_PADIR, OFS_LIB_PAREN, OFS_LIB_PASEL0, and OFS_LIB_PASEL1.
void GPIO_setAsPeripheralModuleFunctionOutputPin | ( | uint_fast8_t | selectedPort, |
uint_fast16_t | selectedPins, | ||
uint_fast8_t | mode | ||
) |
This function configures the peripheral module function in the output direction for the selected pin for either primary, secondary or ternary module function modes.
This function configures the peripheral module function in the output direction for the selected pin for either primary, secondary or ternary module function modes. Accepted values for mode are GPIO_PRIMARY_MODULE_FUNCTION, GPIO_SECONDARY_MODULE_FUNCTION, and GPIO_TERTIARY_MODULE_FUNCTION
selectedPort | is the selected port. Valid values are:
|
selectedPins | is the specified pin in the selected port. Mask value is the logical OR of any of the following:
|
mode | is the specified mode that the pin should be configured for the module function. Valid values are:
|
Modified bits of PxDIR register and bits of PxSEL register.
References GPIO_PRIMARY_MODULE_FUNCTION, GPIO_SECONDARY_MODULE_FUNCTION, GPIO_TERTIARY_MODULE_FUNCTION, HWREG16, OFS_LIB_PADIR, OFS_LIB_PASEL0, and OFS_LIB_PASEL1.
void GPIO_setAsPeripheralModuleFunctionInputPin | ( | uint_fast8_t | selectedPort, |
uint_fast16_t | selectedPins, | ||
uint_fast8_t | mode | ||
) |
This function configures the peripheral module function in the input direction for the selected pin for either primary, secondary or ternary module function modes.
This function configures the peripheral module function in the input direction for the selected pin for either primary, secondary or ternary module function modes. Accepted values for mode are GPIO_PRIMARY_MODULE_FUNCTION, GPIO_SECONDARY_MODULE_FUNCTION, and GPIO_TERTIARY_MODULE_FUNCTION
selectedPort | is the selected port. Valid values are:
|
selectedPins | is the specified pin in the selected port. Mask value is the logical OR of any of the following:
|
mode | is the specified mode that the pin should be configured for the module function. Valid values are:
|
Modified bits of PxDIR register and bits of PxSEL register.
References GPIO_PRIMARY_MODULE_FUNCTION, GPIO_SECONDARY_MODULE_FUNCTION, GPIO_TERTIARY_MODULE_FUNCTION, HWREG16, OFS_LIB_PADIR, OFS_LIB_PASEL0, and OFS_LIB_PASEL1.
void GPIO_setOutputHighOnPin | ( | uint_fast8_t | selectedPort, |
uint_fast16_t | selectedPins | ||
) |
This function sets output HIGH on the selected Pin.
This function sets output HIGH on the selected port's pin.
selectedPort | is the selected port. Valid values are:
|
selectedPins | is the specified pin in the selected port. Mask value is the logical OR of any of the following:
|
Modified bits of PxOUT register.
References HWREG16, and OFS_LIB_PAOUT.
void GPIO_setOutputLowOnPin | ( | uint_fast8_t | selectedPort, |
uint_fast16_t | selectedPins | ||
) |
This function sets output LOW on the selected Pin.
This function sets output LOW on the selected port's pin.
selectedPort | is the selected port. Valid values are:
|
selectedPins | is the specified pin in the selected port. Mask value is the logical OR of any of the following:
|
References HWREG16, and OFS_LIB_PAOUT.
void GPIO_toggleOutputOnPin | ( | uint_fast8_t | selectedPort, |
uint_fast16_t | selectedPins | ||
) |
This function toggles the output on the selected Pin.
This function toggles the output on the selected port's pin.
selectedPort | is the selected port. Valid values are:
|
selectedPins | is the specified pin in the selected port. Mask value is the logical OR of any of the following:
|
Modified bits of PxOUT register.
References HWREG16, and OFS_LIB_PAOUT.
void GPIO_setAsInputPinWithPullDownResistor | ( | uint_fast8_t | selectedPort, |
uint_fast16_t | selectedPins | ||
) |
This function sets the selected Pin in input Mode with Pull Down resistor.
This function sets the selected Pin in input Mode with Pull Down resistor.
selectedPort | is the selected port. Valid values are:
|
selectedPins | is the specified pin in the selected port. Mask value is the logical OR of any of the following:
|
Modified bits of PxDIR register, bits of PxOUT register and bits of PxREN register.
References HWREG16, OFS_LIB_PADIR, OFS_LIB_PAOUT, OFS_LIB_PAREN, OFS_LIB_PASEL0, and OFS_LIB_PASEL1.
void GPIO_setAsInputPinWithPullUpResistor | ( | uint_fast8_t | selectedPort, |
uint_fast16_t | selectedPins | ||
) |
This function sets the selected Pin in input Mode with Pull Up resistor.
This function sets the selected Pin in input Mode with Pull Up resistor.
selectedPort | is the selected port. Valid values are:
|
selectedPins | is the specified pin in the selected port. Mask value is the logical OR of any of the following:
|
Modified bits of PxDIR register, bits of PxOUT register and bits of PxREN register.
References HWREG16, OFS_LIB_PADIR, OFS_LIB_PAOUT, OFS_LIB_PAREN, OFS_LIB_PASEL0, and OFS_LIB_PASEL1.
uint8_t GPIO_getInputPinValue | ( | uint_fast8_t | selectedPort, |
uint_fast16_t | selectedPins | ||
) |
This function gets the input value on the selected pin.
This function gets the input value on the selected pin.
selectedPort | is the selected port. Valid values are:
|
selectedPins | is the specified pin in the selected port. Valid values are:
|
References GPIO_INPUT_PIN_HIGH, GPIO_INPUT_PIN_LOW, HWREG16, and OFS_LIB_PAIN.
void GPIO_enableInterrupt | ( | uint_fast8_t | selectedPort, |
uint_fast16_t | selectedPins | ||
) |
This function enables the port interrupt on the selected pin.
This function enables the port interrupt on the selected pin. Note that only Port 1,2, A have this capability.
selectedPort | is the selected port. Valid values are:
|
selectedPins | is the specified pin in the selected port. Mask value is the logical OR of any of the following:
|
Modified bits of PxIE register.
References HWREG16, and OFS_LIB_PAIE.
void GPIO_disableInterrupt | ( | uint_fast8_t | selectedPort, |
uint_fast16_t | selectedPins | ||
) |
This function disables the port interrupt on the selected pin.
This function disables the port interrupt on the selected pin. Note that only Port 1,2, A have this capability.
selectedPort | is the selected port. Valid values are:
|
selectedPins | is the specified pin in the selected port. Mask value is the logical OR of any of the following:
|
Modified bits of PxIE register.
References HWREG16, and OFS_LIB_PAIE.
uint_fast16_t GPIO_getInterruptStatus | ( | uint_fast8_t | selectedPort, |
uint_fast16_t | selectedPins | ||
) |
This function gets the interrupt status of the selected pin.
This function gets the interrupt status of the selected pin. Note that only Port 1,2, A have this capability.
selectedPort | is the selected port. Valid values are:
|
selectedPins | is the specified pin in the selected port. Mask value is the logical OR of any of the following:
|
References HWREG16, and OFS_LIB_PAIFG.
Referenced by GPIO_getEnabledInterruptStatus().
void GPIO_clearInterruptFlag | ( | uint_fast8_t | selectedPort, |
uint_fast16_t | selectedPins | ||
) |
This function clears the interrupt flag on the selected pin.
This function clears the interrupt flag on the selected pin. Note that only Port 1,2,A have this capability.
selectedPort | is the selected port. Valid values are:
|
selectedPins | is the specified pin in the selected port. Mask value is the logical OR of any of the following:
|
Modified bits of PxIFG register.
References HWREG16, and OFS_LIB_PAIFG.
void GPIO_interruptEdgeSelect | ( | uint_fast8_t | selectedPort, |
uint_fast16_t | selectedPins, | ||
uint_fast8_t | edgeSelect | ||
) |
This function selects on what edge the port interrupt flag should be set for a transition.
This function selects on what edge the port interrupt flag should be set for a transition. Values for edgeSelect should be GPIO_LOW_TO_HIGH_TRANSITION or GPIO_HIGH_TO_LOW_TRANSITION.
selectedPort | is the selected port. Valid values are:
|
selectedPins | is the specified pin in the selected port. Mask value is the logical OR of any of the following:
|
edgeSelect | specifies what transition sets the interrupt flag Valid values are:
|
Modified bits of PxIES register.
References GPIO_LOW_TO_HIGH_TRANSITION, HWREG16, and OFS_LIB_PAIES.
uint_fast16_t GPIO_getEnabledInterruptStatus | ( | uint_fast8_t | selectedPort | ) |
This function gets the interrupt status of the provided PIN and masks it with the interrupts that are actually enabled. This is useful for inside ISRs where the status of only the enabled interrupts needs to be checked.
selectedPort | is the selected port. Valid values are:
|
References ASSERT, GPIO_getInterruptStatus(), GPIO_PORT_P1, GPIO_PORT_P10, GPIO_PORT_P2, GPIO_PORT_P3, GPIO_PORT_P4, GPIO_PORT_P5, GPIO_PORT_P6, GPIO_PORT_P7, GPIO_PORT_P8, GPIO_PORT_P9, GPIO_PORT_PJ, HWREG16, HWREG8, OFS_LIB_P1IE, OFS_LIB_P2IE, and OFS_LIB_PAIE.
void GPIO_registerInterrupt | ( | uint_fast8_t | selectedPort, |
void(*)(void) | intHandler | ||
) |
Registers an interrupt handler for the port interrupt.
selectedPort | is the port to register the interrupt handler |
intHandler | is a pointer to the function to be called when the port interrupt occurs. |
This function registers the handler to be called when a port interrupt occurs. This function enables the global interrupt in the interrupt controller; specific GPIO interrupts must be enabled via GPIO_enableInterrupt(). It is the interrupt handler's responsibility to clear the interrupt source via GPIO_clearInterruptFlag().
Clock System can generate interrupts when
References Interrupt_enableInterrupt(), and Interrupt_registerInterrupt().
void GPIO_unregisterInterrupt | ( | uint_fast8_t | selectedPort | ) |
Unregisters the interrupt handler for the port.
selectedPort | is the port to unregister the interrupt handler |
This function unregisters the handler to be called when a port interrupt occurs. This function also masks off the interrupt in the interrupt controller so that the interrupt handler no longer is called.
References Interrupt_disableInterrupt(), and Interrupt_unregisterInterrupt().
void GPIO_setDriveStrengthHigh | ( | uint_fast8_t | selectedPort, |
uint_fast8_t | selectedPins | ||
) |
This function sets the drive strength to high for the selected port
selectedPort | is the selected port. Valid values are:
|
selectedPins | is the specified pin in the selected port. Valid values are:
|
References HWREG8, and OFS_LIB_PADS.
void GPIO_setDriveStrengthLow | ( | uint_fast8_t | selectedPort, |
uint_fast8_t | selectedPins | ||
) |
This function sets the drive strength to low for the selected port
selectedPort | is the selected port. Valid values are:
|
selectedPins | is the specified pin in the selected port. Valid values are:
|
References HWREG8, and OFS_LIB_PADS.