Build date: 02022016
MSP432 Driver Library is a collection of high level APIs that speed up software development for MSP432. The MSP432 Driver Library package includes API documentaion and examples to help you get started.
This release of MSP432 Driver Library supports all of the following device families:
MSP432 Driver Library is available as a standalone BSD released package. To use the library simply download and unzip the package below. Please read the included user's guide to learn about adding driver library to a new or existing project.
MSP432 Driver Library is also released as a component of MSPWare. You can import and run examples from driver library from the TI Resouce Explorer GUI within the Code Composer Studio (CCS) window when you have MSPWare installed. For more information about MSPWare check the table below for a link to the latest version.
What is the difference between MSPWare and Driver Library?MSPWare is a collection of MSP430 and MSP432 software and tools. One of the main components of MSPWare is Driver Library (DriverLib).
Why are there multiple driverlib folders within MSPWare?MSPWare contains many different software libraries and projects. Some of these components depend on a specific version of Driver Library. Each component ships the version of Driver Library they tested with to ensure that all software works for you out of the box.
Can I have multiple versions of MSPWare installed?Yes! MSPWare installations can exist alongside each other. You should only see the latest installed version within the TI Resource Explorer window of Code Composer Studio however.
How can I get support for MSPWare?Feel free to use the TI E2E forum to ask anything MSPWare related.
Title | Description | Size | |
---|---|---|---|
MSP432_DriverLib_3_10_00_09.zip | BSD Licensed Driver Library | 10596K | |
Code Composer Studio | Recommended CCS Download | ||
MSPWare | Recommended MSPWare Download | ||
MSP430 Driver Library | BSD Licensed Driver Library for MSP430 | ||
MSP432 Driver Library Documentation | |||
MSP432 Driver Library Release Notes | |||
MSP432 Driver Library MSP432P4xx | |||
MSP432 Driver Library MSP432P4xx API Guide | |||
MSP432 Driver Library MSP432P4xx Users Guide | 888K | ||
md5sum.txt | MD5 Checksums | 4K |
Fill in Form. Approved users receive download URL in 1 minute.
Fill in Form. TI will contact you in 1-2+ business days.