Macros | Functions
pmap.h File Reference
#include <stdint.h>
#include <msp.h>

Go to the source code of this file.

Macros

#define PMAP_ENABLE_RECONFIGURATION   PMAP_CTL_PRECFG
 
#define PMAP_DISABLE_RECONFIGURATION   0x00
 
#define PMAP_P1MAP   ((uint32_t)P1MAP - PMAP_BASE)
 
#define PMAP_P2MAP   ((uint32_t)P2MAP - PMAP_BASE)
 
#define PMAP_P3MAP   ((uint32_t)P3MAP - PMAP_BASE)
 
#define PMAP_P4MAP   ((uint32_t)P4MAP - PMAP_BASE)
 
#define PMAP_P5MAP   ((uint32_t)P5MAP - PMAP_BASE)
 
#define PMAP_P6MAP   ((uint32_t)P6MAP - PMAP_BASE)
 
#define PMAP_P7MAP   ((uint32_t)P7MAP - PMAP_BASE)
 
#define PMAP_configurePortsMultipleInstance(a, b, c, d, e)   PMAP_configurePorts(b,c,d,e)
 

Functions

void PMAP_configurePorts (const uint8_t *portMapping, uint8_t pxMAPy, uint8_t numberOfPorts, uint8_t portMapReconfigure)
 

Copyright 2015, Texas Instruments Incorporated