Texas Instruments

MSP432 DriverLib  3_21_00_05

Release Notes 

Document Revision: 012116.0051

Introduction

Set of development tools used for programming, configuring, and utilizing MSP432 devices.

This document is divided into the following sections:

Documentation

  • MSP432 Driver Library API Guide
  • What's New

    Milestone Release (03_21_00_xx)

    Milestone Release (03_10_00_xx)

    Milestone Release (01.04.00.18) Major CS Release

    Incremental Release (01.04.00.17 ) RC3

    Incremental Release (01.04.00.16 ) RC2

    Incremental Release (01.04.00.15 ) RC1

    Incremental Release (01.04.00.14 )

    Incremental Release (01.04.00.12 )

    Incremental Release (01.04.00.11 )

    Internal Tools Release (01.04.00.10 )

    Incremental Release (01.04.00.09 )

    Incremental Release (01.04.00.05 )

    Incremental Release (01.04.00.04 )

    Major ES2 Release (01.03.00.17 )

    Major ES Release (01.02.00.36 )

    RC3 Release (01.02.00.35 )

    RC2 Release (01.02.00.34 )

    RC1 Release (01.02.00.33 )

    Incremental Release (01.02.00.32 )

    Incremental Release (01.02.00.31 )

    Incremental Release (01.02.00.30 )

    Incremental Release (01.02.00.29 )

    Incremental Release (01.02.00.28 )

    Incremental Release (01.02.00.27 )

    Incremental Release (01.02.00.26 )

    Incremental Release (01.02.00.25 )

    Incremental Release (01.02.00.24 )

    Incremental Release (01.02.00.23 )

    Incremental Release (01.02.00.22 )

    Incremental Release (01.02.00.21 )

    Incremental Release (01.02.00.20 )

    Incremental Release (01.02.00.19 )

    Incremental Release (01.02.00.18 )

    Incremental Release (01.02.00.17 )

    Incremental Release (01.02.00.16)

    Incremental Release (01.02.00.15)

    Incremental Release (01.02.00.14)

    Incremental Release (01.02.00.12)

    Incremental Release (01.02.00.11)

    Incremental Release (01.02.00.09)

    Incremental Release (01.02.00.07)

    Incremental Release (01.02.00.06)

    Major Release (1.01.00.22)

    The MSP432 DriverLib  release contains the following components:
    doc API Guides and documentation 
    driverlib  MSP432 peripheral driver library
    examples  Examples on how to use the various components of MSP432
    inc Device specific include files

    Installation and Usage

    Download and unzip the zip file. For more information on how to use the peripheral driver library  please refer to the DriverLib API Guide.

    Upgrade Information

    To upgrade from previous versions of MSP432 Driver Library, simply delete all old instances of components used and replace with the new components

    Device Support

    This release supports the Texas Instruments MSP432  device family.

    The peripheral driver library has been built for the toolchains in the following chart. When toolchain debugging support is available, the  library has been tested with the specified debugger. Although tested with a specific debugger,  code examples and the driver library will work on a variety of different debuggers.

    Toolchain Debugger
    Texas Instruments Code Composer Studio 6.0   XDS100v3
    IAR Embedded Workbench for ARM 7.20 SEGGER J-LINK
    GNU C Compiler 4.8 (gcc) SEGGER J-LINK
    Keil Embedded Development Tools for ARM 5.11 KEIL U-LINK Pro

    Validation Information

    This release is a beta version with initial rounds of validation performed. 

    Known Issues

    Versioning

    This is build 3_21_00_05 of MSP432 DriverLib

    Technical Support and Product Updates

    Support

    Additional Resources

    For more information, visit www.ti.com.