------------Capacitive Touch Library and Getting Started Guide------------------ July 2014 Texas Instruments, Inc. -------------------------------------------------------------------------------- CONTENTS I. Library II. Code_Examples III. Documentation IV. Example_Projects I. Library ----------------------------------- The following files are found in the Library directory: CTS_HAL.c CTS_HAL.h CTS_Layer.c CTS_Layer.h II. Code_Examples ----------------------------------- The following example directories include a main application file and configuration files structure.c/.h. These files are used with the files found in the source directory. The element definition found in the configuration file structure.c uses a designated initializer list. This allows members to be initialized in any order and also enhances the readability of the element being initialized. This feature requires the GCC language extension found in Code Composer Studio (CCS). C99 is the default dialect found in IAR and therefore the default settings can be used. fRO_COMPAp_SW_TA0 fRO_COMPAp_TA0_SW fRO_COMPB_TA1_TA0 fRO_CSIO_TA0_SW fRO_CSIO_TA0_TA1 fRO_CSIO_TA2_TA3 fRO_PINOSC_TA0_SW fRO_PINOSC_TA0_TA1 fRO_PINOSC_TA1_TA0 fRO_PINOSC_TA1_TB0 RC_PAIR_TA0 RO_COMPAp_TA0_WDTp RO_COMPB_TA1_TA0 RO_COMPB_TA1_WDTA RO_COMPB_TB0_WDTA RO_CSIO_TA0_RTC RO_CSIO_TA0_TA1 RO_CSIO_TA0_WDTA RO_CSIO_TA2_TA3 RO_CSIO_TA2_WDTA RO_PINOSC_TA0 RO_PINOSC_TA0_TA1 RO_PINOSC_TA0_WDTp RO_PINOSC_TA1_WDTp RO_PINOSC_TA1_TB0 III. Documentation ----------------------------------- Doxygen for the files found in the Library directory. IV. Example_Projects ----------------------------------- Eight projects for both IAR and CCS. The C source code is found in the Source sub-directory. Both the CCS and IAR projects link to the Library directory.