CapTIvate Design Center Release Notes
Table of Contents
Introduction
This is version 1.50.00.00 of CapTIvate Design Center.
CapTIvate™ is a capacitive user interface design ecosystem that takes the next big step in design process evolution. It brings together a capacitive measurement technology, a design GUI, a capacitive touch software library, and a hardware development platform.
Documentation
What’s New
Documentation
-
Software Library
Design Center
1.50.00.00
ID | Summary |
---|---|
MSPCAPLIB-158 | Add Metal Touch examples and documentation updates |
MSPCAPLIB-150 | Change “PARALLEL BLOCK” column heading to “PARALLEL GROUP” |
MSPCAPLIB-138 | DesignCenter shall be modfied to use the documentation tools from SimpleLink SDK SWTOOLS |
Upgrade and Compatibility Information
No special action is required to upgrade to this release.
Installation and Usage
- Download CapTIvate
- Run the appropriate platform specific installer: CapTIvateDesignCenter-
- -installer - Follow the installer directions
- To launch tool, use the desktop icon or execute the tool directly:
- Windows
- Start Menu -> All Programs -> Texas Instruments -> CapTIvateDesignCenter_<version> -> CapTIvateDesignCenter
- C:/ti/msp/CapTIvateDesignCenter_<version>/CapTIvateDesignCenter.exe
- OS X
- /Applications/ti/msp/CapTIvateDesignCenter_<version>/CapTIvateDesignCenter
- Linux OS
- ~/ti/msp/CapTIvateDesignCenter_<version>/CapTIvateDesignCenter
- Windows
Host Support
Supported Operating Systems:
- Windows 7, 10
- Linux OS
- Apple OS X
Dependencies
Java JRE 1.7 or later must be installed on the host system. Click here to go to Java Download Page.
- Source code generated by this release requires:
- Code Composer Studio (CCS) v6.1.0 or higher
- IAR Embedded Workbench 6.30.1 or higher
Device Support
The following families of devices are supported in this release of CapTIvate Design Center:
- MSP430FR2532, MSP430FR2533
- MSP430FR2632, MSP430FR2633
Validation Information
The CapTIvate Design Center was validated with the following components:
Code Composer Studio 6.1.3.0 or higher IAR Embedded Workbench 6.30.1 or higher
Known Issues
ID | Summary |
---|---|
None | None |
Versioning
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
Prior Release Changes
- 1.40.00.00
- Minimum Java requirement changed to 1.7.0_60
- Add “SetAll” button to element tuning parameter widgets (MSPCAPLIB-126)
- Add confirmation dialog when the target directory of code generation exists (MSPCAPLIB-129)
- Documentation updates
- Minor bug fixes
- v1.30.10.00
- Updated to CapTIvate Software Library v1.04.00.00
- Added support for using the VLO to clock the CapTIvate timer in LPM4 when in wake-on-proximity mode to the CAPT_App layer. This allows applications to achieve very low average power consumption when a crystal is not used for the low frequency clock (ACLK). Entering LPM4 disables ACLK (turning of XT1 or the REFO, whichever was used for ACLK). The CapTIvate peripheral may still be clocked from the VLO in LPM4, if the VLO is selected as the clock source. The trade-off with using this mode is reduced time-keeping accuracy in wake-on-proximity mode. To enable this feature, define CAPT_WOP_VLO_LPM4 in CAPT_App.c. For more details, see the Ultra Low Power section of the Design Guide chapter of the CapTIvate Technology Guide.
- Added the ProximityRangeSensor example project. This example project shows how to implement a basic range sensing application using the CAPTIVATE-PROXIMITY sensing panel.
- The MSP peripheral driver library is updated to include support for the DCO manual trim procedure.
- The CapTIvate Starter Project default stack size was reduced to 256B from 512B. Testing estimates the worst case stack usage for most applications to be <128B.
- Documentation updates
- Updated to CapTIvate Software Library v1.04.00.00
- v1.20.00.00
- Documentation updates
- Minor bug fixes
- v1.10.00.00
- Documentation updates
- Fix intermittent GUI startup issues
- Other minor bug fixes
- v1.00.20.00
- Initial public ES release
Technical Support and Product Updates
- Visit the MSP E2E Forum for support.