Contains the SD24 Configuration. More...
#include <hal_adc_sd24.h>
Data Fields | |
uint16_t | overSampleRatio |
uint16_t | sampleFreq |
uint8_t | referenceSelect |
uint8_t | masterConverter |
HAL_ADC_SD24_Channel * | adcChannelPtr |
The highest converter used to start / stop conversions. More... | |
uint8_t | adcChannelLength |
Pointer to the location where the channel configuration is stored. More... | |
Contains the SD24 Configuration.
uint16_t _HAL_ADC_SD24_Configuration_::overSampleRatio |
uint16_t _HAL_ADC_SD24_Configuration_::sampleFreq |
Selects oversampling ratio for the converter
Valid values are:
uint8_t _HAL_ADC_SD24_Configuration_::referenceSelect |
uint8_t _HAL_ADC_SD24_Configuration_::masterConverter |
Selects the reference source for the SD24 core
Valid values are:
HAL_ADC_SD24_Channel* _HAL_ADC_SD24_Configuration_::adcChannelPtr |
The highest converter used to start / stop conversions.
uint8_t _HAL_ADC_SD24_Configuration_::adcChannelLength |
Pointer to the location where the channel configuration is stored.