Data Fields
_EM_SW_Lib_Result_Handle_ Struct Reference

Contains EM SW Lib Result Handle. More...

#include <emSwLib.h>

Collaboration diagram for _EM_SW_Lib_Result_Handle_:
Collaboration graph
[legend]

Data Fields

EM_Total_ResultsemTotalResult
 Pointer to EM_Total_Results struct. More...
 
EM_Phase_ResultsphaseResults
 Pointer to EM_Phase_Result struct buffer. More...
 
EM_Phase_BG_ResultsphaseBGResults
 Pointer to the EM_Phase_BG_Results struct buffer. More...
 
EM_Metrology ** phaseMetrologyPing
 Pointer to EM_Metrology struct Ping buffer. More...
 
EM_Metrology ** phaseMetrologyPong
 Pointer to EM_Metrology struct Pong buffer. More...
 
uint8_t phaseResultsSupportedLen
 Length of the phaseResultsSupportedPtr buffer. More...
 

Detailed Description

Contains EM SW Lib Result Handle.

Field Documentation

§ emTotalResult

EM_Total_Results* _EM_SW_Lib_Result_Handle_::emTotalResult

Pointer to EM_Total_Results struct.

§ phaseResults

EM_Phase_Results* _EM_SW_Lib_Result_Handle_::phaseResults

Pointer to EM_Phase_Result struct buffer.

§ phaseBGResults

EM_Phase_BG_Results* _EM_SW_Lib_Result_Handle_::phaseBGResults

Pointer to the EM_Phase_BG_Results struct buffer.

§ phaseMetrologyPing

EM_Metrology** _EM_SW_Lib_Result_Handle_::phaseMetrologyPing

Pointer to EM_Metrology struct Ping buffer.

§ phaseMetrologyPong

EM_Metrology** _EM_SW_Lib_Result_Handle_::phaseMetrologyPong

Pointer to EM_Metrology struct Pong buffer.

§ phaseResultsSupportedLen

uint8_t _EM_SW_Lib_Result_Handle_::phaseResultsSupportedLen

Length of the phaseResultsSupportedPtr buffer.


The documentation for this struct was generated from the following file:
© Copyright 1995-2018, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale