Contains EM Phase Result. More...
#include <emSwLib.h>
Data Fields | |
uint32_t | VRMS |
VRMS for previous frame (mV) More... | |
uint32_t | IRMS |
IRMS for previous frame (uA) More... | |
uint32_t | vPeak |
VPeak since system initialization (mV) More... | |
uint32_t | iPeak |
IPeak since system initialization (uA) More... | |
int32_t | powerFactor |
Power Factor calculated when the EM_powerFactor. More... | |
uint16_t | frequency |
EM_Power_t | activePower |
Active Power for previous frame (uW) More... | |
EM_Power_t | reactivePower |
Reactive Power for previous frame (uVAr) More... | |
EM_Power_t | apparentPower |
Apparent Power for previous frame (uVA) More... | |
EM_Energy_t | activeEnergy |
Active Energy for previous frame (uWh) More... | |
EM_Energy_t | reactiveEnergy |
Reactive Energy for previous frame (uVArh) More... | |
EM_Energy_t | apparentEnergy |
Apparent Energy for previous frame (uVAh) More... | |
EM_Phase | phaseID |
Present Phase ID Name. More... | |
Contains EM Phase Result.
uint32_t _EM_Phase_Results_::VRMS |
VRMS for previous frame (mV)
uint32_t _EM_Phase_Results_::IRMS |
IRMS for previous frame (uA)
uint32_t _EM_Phase_Results_::vPeak |
VPeak since system initialization (mV)
uint32_t _EM_Phase_Results_::iPeak |
IPeak since system initialization (uA)
int32_t _EM_Phase_Results_::powerFactor |
Power Factor calculated when the EM_powerFactor.
uint16_t _EM_Phase_Results_::frequency |
The Frequency is stored in 0.01Hz steps. A 16 bit unsigned number supports the range 0.01Hz to 655.35Hz, which is clearly more than we will ever need for the fundamental.
EM_Power_t _EM_Phase_Results_::activePower |
Active Power for previous frame (uW)
EM_Power_t _EM_Phase_Results_::reactivePower |
Reactive Power for previous frame (uVAr)
EM_Power_t _EM_Phase_Results_::apparentPower |
Apparent Power for previous frame (uVA)
EM_Energy_t _EM_Phase_Results_::activeEnergy |
Active Energy for previous frame (uWh)
EM_Energy_t _EM_Phase_Results_::reactiveEnergy |
Reactive Energy for previous frame (uVArh)
EM_Energy_t _EM_Phase_Results_::apparentEnergy |
Apparent Energy for previous frame (uVAh)
EM_Phase _EM_Phase_Results_::phaseID |
Present Phase ID Name.