Data Fields
_EM_Phase_Calibration_ Struct Reference

Contains EM SW Lib Phase Calibration. More...

#include <emSwLib.h>

Data Fields

uint32_t voltageSF
 Voltage Scaling Factor - used to calculate VRMS. More...
 
uint32_t currentSF
 Current Scaling Factor - used to calculate IRMS. More...
 
uint32_t activePowerSF
 Active Power Scaling Factor. More...
 
uint32_t reactivePowerSF
 Active Power Scaling Factor. More...
 
int16_t phaseCorrection
 Phase Correction between voltage and current (register units) More...
 

Detailed Description

Contains EM SW Lib Phase Calibration.

Field Documentation

§ voltageSF

uint32_t _EM_Phase_Calibration_::voltageSF

Voltage Scaling Factor - used to calculate VRMS.

§ currentSF

uint32_t _EM_Phase_Calibration_::currentSF

Current Scaling Factor - used to calculate IRMS.

§ activePowerSF

uint32_t _EM_Phase_Calibration_::activePowerSF

Active Power Scaling Factor.

§ reactivePowerSF

uint32_t _EM_Phase_Calibration_::reactivePowerSF

Active Power Scaling Factor.

§ phaseCorrection

int16_t _EM_Phase_Calibration_::phaseCorrection

Phase Correction between voltage and current (register units)


The documentation for this struct was generated from the following file:
© Copyright 1995-2018, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale