Contains EM Phase Background Results. More...
#include <emSwLib.h>
Data Fields | |
int32_t | vDCEstimate |
DC Estimate for Voltage. More... | |
int16_t | iDCEstimate [3] |
DC Estimate for Current. More... | |
int16_t | reactPowPrevV90 |
Previous V90 voltage used for the IIR filter in the reactive power calculation. More... | |
int16_t | vPrevSample |
Previous Voltage sample used for the IIR filter in the reactive power calculation. More... | |
int32_t | rogowskiPrevI90 |
Previous I90 current used for the IIR filter in the Rogowski ADC current calculation. More... | |
int32_t | iPrevSample |
Previous Current sample used for the IIR filter in the Rogowski ADC current calculation. More... | |
Contains EM Phase Background Results.
int32_t _EM_Phase_BG_Results_::vDCEstimate |
DC Estimate for Voltage.
int16_t _EM_Phase_BG_Results_::iDCEstimate[3] |
DC Estimate for Current.
int16_t _EM_Phase_BG_Results_::reactPowPrevV90 |
Previous V90 voltage used for the IIR filter in the reactive power calculation.
int16_t _EM_Phase_BG_Results_::vPrevSample |
Previous Voltage sample used for the IIR filter in the reactive power calculation.
int32_t _EM_Phase_BG_Results_::rogowskiPrevI90 |
Previous I90 current used for the IIR filter in the Rogowski ADC current calculation.
int32_t _EM_Phase_BG_Results_::iPrevSample |
Previous Current sample used for the IIR filter in the Rogowski ADC current calculation.