The automatic power down feature, when enabled, prevents the CapTIvate peripheral from shutting down into its low power state after the completion of a conversion. Normally (when disabled), The power-down occurs immediately following the completion of each time cycle's measurement. The next time a measurement is started, the peripheral will power back up. There will be a delay associated with the power-up.
Affected Software Parameters
The Frequency_Divider parameter corresponds to the
bLpmControl
member of the
tSensor
type in the CapTIvate Touch Library.